Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
S32 Design Studio for e200 v2.0 已过期 您好,NXP技术支持,我的S32 Design Studio for e200 v2.0许可证已过期。 请问能否延长我的激活码:9BBC-2CD1-60B7-FD1A 的有效期? 谢谢!
記事全体を表示
How to get stream for a Bayer sensor in IMX95 FRDM I am currently trying to port a Bayer sensor in iMX95 FRDM kit. I have got v4l2 stream and it is working fine. I created a dummy entry for my camera in libcamera consisting the yaml and it gets read properly. When I try pushing to the display I am facing an issue. I have attached the logs below. root@imx95-15x15-lpddr4x-frdm:~# v4l2-ctl -d 0 -v width=1920,height=1200,pixelformat='BA10' --strea m-mmap <<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 71.97 fps <<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 71.98 fps <<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 71.98 fps <<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<< 71.98 fps <<<<<<<<<<<<<<<<<<^C root@imx95-15x15-lpddr4x-frdm:~# cam -c 1 --info [0:03:42.550702911] [754] INFO Camera camera_manager.cpp:340 libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:03:42.659767149] [755] INFO MediaPipeline media_pipeline.cpp:240 Found pipeline: [ar0234 3-0042| 0] -> [0|csidev-4ad30000.csi|1] -> [0|4ac10000.syscon:formatter@20|1] -> [2|crossbar] [0:03:42.660611245] [755] WARN CameraSensorProperties camera_sensor_properties.cpp:586 No static pr operties available for 'ar0234' [0:03:42.660680697] [755] WARN CameraSensorProperties camera_sensor_properties.cpp:588 Please consi der updating the camera sensor properties database [0:03:42.660794714] [755] INFO Camera camera_manager.cpp:223 Adding camera '/base/soc/bus@42000000/ i2c@42540000/ar0234_mipi@42' for pipeline handler imx8-isi [0:03:42.661332196] [755] WARN ISI imx8-isi.cpp:296 Cannot find a supported YUV/RGB format Using camera /base/soc/bus@42000000/i2c@42540000/ar0234_mipi@42 as cam0 0: 1920x1200-SGRBG10/Unset * Pixelformat: SGRBG10 (1920x1200)-(1920x1200)/(+1,+1) - 1920x1200 root@imx95-15x15-lpddr4x-frdm:~# cam -l [0:03:45.833147768] [756] INFO Camera camera_manager.cpp:340 libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:03:45.940562253] [757] INFO MediaPipeline media_pipeline.cpp:240 Found pipeline: [ar0234 3-0042| 0] -> [0|csidev-4ad30000.csi|1] -> [0|4ac10000.syscon:formatter@20|1] -> [2|crossbar] [0:03:45.941374870] [757] WARN CameraSensorProperties camera_sensor_properties.cpp:586 No static pr operties available for 'ar0234' [0:03:45.941445068] [757] WARN CameraSensorProperties camera_sensor_properties.cpp:588 Please consi der updating the camera sensor properties database [0:03:45.941557994] [757] INFO Camera camera_manager.cpp:223 Adding camera '/base/soc/bus@42000000/ i2c@42540000/ar0234_mipi@42' for pipeline handler imx8-isi Available cameras: 1: External camera 'ar0234' (/base/soc/bus@42000000/i2c@42540000/ar0234_mipi@42) root@imx95-15x15-lpddr4x-frdm:~# export CAMERA0="/base/soc/bus@42000000/i2c@42540000/ar0234_mipi@42" root@imx95-15x15-lpddr4x-frdm:~# export LIBCAMERA_PIPELINES_MATCH_LIST='nxp/neo,uvc' root@imx95-15x15-lpddr4x-frdm:~# GST_DEBUG=3 gst-launch-1.0 libcamerasrc ! videoconvert ! autovideos ink Setting pipeline to PAUSED ... [0:04:22.673679060] [758] INFO Camera camera_manager.cpp:340 libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:04:22.784435713] [763] WARN CameraSensorProperties camera_sensor_properties.cpp:586 No static pr operties available for 'ar0234' [0:04:22.784524477] [763] WARN CameraSensorProperties camera_sensor_properties.cpp:588 Please consi der updating the camera sensor properties database [0:04:22.785576603] [763] WARN CameraSensorProperties camera_sensor_properties.cpp:586 No static pr operties available for 'ar0234' [0:04:22.785622610] [763] WARN CameraSensorProperties camera_sensor_properties.cpp:588 Please consi der updating the camera sensor properties database [0:04:22.793514826] [763] INFO IPAProxy ipa_proxy.cpp:180 Using tuning file /usr/share/libcamera/ip a/nxp/neo/ar0234.yaml [0:04:22.793673227] [763] INFO NxpNeoIPA neo_ipa.cpp:146 nxpneo: IPANxpNeo NXPNEO_IPA_v0.0.0+6489-l f-6.18.2-1.0.0 [0:04:22.793713608] [763] ERROR NxpNeoIPA neo_ipa.cpp:161 nxpneo: Failed to create camera sensor hel per for ar0234 [0:04:22.793740029] [763] ERROR NxpNeoPipe neo_pipeline.cpp:2169 Failed to initialise the NxpNeo IPA [0:04:22.793987693] [763] WARN NxpNeoPipe neo_pipeline.cpp:1268 Failed to probe camera ar0234 3-004 2: -19 0:00:00.425814325 758 0xaaab119eb6e0 WARN libcamerasrc gstlibcamerasrc.cpp:491:gst_libc amera_src_open: error: Could not find any supported camera on this system. 0:00:00.425887295 758 0xaaab119eb6e0 WARN libcamerasrc gstlibcamerasrc.cpp:491:gst_libc amera_src_open: error: libcamera::CameraMananger::cameras() is empty ERROR: from element /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0: Could not find any support ed camera on this system. Additional debug info: /usr/src/debug/libcamera/0.6.0.imx/src/gstreamer/gstlibcamerasrc.cpp(491): gst_libcamera_src_open () : /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0: libcamera::CameraMananger::cameras() is empty ERROR: pipeline doesn't want to preroll. Failed to set pipeline to PAUSED. Setting pipeline to NULL ... Freeing pipeline ... root@imx95-15x15-lpddr4x-frdm:~# cam -c 1 --info [0:04:28.421646898] [764] INFO Camera camera_manager.cpp:340 libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:04:28.529717355] [765] WARN CameraSensorProperties camera_sensor_properties.cpp:586 No static pr operties available for 'ar0234' [0:04:28.529795824] [765] WARN CameraSensorProperties camera_sensor_properties.cpp:588 Please consi der updating the camera sensor properties database [0:04:28.530673193] [765] WARN CameraSensorProperties camera_sensor_properties.cpp:586 No static pr operties available for 'ar0234' [0:04:28.530718283] [765] WARN CameraSensorProperties camera_sensor_properties.cpp:588 Please consi der updating the camera sensor properties database [0:04:28.535806348] [765] INFO IPAProxy ipa_proxy.cpp:180 Using tuning file /usr/share/libcamera/ip a/nxp/neo/ar0234.yaml [0:04:28.535946325] [765] INFO NxpNeoIPA neo_ipa.cpp:146 nxpneo: IPANxpNeo NXPNEO_IPA_v0.0.0+6489-l f-6.18.2-1.0.0 [0:04:28.535994624] [765] ERROR NxpNeoIPA neo_ipa.cpp:161 nxpneo: Failed to create camera sensor hel per for ar0234 [0:04:28.536070926] [765] ERROR NxpNeoPipe neo_pipeline.cpp:2169 Failed to initialise the NxpNeo IPA [0:04:28.536326960] [765] WARN NxpNeoPipe neo_pipeline.cpp:1268 Failed to probe camera ar0234 3-004 2: -19 Camera 1 not found Failed to create camera session root@imx95-15x15-lpddr4x-frdm:~# cam -l [0:04:32.340920574] [766] INFO Camera camera_manager.cpp:340 libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:04:32.448621532] [767] WARN CameraSensorProperties camera_sensor_properties.cpp:586 No static pr operties available for 'ar0234' [0:04:32.448700208] [767] WARN CameraSensorProperties camera_sensor_properties.cpp:588 Please consi der updating the camera sensor properties database [0:04:32.449531226] [767] WARN CameraSensorProperties camera_sensor_properties.cpp:586 No static pr operties available for 'ar0234' [0:04:32.449568106] [767] WARN CameraSensorProperties camera_sensor_properties.cpp:588 Please consi der updating the camera sensor properties database [0:04:32.454467330] [767] INFO IPAProxy ipa_proxy.cpp:180 Using tuning file /usr/share/libcamera/ip a/nxp/neo/ar0234.yaml [0:04:32.454600179] [767] INFO NxpNeoIPA neo_ipa.cpp:146 nxpneo: IPANxpNeo NXPNEO_IPA_v0.0.0+6489-l f-6.18.2-1.0.0 [0:04:32.454637351] [767] ERROR NxpNeoIPA neo_ipa.cpp:161 nxpneo: Failed to create camera sensor hel per for ar0234 [0:04:32.454663562] [767] ERROR NxpNeoPipe neo_pipeline.cpp:2169 Failed to initialise the NxpNeo IPA [0:04:32.454898508] [767] WARN NxpNeoPipe neo_pipeline.cpp:1268 Failed to probe camera ar0234 3-004 2: -19 Kindly let me know a solution for this.
記事全体を表示
FlexIoはUARTをシミュレートします こんにちは、 現在、御社のS32K118チップには以下の問題があります: (1) FlexIOを使ってSDKsバージョン(S32SDK_S32K1XX_RTM_4.0.1)でUARTをシミュレートすることでループバックテストが可能であり、公式デモもループバックの一例です。しかし、FlexIOのMCALバージョン(SW32K1_S32M24x_RTD_R21-11_3.0.0)を使ってUARTをシミュレートしたところ、ループバックテストが実行できないことが判明しました。MCAL版がサポートしていないからでしょうか? (2) MCAL版がサポートしていないことを踏まえ、FlexIOのSDK版を量産プロジェクトのUARTシミュレーションに使用した場合、セーフティの懸念はありますか? 幸運をお祈りしています、 NXP2。 Re: FlexIo Simulates UART こんにちは、 @NXP2さん ご質問を正しく理解できたかどうか自信がありませんが、FlexIO自体には専用の内部ループバック機能は搭載されていないことにご注意ください。SDKの例では、ループバックテストはFlexIO TXとRX信号を外部にワイヤーで接続することで実現されます。 S32SDK_S32K1XX_RTM_4.0.1に関しては、これは比較的古いソフトウェアリリースであり、現在は積極的にメンテナンスされていないことにご注意ください。一般的には、S32K1ファミリの最新ソフトウェアリリースであるSW32K1_S32M24x_RTD_R21-11_3.0.0の使用を推奨しており、メンテナンスアップデートやバグ修正、新機能が継続的に提供されています。 また、意図されたアプリケーションについてもう少し詳しく教えてもらえますか?そうすればあなたのユースケースをよりよく理解できるでしょう。 BR、VaneB Re: FlexIo Simulates UART こんにちは、 あなたの現在の理解は正しいです。現在の試験方法は、FlexIOTXとRX信号を外部の配線で接続するものです。 (1) 現在、乗用車ヘッドライトプロジェクトで使用は必要ですか?セーフティで何か懸念はありますか?、 (2)通常のLPUARTと何か違いはありますか?性能面で安定性と信頼性はありますか? よろしくお願いします、 NXP2 Re: FlexIo Simulates UART こんにちは、 @NXP2さん 通常、ループバックはペリフェラルや通信経路の機能性を検証するためのテストや検証目的で使用されます。これは一般的に、生産システムの通常の運用モードの一部として推奨されるものではありません。
記事全体を表示
E200 v2.0用のS32 Design Studioが期限切れとなりました こんにちは、NXPサポートの皆さん。私のS32 Design Studio v2.0のライセンスが切れました。 私のアクティベーションコード:9BBC-2CD1-60B7-FD1Aの権利を延長してもらえますか? よろしくお願いします。
記事全体を表示
[i.MX95] How to Change Lifecycle to OEM_CLOSED for Secure Boot on i.MX95 Rev.C We are working on enabling Secure Boot on an i.MX95 Rev.C hardware platform. We need to change the lifecycle state to OEM_CLOSED to lock down the bootloader and enable secure boot. Could you please provide guidance on: The proper procedure to transition the lifecycle to OEM_CLOSED on i.MX95 Rev.C? Any prerequisites or dependencies needed before making this change? Any documentation, examples, or best practices would be greatly appreciated. Thank you. Re: [i.MX95] How to Change Lifecycle to OEM_CLOSED for Secure Boot on i.MX95 Rev.C Please find the secure boot guide here : https://github.com/nxp-imx/uboot-imx/blob/lf-6.18.20-2.0.0/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt Re: [i.MX95] How to Change Lifecycle to OEM_CLOSED for Secure Boot on i.MX95 Rev.C We have followed the guide and following uboot command was used to set fuse values but values were not applied properly when read panchalprakrit_0-1782821101501.png We want to ask if there is any other way for changing lifecycle in Rev C board in GM CHM. Since, fuse prog seems to not work with uboot console. Re: [i.MX95] How to Change Lifecycle to OEM_CLOSED for Secure Boot on i.MX95 Rev.C Sorry, the link provided before doesn't contain AHAB 2.0, please ignore that. Here are the  SPSDK docs for enabling AHAB on i.MX95 Rev.C:  https://spsdk.readthedocs.io/en/latest/examples/ahab/imx95/imx95_ahab_uboot.html
記事全体を表示
FlexIo 模拟 UART 你好, 目前贵公司生产的S32K118芯片存在以下问题: (1)使用 FlexIO 模拟 SDK 版本(S32SDK_S32K1XX_RTM_4.0.1)的 UART 可以进行环回测试,官方演示也是环回测试的一个示例。然而,当使用 FlexIO 的 MCAL 版本 (SW32K1_S32M24x_RTD_R21-11_3.0.0) 模拟 UART 时,发现无法进行环回测试。是因为 MCAL 版本不支持吗? (2)考虑到 MCAL 版本不支持,如果使用 FlexIO 的 SDK 版本来模拟量产项目中的 UART,是否存在功能安全隐患? 最好的祝愿, NXP2。 Re: FlexIo Simulates UART 您好@NXP2 我不确定我是否正确理解了您的问题,但请注意,FlexIO 本身并不提供专用的内部环回功能。在 SDK 示例中,环回测试是通过使用导线将 FlexIO TX 和 RX 信号外部连接来实现的。 关于 S32SDK_S32K1XX_RTM_4.0.1,请注意,这是一个相对较旧的软件版本,目前已停止积极维护。我们通常建议使用 SW32K1_S32M24x_RTD_R21-11_3.0.0,因为它是 S32K1 系列的最新软件版本,并且会持续获得维护更新、错误修复和新功能。 另外,您能否提供更多关于该应用场景的信息?这将有助于我们更好地了解您的使用场景。 BR,VaneB Re: FlexIo Simulates UART 您好@NXP2 通常,环回用于测试和验证目的,以验证外围设备和通信路径的功能。一般不建议将其作为生产系统正常运行模式的一部分。 Re: FlexIo Simulates UART 你好, 你目前的理解是正确的。目前的测试方法是通过外部导线连接 FlexIOTX 和 RX 信号。 (1)目前,乘用车前照灯项目中是否有必要使用它?是否存在功能安全隐患?、 (2)与普通的LPUART有什么区别?它的性能是否稳定可靠? 此致, 恩智浦2
記事全体を表示
IMX95 FRDMでバイエルセンサーのストリームを取得する方法 現在、BayerのセンサをiMX95 FRDMキットに移植しようとしています。v4l2ストリームを取得しましたが、問題なく動作しています。libcameraにカメラ用のダミーエントリを作成し、YAMLファイルで記述したところ、正しく読み込まれました。ディスプレイにプッシュしようとすると問題が発生します。ログファイルを以下に添付しました。 root@imx95-15x15-lpddr4x-frdm:~# v4l2-ctl -d 0 -v width=1920,height=1200,pixelformat='BA10' --strea m-mmap <<< <<< <<< <<< <<<<<<<<<<<<<<<<<<^C root@imx95-15x15-lpddr4x-frdm:~# cam -c 1 --info [0:03:42.550702911][754] INFO カメラ camera_manager.cpp:340libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:03:42.659767149][755] INFO MediaPipeline media_pipeline.cpp:240パイプラインが見つかりました: [ar0234 3-0042| 0] -> [0|csidev-4ad30000.csi|1]-> [0|4ac10000.syscon:formatter@20|1]-> [2|クロスバー] [0:03:42.660611245][755] 警告 CameraSensorProperties camera_sensor_properties.cpp:586静的なprはありません 「ar0234」で利用可能な機能 [0:03:42.660680697][755] WARN カメラセンサープロパティ camera_sensor_properties.cpp:588 どうか カメラセンサープロパティデータベースの更新 [0:03:42.660794714][755] INFO カメラ camera_manager.cpp:223カメラ '/base/soc/bus@42000000/' を追加しています i2c@42540000/ar0234_mipi@42' (パイプライン ハンドラー imx8-isi) [0:03:42.661332196][755] ISI を警告 imx8-isi.cpp:296対応するYUV/RGBフォーマットが見つかりません カメラ/base/soc/bus@42000000/i2c@42540000/ar0234_mipi@42をcam0として使用しています。 0: 1920x1200-SGRBG10/未設定 * ピクセルフォーマット:SGRBG10 (1920x1200)-(1920x1200)/(+1,+1) - 1920x1200 root@imx95-15x15-LPDDR4x-frdm:~# cam -l [0:03:45.833147768][756] INFO カメラ camera_manager.cpp:340libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:03:45.940562253][757] INFO MediaPipeline media_pipeline.cpp:240パイプラインが見つかりました: [ar0234 3-0042| 0] -> [0|csidev-4ad30000.csi|1]-> [0|4ac10000.syscon:formatter@20|1]-> [2|クロスバー] [0:03:45.941374870][757] 警告 CameraSensorProperties camera_sensor_properties.cpp:586静的なprはありません 「ar0234」で利用可能な機能 [0:03:45.941445068][757] WARN カメラセンサープロパティ camera_sensor_properties.cpp:588 どうか カメラセンサープロパティデータベースの更新 [0:03:45.941557994][757] INFO カメラ camera_manager.cpp:223カメラ '/base/soc/bus@42000000/' を追加しています i2c@42540000/ar0234_mipi@42' (パイプライン ハンドラー imx8-isi) 利用可能なカメラ: 1: 外部カメラ「ar0234」(/base/soc/bus@42000000/i2c@42540000/ar0234_mipi@42) root@imx95-15x15-lpddr4x-frdm:~# export CAMERA0="/base/soc/bus@42000000/i2c@42540000/ar0234_mipi@42" root@imx95-15x15-lpddr4x-frdm:~# export LIBCAMERA_PIPELINES_MATCH_LIST='nxp/neo,uvc' root@imx95-15x15-lpddr4x-frdm:~# GST_DEBUG=3 gst-launch-1.0libcamerasrc !ビデオ変換!自動車動画 インク パイプラインを一時停止状態に設定しています... [0:04:22.673679060][758] INFO カメラ camera_manager.cpp:340libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:04:22.784435713][763] 警告 CameraSensorProperties camera_sensor_properties.cpp:586静的なprはありません 「ar0234」で利用可能な機能 [0:04:22.784524477][763] WARN カメラセンサープロパティ camera_sensor_properties.cpp:588 調和してください カメラセンサープロパティデータベースの更新 [0:04:22.785576603][763] 警告 CameraSensorProperties camera_sensor_properties.cpp:586静的なprはありません 「ar0234」で利用可能な機能 [0:04:22.785622610][763] WARN カメラセンサープロパティ camera_sensor_properties.cpp:588 調和してください カメラセンサープロパティデータベースの更新 [0:04:22.793514826][763] INFO IPAProxy ipa_proxy.cpp:180チューニングファイル /usr/share/libcamera/ip を使用しています a/nxp/neo/ar0234.yaml [0:04:22.793673227][763] INFO NxpNeoIPA neo_ipa.cpp:146nxpneo: IPANxpNeo NXPNEO_IPA_v0.0.0+6489-l f-6.18.2-1.0.0 [0:04:22.793713608][763] エラー NxpNeoIPA neo_ipa.cpp:161nxpneo:カメラセンサーヘルの作成に失敗しました ar 0234 の [0:04:22.793740029][763] エラー NxpNeoPipe neo_pipeline.cpp:2169NxpNeo IPA の初期化に失敗しました [0:04:22.793987693][763] 警告 NxpNeoPipe neo_pipeline.cpp:1268カメラar0234 3-004のプローブに失敗しました 2: -19 0:00:00.425814325 758 0xaaab119eb6e0 WARN libcamerasrc gstlibcamerasrc.cpp:491:gst_libc amera_src_open: エラー:このシステムでサポートされているカメラが見つかりませんでした。 0:00:00.425887295 758 0xaaab119eb6e0 WARN libcamerasrc gstlibcamerasrc.cpp:491:gst_libc amera_src_open: error: libcamera::CameraMananger::cameras() が空です エラー:from element /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0: サポートが見つかりませんでした このシステムにEDカメラが入っています。 追加のデバッグ情報: /usr/src/debug/libcamera/0.6.0.imx/src/gstreamer/gstlibcamerasrc.cpp(491):gst_libcamera_src_open() : /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0: libcamera::CameraMananger::cameras() は空です エラー: パイプラインがプリロールを実行しません。 パイプラインをPAUSED状態に設定できませんでした。 パイプラインをNULLに設定中... パイプラインを解放する... root@imx95-15x15-lpddr4x-frdm:~# cam -c 1 --info [0:04:28.421646898][764] INFO カメラ camera_manager.cpp:340libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:04:28.529717355][765] 警告 CameraSensorProperties camera_sensor_properties.cpp:586静的なprはありません 「ar0234」で利用可能な機能 [0:04:28.529795824][765] WARN カメラセンサープロパティ camera_sensor_properties.cpp:588 どうか カメラセンサープロパティデータベースの更新 [0:04:28.530673193][765] 警告 CameraSensorProperties camera_sensor_properties.cpp:586静的なprはありません 「ar0234」で利用可能な機能 [0:04:28.530718283][765] WARN カメラセンサープロパティ camera_sensor_properties.cpp:588 どうか カメラセンサープロパティデータベースの更新 [0:04:28.535806348][765] INFO IPAProxy ipa_proxy.cpp:180チューニングファイル /usr/share/libcamera/ip を使用しています a/nxp/neo/ar0234.yaml [0:04:28.535946325][765] INFO NxpNeoIPA neo_ipa.cpp:146nxpneo: IPANxpNeo NXPNEO_IPA_v0.0.0+6489-l f-6.18.2-1.0.0 [0:04:28.535994624][765] エラー NxpNeoIPA neo_ipa.cpp:161nxpneo:カメラセンサーヘルの作成に失敗しました ar 0234 の [0:04:28.536070926][765] エラー NxpNeoPipe neo_pipeline.cpp:2169NxpNeo IPA の初期化に失敗しました [0:04:28.536326960][765] 警告 NxpNeoPipe neo_pipeline.cpp:1268カメラar0234 3-004のプローブに失敗しました 2: -19 カメラ1が見つかりません カメラセッションの作成に失敗しました root@imx95-15x15-lpddr4x-frdm:~# cam -l [0:04:32.340920574][766] INFO カメラ camera_manager.cpp:340libcamera v0.0.0+6489-lf-6.18.2-1.0.0 [0:04:32.448621532][767] 警告 CameraSensorProperties camera_sensor_properties.cpp:586静的なprはありません 「ar0234」で利用可能な機能 [0:04:32.448700208][767] WARN カメラセンサープロパティ camera_sensor_properties.cpp:588 お願いします カメラセンサープロパティデータベースの更新 [0:04:32.449531226][767] 警告 CameraSensorProperties camera_sensor_properties.cpp:586静的なprはありません 「ar0234」で利用可能な機能 [0:04:32.449568106][767] WARN カメラセンサープロパティ camera_sensor_properties.cpp:588 お願いします カメラセンサープロパティデータベースの更新 [0:04:32.454467330][767] INFO IPAProxy ipa_proxy.cpp:180チューニングファイル /usr/share/libcamera/ip を使用しています a/nxp/neo/ar0234.yaml [0:04:32.454600179][767] INFO NxpNeoIPA neo_ipa.cpp:146nxpneo: IPANxpNeo NXPNEO_IPA_v0.0.0+6489-l f-6.18.2-1.0.0 [0:04:32.454637351][767] エラー NxpNeoIPA neo_ipa.cpp:161nxpneo:カメラセンサーヘルの作成に失敗しました ar 0234 の [0:04:32.454663562][767] エラー NxpNeoPipe neo_pipeline.cpp:2169NxpNeo IPA の初期化に失敗しました [0:04:32.454898508][767] 警告 NxpNeoPipe neo_pipeline.cpp:1268カメラar0234 3-004のプローブに失敗しました 2: -19 この問題の解決策を教えていただけないでしょうか。
記事全体を表示
[i.MX95] 如何在 i.MX95 Rev.C 上将生命周期更改为 OEM_CLOSED 以启用安全启动 我们正在努力在 i.MX95 Rev.C硬件平台上启用安全启动。我们需要将生命周期状态更改为 OEM_CLOSED 以锁定引导加载程序并启用安全启动。 请问您能否就以下方面提供指导: 在i.MX95 Rev.C上将生命周期过渡到OEM_CLOSED的正确步骤是什么? 进行此更改之前需要任何先决条件或依赖项吗? 任何文档、示例或最佳实践都将不胜感激。 谢谢! Re: [i.MX95] How to Change Lifecycle to OEM_CLOSED for Secure Boot on i.MX95 Rev.C 请在此处查看安全启动指南: https://github.com/nxp-imx/uboot-imx/blob/lf-6.18.20-2.0.0/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt Re: [i.MX95] How to Change Lifecycle to OEM_CLOSED for Secure Boot on i.MX95 Rev.C 我们按照指南操作,并使用以下 uboot 命令设置了熔丝位值,但读取时这些值并未正确应用。 panchalprakrit_0-1782821101501.png 我们想请问在 GM CHM 中,Rev C 板的生命周期是否还有其他更改方法?因为 熔丝 prog 似乎无法与 uboot 控制台配合使用。 Re: [i.MX95] How to Change Lifecycle to OEM_CLOSED for Secure Boot on i.MX95 Rev.C 抱歉,之前提供的链接不包含 AHAB 2.0,请忽略。 以下是用于在 i.MX95 Rev.C 上启用 AHAB 的 SPSDK 文档: https://spsdk.readthedocs.io/en/latest/examples/ahab/imx95/imx95_ahab_uboot.html
記事全体を表示
FlexIo Simulates UART Hello, Currently, there are the following issues with the S32K118 chip from your company: (1) Using FlexIO to simulate UART with the SDK version (S32SDK_S32K1XX_RTM_4.0.1) allows for loopback testing, and the official demo is also an example of loopback. However, when using the MCAL version (SW32K1_S32M24x_RTD_R21-11_3.0.0) of FlexIO to simulate UART, it was found that loopback testing could not be performed. Is it because the MCAL version does not support it? (2) Considering that the MCAL version does not support it, if the SDK version of FlexIO is used to simulate UART for mass production projects, are there any safety concerns? Best Wishes, NXP2. Re: FlexIo Simulates UART Hi @NXP2  I am not sure if I understood your question correctly, but please note that FlexIO itself does not provide a dedicated internal loopback feature. In the SDK example, the loopback test is achieved by connecting the FlexIO TX and RX signals externally using a wire. Regarding S32SDK_S32K1XX_RTM_4.0.1, please note that this is a relatively old software release and is no longer being actively maintained. We generally recommend using SW32K1_S32M24x_RTD_R21-11_3.0.0, as it is the latest software release for the S32K1 family and continues to receive maintenance updates, bug fixes, and new features. Also, could you provide a bit more information about the intended application? That would help to better understand your use case. BR, VaneB Re: FlexIo Simulates UART Hi @NXP2  Typically, a loopback is used for testing and validation purposes to verify the functionality of the peripheral and communication path. It is generally not recommended as part of the normal operating mode of a production system. Re: FlexIo Simulates UART Hello, Your current understanding is correct. The current testing method involves connecting FlexIOTX and the RX signal through external wires. (1) Currently, is it necessary to use it in the passenger vehicle headlight project? Are there any safety concerns? 、 (2) Is there any difference from the normal LPUART? Is it stable and reliable in terms of performance? Best regards, NXP2
記事全体を表示
CAN Bus Handling in MBDT I’m using NXP’s MBDT for S32K344 for configuring FlexCAN0. I want to understand what part of CAN message handling is managed by the NXP blocks/toolbox and what needs to be handled by the application. Are arbitration and buffer handling managed by the driver/toolbox? Example: If I send 0x18FEF111 first, then 0x18FEEF00 neither appears on the bus. But if 0x18FEEF00 is sent first, both are transmitted. When triggered together, only one appears. So, do we need to assign dedicated Tx Hardware Objects to each message ID when sending multiple frames simultaneously? Does the MBDT or SDK handle message prioritization and retries automatically if ACK is not received? If a high-priority ID fails (e.g., no ACK), will it block other messages? How do we detect and recover from this? Do we need to manage buffer allocation or transmission timing manually in the model to avoid blocking or message loss? What’s the best way to configure multiple Tx message IDs in MBDT? With dynamic buffers. Please clarify what is handled internally vs. what we must handle in the application. Example Models Re: CAN Bus Handling in MBDT Hello @SorinIBancila , I've run into a scenario where I need to send more frames than the available HTH hardware object count. Since the CanIf transmit buffering implementation cannot be leverage in S32CT, can you recommend simulink-based buffer solution to this problem? Thanks & regards, Sandesh Re: CAN Bus Handling in MBDT Hello, The 32 Can Hw Object Count is not the limit. You can increase the limit even further, depending on what MCU you have. You can modify the number of Can Hw Object Count and if you put a number too large, the S32CT is going to throw an error. Best regards, Sorin Bancila Re: CAN Bus Handling in MBDT Understood! So If I need to transmit more than 32 messages, should I create additional Tx Hardware Objects? Also, what is the maximum number of Hardware Objects that can be configured under a single CAN transceiver or controller in S32K3 using S32CT? Looking to understand the best way to structure HOHs for large message sets while staying within the limits. Re: CAN Bus Handling in MBDT Hello, How many messages do you think you need to transmit at one time? I've tested on a S32K358 HVBMS reference design the following scenario: Use a single TX Hardware Object and set the Can Hw Object Count to 32 (to allow a maximum of 32 messages in the buffer). SorinIBancila_0-1751890828580.png In Simulink, I populated the message buffer with 32 messages, increasing the priority as it populates the buffer, to prove the arbitration process. SorinIBancila_3-1751891054922.png The results: As expected, the first messages sent are with low priority, as the message buffer is not completely populated. Around the 6th message, the buffer is populated and we can see that the messages with higher priority are sent first. SorinIBancila_5-1751891107134.png Since you want to use a single transceiver, it is not really possible to simultaneously send all the messages at the same time. Best regards, Sorin Bancila Re: CAN Bus Handling in MBDT Hi Sorin, Thanks for your input! I wanted to clarify the best way to configure multiple Tx message IDs in MBDT when using dynamic buffers. In my case, the controller is being used for an EV application with a J1939-based CAN setup involving hundreds of cyclic messages. Creating separate hardware objects for each message in S32CT doesn’t seem scalable or practical. I’m looking to use a single Tx Hardware Object to handle multiple messages dynamically and transmit them simultaneously over one CAN interface. Could you please guide on the recommended setup or best practice for this use case? Also please do suggest the documentation I must refer in order to understand the working of config setting and involved Functions used in MBDT. Re: CAN Bus Handling in MBDT Hello, First of all, I want to point out that the MBDT for S32K3xx is build on top of the S32K3 RTD. The configuration of a peripheral is done in the S32 Configuration Tool to allow full flexibility on the settings you need. So basically, to check if a feature is supported by the NXP's MBDT S32K3xx, you can check the source code used by the peripheral (in the S32K3 RTD) and its available settings in the S32 Configuration Tool. In the toolbox, you can find the implementation for the FlexCAN peripheral here: {toolboxRoot}/src/S32K3_RTD/SW32K3_S32M27x_RTD_R21-11_6.0.0/eclipse/plugins/Can_43_FLEXCAN_TS_T40D34M60I0R0/ Note! The name of the S32K3 RTD might differ, depending on which version of the MBDT S32K3 do you use. The answers to your questions are based on my experience and they might not be totally accurate. 1 & 2 & 5: The toolbox does not handle any arbitration, but I am not sure what options are available in the SDK for this matter. In your example, you create another CanHardwareObject and use it to send the second message, but this approach might be difficult to manage. The second solution might be to increate the Can Hw Object Count to allow more messages in the buffer. SorinIBancila_0-1751638634625.png 3: The MBDT for S32K3 does not handle any message prioritization. As far as I know, that's the job of the FlexCAN controller to retry to send the message until the ACK is received, while blocking the message the buffer. 4. One way to detect if a message is sent or not is to use interrupt CanIf_TxConfirmation in the Hardware Interrupt Callback to mark that a message is sent. If the interrupt is not triggered for the specified PDU, it means that the message is not sent. Moreover, there is another interrupt (CAN_ControllerBusOff) available that triggers when the conditions for CAN Bus Off are met. In the S32 Configuration Tool, there is an option to automatically recover from Bus Off. SorinIBancila_1-1751640323228.png If you have any questions, do not hesitate to reply. Best regards,  Sorin Bancila Re: CAN Bus Handling in MBDT Hello, Hello, I think one way to bypass the Hw Object Count limit is to configure multiple CAN controllers and to connect them to the same bus. Then, to avoid receiving messages sent from the other CAN Controller, you can take advantage of filter codes and masks to discard the messages right at the controller level. (offloading the MCU). Then, in the Simulink, you can use both CAN Controller to send data to the bus, either by round robin or any method you find suitable. I did not try this method yet, but I will keep you updated to see if it works. Best regards, Sorin Bancila
記事全体を表示
S32K388 LPSPIのSCKDIV計算に関する質問 - 1MHzのボーレートでSCKDIV=38になるのはなぜですか? こんにちは、NXPコミュニティの皆さん、 私はS32K388を使用してLPSPIのボーレートを設定しています。SCKDIVの値の計算について質問があります。 **私の理解:** S32K3xxリファレンスマニュアルによると、LPSPIのボーレートの公式は以下の通りです: ``` SCK = LPSPI_CLK / (PRESCALE_DIV × (SCKDIV + 1)) ``` **私の設定:** - LPSPIクロックソース:AIPS_SLOW_CLK = 40 MHz 目標ボーレート:1MHz - プリスケール = 0 (÷1) **私の計算:** 「`」 SCKDIV = (LPSPI_CLK / Baud) - 1 SCKDIV = (40 MHz / 1 MHz) - 1 = 39 「`」 **S32DS生成コード:** しかし、S32DSを使用して構成を生成すると、次のようになります。 「`c」 LPSPI_CCR_SCKDIV(38U) // SCKDIV = 38 「`」 **質問:** SCKDIV=38の場合、実際の除算係数は39となり、これは次のことを意味します。 「`」 実際のボーレート = 40 MHz / 39 = 1,025,641 Hz ≈ 1.026 MHz 「`」 これは目標値である1MHzから約2.56%の誤差がある。 S32DSはなぜSCKDIV=39ではなくSCKDIV=38を使用するのですか?S32DS構成では、異なるLPSPIクロック周波数が使用されているのでしょうか?それとも、この選択には別の理由があるのでしょうか? **追加の背景:** - 私はS32DS 3.5を使っています - S32K388リファレンス・マニュアル Rev. 6 - プロジェクトはデフォルトのクロック構成で作成されました ご説明いただければ幸いです。よろしくお願いいたします。 よろしくお願いいたします。 Re: S32K388 LPSPI SCKDIV calculation question - why SCKDIV=38 for 1MHz baud rate? こんにちは、 @xlele まず、S32K3xxリファレンスマニュアルの最新版はRev. 12であることにご注意ください。現在ご利用の改訂版には、S32K310、S32K311、およびS32K3x8デバイスに関する予備情報が含まれていますが、これらのデバイスは当該文書の発行時点ではまだリリースされていませんでした。したがって、RMの最新版をダウンロードして参照することをお勧めします。 LPSPIのボーレート計算に関して、クロック構成レジスタ(CCR)のSCKDIVフィールドの説明には次のように記載されています。 ボーレート = 機能クロック ÷ (2^PRESCALE × (SCKSET + SCKHLD + 2)) ここで、SCKSETとSCKHLDはSCKDIV÷2から導出される。 SCKDIV = 38 であることを考慮すると、次のようになります。 SCKSET = SCKHLD = 38 ÷ 2 = 19 ボーレート = 40 MHz ÷ (2^0 × (19 + 19 + 2)) = 1 MHz となり、これは期待値と一致します。 BR、VaneB
記事全体を表示
S32 Design Studio version v.3.4 expired My S32 Design Studio for S32 Platform v.3.4  expired, could you please expand the license? Order Number: S32DS-3-4_156834637 Total Number of Licenses: 101 Activation Code: 7F70-B731-EFE8-3F4B Thank you very much. Re: S32 Design Studio version v.3.4 expired Hi,  your S32DS license has been extended, please activate S32DS again with your old code. 
記事全体を表示
Wi-Fi芯片组MCU控制 大家好, 我正在寻找一些具有 AP+STA 功能的 Wi-Fi 模块。例如,我找到了一些来自恩智浦半导体(NXP)、微芯科技(Microchip)和英飞凌科技(Infineon)的模块。然而,大多数模块仅通过 PCIe 和高级操作系统启用 wifi 接口。 不过,我找到了一套来自英飞凌的名为 AIROC CYW55X(系列)的 MCU+Wifi 模块。 您在集成和控制这类模块方面有经验吗?如果可以的话,您能否分享一下您之前使用过并成功与外部MCU集成的不同模块?我的目的不是将数据卸载到微控制器,而只是为了控制例如网状网络和接入点功能。 我想使用 MCU(例如 STM)对一些基本的 AI 模型进行一些推理,同时控制 wifi 模块。 谢谢大家 Re: Wi-Fi Chipset MCU Control 你好@maiyaa ,希望你一切都好。 如果您对托管无线模块感兴趣,我建议您查看IW611 ,因为该 SoC 通过 SDIO 提供 Wi-Fi 接口,并且受 FreeRTOS 支持。此外,请参阅我们的Wi-Fi + 蓝牙 + 802.15.4 合作伙伴模块页面,其中包含所有集成 IW611 的模块。您还会看到每个模块的推荐主机,对于 MCU,建议与 IW611+RT1060 配合使用。 顺便提一下,我建议查看一下RW61X 系列,因为这些是无主机解决方案,在 MCU 中集成了 Wi-Fi+蓝牙+802.15.4(RW612)或 Wi-Fi+蓝牙(RW610)无线电。 请告诉我这些解决方案是否符合您的要求,或者您是否有需要涵盖的特定功能,以便我能提供更好的建议。
記事全体を表示
S32 Design Studio for e200 v2.0 expired Hi NXP Support, my license for S32 Design Studio for e200 v2.0 has expired. Could you please extend the entitlement for my Activation code: 9BBC-2CD1-60B7-FD1A? Thank you.
記事全体を表示
Wi-Fi Chipset MCU Control Hello everyone, I was browsing for some wifi modules with AP+STA functionalities. I found some modules from NXP, Microchip, and Infineon for example. However, most of the modules are only enabling wifi interface through PCIe and with advanced OS. However, I found a set of MCU+Wifi module from infineon called AIROC CYW55X (series). Do you have any experience integrating and controlling these type of modules? If so, can you share different modules that you have used before and were able successful to integrate with an external MCU? My intention is not to offload data to the microcontroller, only to control for example the mesh and AP capabilities. I want to use a MCU (STM for example) to perform some inference on some basic AI models while controlling the wifi module. Thanks guys Re: Wi-Fi Chipset MCU Control Hello @maiyaa, hope you are doing well. If you are interested on hosted wireless modules, I would suggest checking the IW611 as this SoC provides Wi-Fi interfacing through SDIO and is supported on FreeRTOS. Additionally, please refer to our Wi-Fi + Bluetooth + 802.15.4 Partner Modules page which includes all of the modules that integrate the IW611. You will also see the recommended hosts for each module, which for MCUs, it is suggested to work with IW611+RT1060. As a side note, I would recommend checking the RW61X family, as these are hostless solutions that integrate Wi-Fi+Bluetooth+802.15.4 (for RW612) or Wi-Fi+Bluetooth (for RW610) radios within the MCU. Please let me know if any of these solutions meet your requirements, or if you have an specific feature to cover so I can provide a better recommendation.
記事全体を表示
S32 设计工作室版本 v.3.4 已过期 我的 S32 设计工作室(适用于 S32 平台)v.3.4许可证已过期,请问能否延长许可证期限? 订单号: S32DS-3-4_156834637 许可证总数: 101 激活码: 7F70-B731-EFE8-3F4B 非常感谢。 Re: S32 Design Studio version v.3.4 expired 你好, 您的 S32DS 许可证已延期,请使用您的旧代码重新激活 S32DS。
記事全体を表示
为了完善解决方案,本文将介绍如何在 MCUXpresso IDE 中使用 printf 函数打印浮点数。 您好: 之前的主题中讨论过如何在 MCUXpresso IDE 和 SDK 中打印浮点数。 尝试这些方法并总结最终解决方案: 1. 将浮点数打印到 UART 控制台 在项目配置->C/C++ 版本->设置中设置以下宏 PRINTF_FLOAT_ENABLE=1 这样的代码可以运行。 float test1 = 0.15; PRINTF("%f\r\n",test1); 2.使用 sprintf() 函数将浮点数转换为字符串。 SDK 用户手册中有一处错误:“请确保已选择 Redlib: 使用 printf 的浮空版本”。 “在项目创建过程中不起作用。” 默认的 C 库 Redlib 不支持浮空,因此无法与 redlib 一起使用。 daweiyou_0-1647929545419.png 正确答案是: (1)将链接库更改为 NewLib,它是一个完整的 C 库,支持浮点 printf。 但请注意,需要在相关的 c 文件中包含 ,否则 sprintf(float) 将无法按预期工作。 daweiyou_1-1647929662327.png (2)将链接库更改为 NewLib Nano,这是一个紧凑的 C 库,需要点击“启用 print float”来启用 float 函数,这实际上会添加“-u _printf_float”链接符号。 但请注意,需要在相关的 c 文件中包含 ,否则 sprintf(float) 将无法按预期工作。 daweiyou_2-1647929807476.png 因此,该解决方案肯定会增加项目的闪存和内存消耗,但对于 i.MXRT 系列来说,这不是问题。 附件是 RT1020 EVK 的一个例子。 Re: To complement solution how to printf float number in MCUXpresso IDE 谢谢你!问题解决了。 Re: To complement solution how to printf float number in MCUXpresso IDE 嗨@daweiyou 非常感谢您的贡献。这些信息很有帮助,可能对很多人都有用。 再次感谢。 此致。 巴勃罗·阿瓦洛斯。
記事全体を表示
S32 Design Studio バージョン v.3.4 の期限切れ 私のS32 Design Studio for S32 プラットフォーム v.3.4期限切れです。ライセンスを拡大していただけますか? 注文番号: S32DS-3-4_156834637 ライセンス総数: 101 アクティベーションコード: 7F70-B731-EFE8-3F4B ご返信よろしくお願いします。 Re: S32 Design Studio version v.3.4 expired こんにちは、 S32DSのライセンス期間が延長されました。以前のコードを使用してS32DSを再度アクティベートしてください。
記事全体を表示
MCUXpresso IDEsでfloat番号を印刷する方法を補完するために こんにちは: 以前のトピックでは、MCUXpresso IDEsやSDKsでfloat番号を印刷する方法についての議論がありました。 それらを試してみて、最終的な解決策をまとめると次のようになります。 1.浮動小数点数をUARTコンソールに出力します。 プロジェクト構成->C/C++ビルド->設定で以下のマクロを設定してください。 PRINTF_FLOAT_ENABLE=1 そのコードは動作するはずです。 float test1 = 0.15; PRINTF("%f\r\n",test1); 2. sprintf() 関数を使用して浮動小数点数を文字列に変換します。 SDKユーザーマニュアルには「Ensure Redlib: Use floating some version of printfが選択される」というエラーがあります プロジェクト作成中は動作しません。 デフォルトのCライブラリであるRedlibはフローティングをサポートしていないため、redlibでは動作しません。 daweiyou_0-1647929545419.png 正解は以下の通りです。 (1)リンクライブラリをNewLibに変更してください。完全なCライブラリでfloat printfもサポートします。 ただし、関連する c ファイルに を含める必要があることに注意してください。そうしないと、sprintf(float) が期待どおりに動作しません。 daweiyou_1-1647929662327.png (2)リンクライブラリをNewLib Nanoに変更します。これはコンパクトなCライブラリで、「enable print float」をクリックしてfloat関数を有効にする必要があります。これにより、実際には「-u _printf_float」リンクシンボルが追加されます。 ただし、関連する c ファイルに を含める必要があることに注意してください。そうしないと、sprintf(float) が期待どおりに動作しません。 daweiyou_2-1647929807476.png SO、プロジェクトでは確実にフラッシュとRAM消費が増えますが、i.MXRTシリーズでは問題ありません。 AttachはRT1020 EVKの一例です。 Re: To complement solution how to printf float number in MCUXpresso IDE ありがとう!これで問題は解決しました。 Re: To complement solution how to printf float number in MCUXpresso IDE こんにちは@daweiyou ご協力ありがとうございますSO。その情報はとても役に立ち、多くの人にも役立つかもしれない。 改めてありがとうございました。 よろしくお願いします。 パブロ・アバロス。
記事全体を表示
Wi-FiチップセットMCU制御 こんにちは、みんな、 AP+STA機能を備えたWi-Fiモジュールを探していました。例えば、NXP、Microchip、Infineonなどのモジュールを見つけました。しかし、ほとんどのモジュールはPCIe経由でWiFiインターフェースを使えず、高度なOSでしか対応していません。 しかし、InfineonのAIROC CYW55X(シリーズ)というMCU+WiFiモジュールのセットを見つけました。 こういったタイプのモジュールの統合や制御に関する経験はありますか?もしそうなら、これまでに使っていて外部MCUとうまく統合できた他のモジュールを教えてもらえますか?私の意図は、データをマイクロコントローラにオフロードするのではなく、例えばメッシュやAPの機能を制御することです。 Wi-Fiモジュールを制御しながら基本的なAIモデルに対して推論を行うために、MCU(例えばSTM)を使っています。 ありがとう、みんな Re: Wi-Fi Chipset MCU Control こんにちは、 @maiyaa さん。お元気でお過ごしでしょうか。 ホスト型ワイヤレスモジュールにご興味があるなら、 IW611を検討してみてはいかがでしょうか。このSoCはSDIOを介してWi-Fiインターフェースを提供し、FreeRTOSでサポートされています。さらに、IW611を統合するすべてのモジュールを含む Wi-Fi + Bluetooth + 802.15.4パートナーモジュール のページもご参照ください。また、各モジュールの推奨ホストも表示されます。MCUの場合はIW611+RT1060で動作することが推奨されています。 ちなみに、 RW61Xファミリはホストレスで、Wi-Fi+Bluetooth+802.15.4(RW612用)やWi-Fi+Bluetooth(RW610用)ラジオをMCU内に統合するソリューションです。 これらのソリューションのどれかがご要望に合っているか、または特定の特徴があれば教えてください。より良いおすすめをお伝えします。
記事全体を表示