Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
BFU910Fモデル SPICE対応のGummel-Poonデバイスモデルは11年前のデータシートで約束されていました。提供されているのは、独自のフォーマットで作られたMextramモデルのみです。LTspiceはMextram 504モデルの互換性を謳っていますが、なぜでしょうか? RF Re: BFU910F model 知っていますが、2021年のNXPの記事で「ハイエンドRFのFUTURE」と称されているにもかかわらず、代替品は存在しません。いずれにせよ、データシートを見る限りかなり印象的な部品です。在庫がなくなる前に、もっと詳しく記録に残してほしいですね :3 Re: BFU910F model Hello BFU910Fは現在製造中止となっておりますのでご注意ください。
View full article
关于 LC 晋升的查询(S32K3,无 HSE) 你好, 关于在不使用 HSE 时锁定调试访问权限的顺序,我有一些疑问,特别是关于生命周期推进过程。 1) 在 IVT 中将配置字写入生命周期配置地址后,功能 RESET (SW_FUNC) 是否足以推进生命周期,还是需要破坏性 RESET (SW_DEST)? 2) 如果功能 RESET 足以推进生命周期,那么在 IVT 中配置的生命周期配置地址可以是 RAM 地址吗? 3) 我希望我的应用程序有条件地锁定调试访问端口(假设应用程序只有在收到特定的 CAN 消息后才应该设置密码并推进生命周期)。此外,我不想仅仅为了设置配置字来推进 MCU 的生命周期而占用/保留整个闪存扇区。因此,与其在 IVT 中永久设置生命周期配置地址,并在需要推进生命周期时向该地址写入 0xDADADADA/0xBABABABA,我想知道是否可以将配置字嵌入到我的应用程序中的固定地址,这样,每当应用程序决定限制调试访问时,应用程序就可以修改 IVT 来设置生命周期配置地址并启动 RESET。 这种方法可行吗? 如果可以,我该如何在运行时修改 IVT(是否有任何注意事项)?此外,IVT 是否可以包含 MCU 剩余工作生命周期内的生命周期地址(假设指定地址中的数据固定为配置字)? 如果没有,是否有其他方法可以达到同样的目的? 4) 关于设置密码本身 (cust_db_pswd_a) - 我可以通过调试器对此(以及一般的 UTEST OTP 数据)进行编程吗?还是必须由固件来完成? 此致, 哈里什·S Re: Query regarding LC advancement (S32K3, No HSE) 嗨@Hareesh_S 1.是的,发出功能 RESET 足以触发信号生命周期推进过程。 2.一般而言,我不建议使用 RAM 地址作为 LC 配置字。建议将其存储在非易失性存储器中,以确保在 SBAF 尝试读取它时它仍然可用。 3.你的总体目标是可行的;但是,我不建议在运行时修改 IVT。 建议的做法是在生产编程期间在 IVT 中配置生命周期配置地址,并保持其固定不变。当您的应用程序收到所需的 CAN 消息时,它可以简单地将适当的 LC 配置字(例如,0xDADADADA 或 0xBABABABA,具体取决于所需的转换)写入预定义的位置,然后发出功能复位。 4.是的,密码可以通过调试脚本进行编程;不一定需要通过固件进行编程。 但是,在对它或任何其他 UTEST OTP 数据进行编程之前,必须通过写入位于地址 0x40268358 的 PFCBLKU_SPELOCK 寄存器来解锁 UTEST 扇区。 BR,VaneB Re: Query regarding LC advancement (S32K3, No HSE) 你好@VaneB , 很抱歉回复晚了,非常感谢您的澄清!
View full article
Query regarding LC advancement (S32K3, No HSE) Hello, I have a few queries regarding the sequence to lock debug access when HSE is not used, specifically with regard to the life cycle advancement process. 1) After writing the configuration word to the life cycle configuration address in the IVT, will a functional reset(SW_FUNC) be sufficient to advance the life cycle or would I require a destructive reset (SW_DEST)? 2) If a functional reset is sufficient to advance the life cycle, can the life cycle configuration address configured in the IVT be a RAM address? 3) I want my application to conditionally lock the debug access port (let's say the application should only set the password and advance the life cycle once it receives a specific CAN message). Additionally I do not want to block/reserve a whole sector of flash just to set the configuration word to advance the life cycle of the MCU - As such, instead of permanently setting the LC configuration address in the IVT and writing 0xDADADADA/0xBABABABA to said address when I want to advance the life cycle, I was wondering if I could embed the configuration word as part of my application at a fixed address, and whenever the application decides to restrict debug access, the application could modify the IVT to set the life cycle configuration address and initiate a reset. Is this approach feasible? If yes, how can I go about modifying the IVT in runtime(are there any precautions I must take)? Additionally, is it okay for the IVT to contain the life cycle address for the remainder of the MCU's operating lifetime (assuming the data in the specified address is fixed to the configuration word) If no, are there alternate suggestions to achieve the same? 4) Regarding setting the password itself (cust_db_pswd_a) - Can I program this (and UTEST OTP data in general) via a debugger or must the firmware do it? With regards, Hareesh S  Re: Query regarding LC advancement (S32K3, No HSE) Hi @Hareesh_S  1. Yes, issuing a functional reset is sufficient to trigger the life cycle advancement process. 2. In general, I would not recommend using a RAM address for the LC configuration word. It is recommended to store it in non-volatile memory  to ensure that it remains available when the SBAF attempts to read it. 3. Your overall goal is feasible; however, I would not recommend modifying the IVT at runtime. A recommended approach would be to configure the life cycle configuration address in the IVT during production programming and keep it fixed. When your application receives the required CAN message, it can simply write the appropriate LC configuration word (for example, 0xDADADADA or 0xBABABABA, depending on the desired transition) to the predefined location and then issue a functional reset. 4. Yes, the password can be programmed using a debugger script; it does not need to be programmed exclusively by the firmware. However, before programming it or any other UTEST OTP data, it is necessary to unlock the UTEST sector by writing to the PFCBLKU_SPELOCK register located at address 0x40268358. BR, VaneB Re: Query regarding LC advancement (S32K3, No HSE) Hello @VaneB, Apologies for the delayed response, and much thanks for the clarification!
View full article
离线 MISR 值计算 我目前正在研究 S32K312 控制器的闪存阵列完整性实现。 根据参考手册,MISR 值是使用下图所示的特定多项式计算的。然而,即使多次尝试,我离线计算的 MISR 值也与用户模式 (UM) 寄存器中生成的值不符。 经进一步审查,我注意到 MISR 计算是在 ECC 检测之后进行的,而 ECC 奇偶校验不能离线计算。 能否请您提供一下该实现方案的标准生产级方法?具体来说,我想了解: 1. 是否可以离线计算预期的 MISR 值并将其存储在 Flash 或 NVM 中? 2. 或者是否需要运行一次代码,直接从 UM 寄存器中捕获计算出的 MISR 值并将其保存以供将来检查? 请指导我如何制定一个可用于生产环境的解决方案的推荐策略。 此致, 桑迪普·辛格 Re: Offline MISR value calculation 你好@sandeepSingh18606 , 1. 让我内部确认一下离线计算是否有任何进展。 我会尽快回复您。 2. 这也是一种选择。以下是一个示例: https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FLS-Integrity-Margin-Check-v1-0-S32DS36-RTD701/ta-p/2416160 BR,丹尼尔 Re: Offline MISR value calculation 嗨,丹尼尔, 过去七八个月以来,我一直收到同样的回复。之前我曾就此问题提交过工单,得到的回复与现在完全相同。我也联系过恩智浦的销售代表,但问题仍然没有解决。 请问NXP是否测试过此功能,以及目前是否有针对此问题的有效修复或变通方案? 期待您的尽快回复。 此致, 桑迪普·辛格
View full article
LMBCTLEN、LMAUTOEN、LMEN、LMSTAT の関係 こんにちは、NXPサポートの皆さん、 - 次の図のように、LMAUTOENとLMENを同時に有効にした場合、何か競合が発生しますか? 推奨される構成は何ですか?手動モード(LMEN経由)または自動モード(LMAUTOEN経由)? 自動モードがあるのに、どのような場合に手動モードを使用する必要があるのでしょうか? ありがとうございます。 BR/くまモン Re: LMBCTLEN, LMAUTOEN, LMEN, LMSTAT Relation こんにちは、 @kumamon さん。 1.実際には、利益相反はなく、S32K3XXリファレンス・マニュアルのパワーマネージメント章の中にも関連注意があります。 2. & 3.自動ラストマイル自動イネーブ機能により、チップの起動やスタンバイモードの復旧時に、起動レギュレーターの代わりにラストマイルレギュレーターを使用できます。 「手動モード」では、PLLを有効にする前にLMENを有効にする必要があります。スタンバイモード終了後、より高速なクロック周波数に移行する前に、PMCラストマイルレギュレータを再度有効にする必要があります。 図180を参照してください。ラストマイルレギュレータ有効化シーケンス: LMBCTLENについては、PCB上でVDD_HV_AとV15の間に外部BJTを使用する場合は、1に設定する必要があります。例えば、S32K3X4EVBでNPNを使用する場合は、LMBCTLEN = 1に設定します。 よろしくお願いします、 ジュリアン Re: LMBCTLEN, LMAUTOEN, LMEN, LMSTAT Relation こんにちは、 @Julián_AragónM さん、 ご返信ありがとうございます。 PMC.CONFIG[LMAUTOEN] フィールドの設定に関係なく、より高速なクロック周波数に移行する前に、PMC.CONFIG[LM_EN] フィールドに 1 を書き込む必要があります。これは、ブートレギュレータを使用する際にクロック速度が低下するためです。 1. 上記の発言の背景には何がありますか?自動モードはチップ自体でできると思うのに、なぜこの場合もソフトウェアの干渉が必要なのでしょうか?そして、以下の理解は正しいでしょうか? 自動モードのみ:不可。 手動モードのみ: OK 。 手動モード+自動モード: OK 。 2. 「マニュアルモード+オートマチックモード」は「マニュアルモードのみ」よりも常に優れているようですね?どのような状況で、自動モードは想定されないのでしょうか?これは、例えばチップの起動時にブートレギュレータのみを使用したいというシナリオでしょうか? 3. 従来のプロジェクトでは、FIRCよりも高いクロック(160MHz)を使用する場合でも、ラストマイルレギュレータをオンにしませんでした。私たちはそれがRMの規定に違反していることを知っています。そして私たちはリスクを推定しているのですが、最悪の場合、どのような結果になるかご存知ですか? ありがとうございます。 BR/くまモン Re: LMBCTLEN, LMAUTOEN, LMEN, LMSTAT Relation こんにちは、 @kumamon さん。 LMAUTOEN + LMENの機能に関する包括的な回答を提供するために、社内チームに動作確認をさせてください。 質問3について: PLLが有効になっているにもかかわらず、ラストマイルレギュレータが有効になっていない場合、チップはブートレギュレータによって給電されます。PLLクロックでは、コアが大きな電流を要求し、ブートレギュレータに熱が蓄積されます。これにより、チップが過熱して損傷する可能性があります。 リファレンス・マニュアルに従うことは必須です:「LMEN=0の間、ソフトウェアはシステムクロックがFIRCクロックかそれ以下であることを必ず確認しなければなりません。より高いクロック速度を使用するには、ソフトウェアがLMEN=1に設定されなければなりません。" Q1の回答を提供いたします。そしてQ2。内部チームから確認が来次第、 よろしくお願いします、 ジュリアン Re: LMBCTLEN, LMAUTOEN, LMEN, LMSTAT Relation こんにちは、 @Julián_AragónM さん、 問題ありません、よろしくお願いします。 BR/くまモン。
View full article
BFU910F model A SPICE compatible Gummel-Poon device model was promised 11 years ago in the datasheet. Only a Mextram model, in a proprietary format, is provided. LTspice claims Mextram 504 model compatibility, so what gives?  RF Re: BFU910F model I'm aware, but no replacement exists, despite a NXP article from 2021 calling it "the Future of High-End RF". In any case, it's a fairly impressive part judging by the datasheet. I'd like to see it documented more thoroughly before the remaining stock runs out :3 Re: BFU910F model Hello Please note that the BFU910F is no longer manufactured.
View full article
designer studio download All links to Designer Studio download the debugger install file only.  Re: designer studio download Hello, Thank you for reporting this. The S32 Design Studio IDE download is available from the S32 Design Studio for S32 Platform page. Under Downloads, please select S32 Design Studio – Windows/Linux. Please make sure not to select the separate S32 Design Studio Debugger download, which provides only the debugger installer. Sign-in may be required to access the download. Best regards, Peter
View full article
ペリフェラル Toolでのedma4エラーメッセージがSD 26 09 00以降に発生しています 皆様、 SDK 26.06.00以降、ペリフェラル Toolを使ってDMA周辺機器を追加しており、完璧に動作し、今も問題ありません。しかし、SDK 26.09.00以降はペリフェラル Toolでエラーメッセージが表示されます: 問題点:EDMAドライバはツールチェーン/IDEsプロジェクトに存在しません。プロジェクトはコンパイルできません! レベル:誤差 タイプ:検証 ツール:ツールチェーン/IDEプロジェクト 起源:ペリフェラル 対象:ツールチェーン/IDEプロジェクト:cm33_core0 リソース: platform.drivers.edma4 私はEDMAコンポーネントを直接使用していません。私はlpspi_edmaコンポーネントを使用していますが、私の記憶が正しければ、これにはedmaコンポーネントも含まれています。 私の主な質問は、lpspi_edma 2.1.4 を使用することです。SPI設定でDMAを実装するのは最新の方法でしょうか(私のSDKウィザードでは2.10.14がEDMAとして、バージョン2.10.13も同様です)?確かに、プロジェクトは問題なくコンパイルされ、実行されます。 私の.mex言う: Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</FEATURE><LINGO-BODY id="lingo-body-2421543" slang="en-US" mode="CREATE"></LINGO-BODY></P><P>親愛なるセレステへ、</P><P>はい、MCXN947を使用しています。</P></DIV></DIV></LINGO-BODY><LINGO-SUB id="lingo-sub-2421536" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</LINGO-SUB><LINGO-BODY id="lingo-body-2421536" slang="en-US" mode="CREATE"><P>こんにちは、 <A href="<A href="<A href="<A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A>" target="_blank"><A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A></A>" target="_blank"><A href="<A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A>" target="_blank"><A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A></A></A>" target="_blank">@PAChristiaans さん</A>、</P> <P>投稿ありがとうございます。</P> <P>質問に答える前に、MCXN947を使っているかどうか確認していただけますか?</P> <P>BR</P> <P>セレステ</P></LINGO-BODY><lingo-sub id="lingo-sub-2422493" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</FEATURE><LINGO-BODY id="lingo-body-2422493" slang="en-US" mode="CREATE"></LINGO-BODY></P><P>こんにちは、 <A href="<A href="<A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A>" target="_blank"><A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A></A>" target="_blank">@PAChristiaans さん</A>、</P> <P>ご辛抱いただきありがとうございます。こちら側でいくつかテストを行ったところ、同様の問題を再現することができました。</P> <P>テストによると、SDKに提供されているドライバーバージョンは正しいです。この問題は、設定ツールペリフェラルツールのeDMAコンポーネント検証に関連しているようです。この件は、さらなる調査のために設定ツールチームにエスカレーションします。</P> <P>最新情報があれば随時お知らせします。</P> <P>BR</P> <P>セレステ</P></DIV></DIV></LINGO-BODY><lingo-sub id="lingo-sub-2423302" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</FEATURE><LINGO-BODY id="lingo-body-2423302" slang="en-US" mode="CREATE"></LINGO-BODY></P><P>こんにちは、 <A href="<A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260452" target="_blank">https://community.nxp.com/t5/user/viewprofilepage/user-id/260452</A>" target="_blank">@PAChristiaans さん</A>、</P> <P>理由が分かった。新しいSDK 26.09にはplatform.drivers.edma4ドライバが含まれていません。これは、ソフトウェアチームがコンポーネント名を <STRONG>platform.drivers.edma_unified</STRONG>に変更したためです。MCXN947はedma4ドライバが搭載されている古いSDKsでサポートされていたため、古いSDKsとの後方互換性があるため、すべてのオプションを提供しています。プロジェクトに使っているドライバを正確に選ぶべきです。</P> <P>下の画像をご覧ください。</P> <P><SPAN class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1792751388672.png" style="width: 400px;"><span class="lia-inline-image-display-wrapper" image-alt="Celeste_Liu_0-1792751388672.png" style="width: 400px;"><img src="<A href="https://community.nxp.com/t5/image/serverpage/image-id/398421iB582FD0BF6C76349/image-size/medium?v=v2&px=400" target="_blank">https://community.nxp.com/t5/image/serverpage/image-id/398421iB582FD0BF6C76349/image-size/medium?v=v2&px=400</A>" role="button" title="Celeste_Liu_0-1792751388672.png" alt="Celeste_Liu_0-1792751388672.png" /></span></SPAN></P> <BR /> <P>ツールチェーンプロジェクトのフィルターを選択すると、正しいドライバのみが提示されます:</P> <P><SPAN class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_1-1792751421202.png" style="width: 400px;"><span class="lia-inline-image-display-wrapper" image-alt="Celeste_Liu_1-1792751421202.png" style="width: 400px;"><img src="<A href="https://community.nxp.com/t5/image/serverpage/image-id/398422i03C5C91ED1058759/image-size/medium?v=v2&px=400" target="_blank">https://community.nxp.com/t5/image/serverpage/image-id/398422i03C5C91ED1058759/image-size/medium?v=v2&px=400</A>" role="button" title="Celeste_Liu_1-1792751421202.png" alt="Celeste_Liu_1-1792751421202.png" /></span></SPAN></P> <P>お役に立てば幸いです。</P> <P>BR</P> <P>セレステ</P></DIV></DIV></LINGO-BODY><lingo-sub id="lingo-sub-2423396" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool</FEATURE><LINGO-BODY id="lingo-body-2423396" slang="en-US" mode="CREATE"></LINGO-BODY></P><P>こんにちは、セレステさん。</P><P>ご回答いただき、誠にありがとうございます。<BR />私はMCUXpresso 25.6とSDK 26 09 00 FRDM MCXN947を使っていますが、クライアント上では少し見た目が異なります。<BR />実際のfsl_edma.cを見てみるとドライバーファイルは正しいと思いますが、なぜかUIが違って見えます。<BR />繰り返しますが、プロジェクトのコンパイル自体には問題は発生していませんが、エラーメッセージが表示されます。安全に無視してもいいのでしょうか?</P><P>敬具</P></DIV></DIV></LINGO-BODY><lingo-sub id="lingo-sub-2423678" slang="en-US" mode="CREATE" translate="no">Re: edma4 error message since SDK 26 09 00 in Peripherals Tool こんにちは、 @PAChristiaans さん、 はい。スクリーンショットを見る限り、これはエラーではなく警告のようなので無視しても大丈夫です。 UIの違いについては、統合されているMCUXpresso Config Toolsのバージョンが異なることが原因である可能性があります。私はバージョン26.09を使用しています。 アップデートについては、MCUXpresso IDEリンク内の「設定ツールの更新 」を参照してください。もちろん、現在のバージョンが問題なく動作しているなら、更新しなくても使い続けることもできます。 お役に立てば幸いです。 BR セレステ
View full article
设计师工作室下载 所有指向 Designer Studio 的链接都仅下载调试器安装文件。 Re: designer studio download 你好, 感谢您的举报。可从S32 Design Studio for S32 Platform 页面下载 S32 Design Studio IDE。在“下载”下,请选择“S32 Design Studio – Windows/Linux”。请确保不要选择单独的 S32 Design Studio 调试器下载,该下载仅提供调试器安装程序。可能需要登录才能下载。 顺祝商祺! Peter
View full article
LMBCTLEN, LMAUTOEN, LMEN, LMSTAT Relation Hello NXP Support, - Is there any conflict if we enable LMAUTOEN, LMEN at the same time as in the following figure? - What is suggested configuration? Manual mode (via LMEN) or automatic mode (via LMAUTOEN)? - In which scenario, we have to use manual mode since there is already automatic mode? Thanks. BR/Kumamon Re: LMBCTLEN, LMAUTOEN, LMEN, LMSTAT Relation Hello @kumamon, 1. No conflict, actually, you can find a relevant note inside the Power Management chapter from the S32K3XX Reference Manual: 2. & 3. Automatic last mile auto-enable feature allows you to use the last-mile regulator (instead of the boot regulator) during chip startup and standby mode recovery. In "manual mode", LMEN must be enabled before PLL is enabled. After Standby mode exit, you must re-enable the PMC last-mile regulator before transitioning to faster clock frequencies.  You can refer to Figure 180. Last-mile regulator enable sequence: Regarding LMBCTLEN, it must be set to 1 if external BJT between VDD_HV_A and V15 is used on the PCB. For example, in S32K3X4EVB, if you want to use the NPN, set LMBCTLEN = 1. Best regards, Julián Re: LMBCTLEN, LMAUTOEN, LMEN, LMSTAT Relation Hello @Julián_AragónM , Thanks a lot for your reply. You must write 1 to PMC.CONFIG[LM_EN] field before transtioning to faster clock frequencies irrespective of the setting of PMC.CONFIG[LMAUTOEN] field. This is because of the reduced clock speed when using the boot regulator. 1. What is the reason behind the above statement you mentioned, because I think automatic mode can do it by chip itself, why still need software to interfere in this case? And is the following understanding correct?  Only automatic mode: not ok.  Only manual mode: ok.  Manual mode + automatic mode: ok. 2.  It looks like "Manual mode + automatic mode" is always better than "Only manual mode"? In which scenario, automatic mode is not expected? Is it the scenario where we just strictly want to use boot regulator in chip startup time (for example)? 3. In legacy project, we even did not turn on last mile regulator when we use higher clock (160 MHz) than FIRC. We now know it violates the statement in RM. And we are estimating the risk, do you know what will be worst result here? Thanks. BR/Kumamon Re: LMBCTLEN, LMAUTOEN, LMEN, LMSTAT Relation Hello @kumamon, Let me confirm the behavior with the internal team, in order to provide a consolidated answer regarding LMAUTOEN + LMEN functionality. Regarding question 3: If PLL is enabled but the last-mile regulator is not enabled, the chip will be powered by the boot regulator. Under PLL clock, the core demands a large current and heat will accumulate on the boot regulator. This will overheat the chip until it is damaged. Following the reference manual is mandatory: "As long as LMEN=0 software must make sure that the system clock is on FIRC clock or slower. To use higher clock speed software must set LMEN=1." I will provide a response for Q1. & Q2. as soon as I get confirmation from the internal team. Best regards, Julián Re: LMBCTLEN, LMAUTOEN, LMEN, LMSTAT Relation Hello @Julián_AragónM , No problem, thanks in advance. BR/Kumamon.
View full article
オフラインMISR値計算 現在、S32K312コントローラー用のFlash Array Integrity実装に取り組んでいます。 リファレンス・マニュアルによると、MISR値は下の画像に示された特定の多項式で計算されます。しかし、オフラインで計算したMISR値は、複数回試してもユーザーモード(UM)レジスタで生成される値と一致しません。 さらに詳しく調べたところ、MISRの計算はECC検出後に行われ、ECCパリティはオフラインでは計算できないことが分かりました。 この実装における標準的な本環境レベルのアプローチについてアドバイスいただけますか?具体的には、以下の点を知りたいです: 1. オフラインで期待されるMISR値を計算し、それをFlashやNVMに保存することは可能ですか? 2. それとも、UMレジスタから直接計算されたMISR値を取得し、FUTUREのチェックのために保存するためにコードを一度実行する必要があるのでしょうか? 本番環境に対応できるソリューションを実現するための推奨戦略についてご指導ください。 よろしくお願いします、 サンディープ・シン Re: Offline MISR value calculation こんにちは、ダニエルさん。 過去7~8ヶ月間、ずっと同じ回答を受け取っています。以前にもこの件について問い合わせましたが、その時の回答も今回と全く同じでした。NXPの営業担当者にも確認しましたが、未だに解決策は見つかっていません。 この機能がNXPによってテストされたのか、またこの問題に対する有効な修正や回避策があるのか、教えていただけますか? 迅速なご回答をお待ちしております。 よろしくお願いします、 サンディープ・シン Re: Offline MISR value calculation こんにちは、@sandeepSingh18606 さん。 1. オフライン計算の進捗状況について、社内で確認してみます。 できるだけ早くご連絡いたします。 2. これは選択肢の一つです。以下に例を示します。https: //community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FLS-Integrity-Margin-Check-v1-0-S32DS36-RTD701/ta-p/2416160 BR、ダニエル
View full article
The version of the IPCF software package corresponding to the RTD package of S32G2 could not be foun When I was developing the multi-core communication for the S32G2, I found that I couldn't locate the version of the IPCF software package corresponding to the RTD package of the S32G2. The version of the M core RTD package of my S32G2 is SW32G_RTD_4.4_4.0.2_HF02. Could you provide me with the website address of the corresponding IPCF package version? Thank you. Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be This website refused my download due to export control. Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be Hi, Please try to this link:  Automotive Software Package Manager | NXP Semiconductors , and download it from GoldVIP SW package. BR Joey Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be Thank you for your reply. However, when I opened the download website of IPCF, I found that I couldn't access the "Previous" option. Moreover, I couldn't download anything within the vehicle software management tool. Could you please tell me how to solve this problem? Can I use IPCF 4.9.0 as a substitute? Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be Hi,qrsljx Thank you for contacting us. Refer to the GoldVIP-S32G3-1.12.0, you can use the IPCF version of 4.10.0 with the RTD 4.0.2 HF02. You can try to download the relevant Goldvip SW package by this link: Automotive Software Package Manager | NXP Semiconductors Or separately download the IPCF 4.10.0. BR Joey Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be Hi,qrsljx 1. Please log in to the website using your company's email and try to download. 2. Check if your colleague can download this software using their account. It might be an issue with the permissions of your account. BR Joey
View full article
找不到与S32G2的RTD软件包对应的IPCF软件包版本。 在为 S32G2 开发多核通信时,我发现找不到与 S32G2 的 RTD 软件包对应的 IPCF 软件包版本。我的 S32G2 的 M 核心 RTD 软件包版本为 SW32G_RTD_4.4_4.0.2_HF02。请问能否提供对应 IPCF 软件包版本的网站地址?谢谢。 Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be 由于出口管制,该网站拒绝了我的下载请求。 Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be 您好, 请尝试点击此链接: 汽车软件软件包管理器 | 恩智浦半导体 并从 GoldVIP 软件套装中下载。 BR 乔伊 Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be 感谢你的回复。但是,当我打开 IPCF 的下载网站时,我发现我无法访问“上一页”选项。此外,我无法在车辆软件管理工具中下载任何内容。请问如何解决这个问题?我可以使用 IPCF 4.9.0 作为替代方案吗? Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be 你好, qrsljx 感谢您与我们联系。 请参考 GoldVIP- S32G3-1.12.0 ,您可以将 IPCF 版本 4.10.0 与 RTD 4.0.2 配合使用。HF02。 您可以尝试通过此链接下载相关的 Goldvip 软件软件包: 汽车软件软件包管理器 | 恩智浦半导体 或者单独下载 IPCF 4.10.0。 BR 乔伊 Re: The version of the IPCF software package corresponding to the RTD package of S32G2 could not be 你好, qrsljx 1. 请使用贵公司邮箱登录网站并尝试下载。 2. 检查你的同事是否可以使用他们的帐户下载此软件。这可能是您的账户权限问题。 BR 乔伊
View full article
edma4 error message since SDK 26 09 00 in Peripherals Tool Dear all, I have used the Peripherals Tool to add a DMA peripheral since SDK 26.06.00 which worked perfect and it still does, but since SDK 26.09.00 I get an error message in the Peripherals Tool: Issue: EDMA Driver is not found in the toolchain/IDE project. The project will not compile! Level: Error Type: Validation Tool: Toolchain/IDE project Origin: Peripherals Target: Toolchain/IDE project: cm33_core0 Resource: platform.drivers.edma4 I'm not using the edma component directly. I use the lpspi_edma component, but if I'm not amiss it includes the edma component. My main question is whether using lpspi_edma 2.1.4 is the up-to-date way to implement DMA in an SPI setting (my SDK wizard lists 2.10.14 as edma, as well as version 2.10.13)? To be sure: the project compiles and runs without problems. My .mex says: 2.9.0 My eDMA driver version is: #define FSL_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 10, 14)) /*!< Version 2.10.14. */ Re: edma4 error message since SDK 26 09 00 in Peripherals Tool Dear Celeste, Yes, I'm using the MCXN947. Re: edma4 error message since SDK 26 09 00 in Peripherals Tool Hello @PAChristiaans , Thanks for your post. Before I look into your questions, could you please confirm whether you are using the MCXN947? BR Celeste Re: edma4 error message since SDK 26 09 00 in Peripherals Tool Hello @PAChristiaans , Thank you for your patience. I performed some tests on my side and was able to reproduce the issue. Based on my testing, the driver version provided in the SDK is correct. The issue appears to be related to the eDMA component validation in the Config Tools Peripherals Tool. I will escalate this to the Config Tools team for further investigation. I’ll keep you informed of any updates. BR Celeste Re: edma4 error message since SDK 26 09 00 in Peripherals Tool Hello @PAChristiaans , I found the reason. The new SDK 26.09 does not include the platform.drivers.edma4 driver because the SW team decided to rename the component to platform.drivers.edma_unified. Since MCXN947 was supported by older SDKs where the edma4 driver was present the tool offers all options due to backward compatibility with older SDKs. You should choose the exact driver that you have present in your project. Please see the picture below: After selecting a filter to a toolchain project you are offered only the correct driver: Hope it helps. BR Celeste Re: edma4 error message since SDK 26 09 00 in Peripherals Tool Hello Celeste, Thank you very much for your response. I use MCUXpresso 25.6 and SDK 26 09 00 FRDM MCXN947, but it looks slightly different on my client. If I look at my actual fsl_edma.c driver file, I assume I have the correct version, but for some reason the UI looks different. Again, I'm not experiencing any problems compiling my projects, but I do get the error messages. Can I safely ignore them? Kind regards Re: edma4 error message since SDK 26 09 00 in Peripherals Tool Hello @PAChristiaans , Yes. Based on your screenshot, this seems to be a warning rather than an error, so you can ignore it. As for the UI difference, it may be caused by different versions of the integrated MCUXpresso Config Tools. I am using version 26.09. You can refer to the Updating Config Tools in the MCUXpresso IDE link for the update. Of course, if your current version works fine, you can also keep using it without updating. Hope it helps。 BR Celeste
View full article
自 SDK 26 09 00 起,外围设备工具中出现 edma4 错误消息 尊敬的各位, 从 SDK 26.06.00 版本开始,我一直使用外设工具添加 DMA 外设,一直运行良好,现在仍然如此。但是从 SDK 26.09.00 版本开始,我在外设工具中收到错误消息: 问题:工具链/IDE 项目中找不到 EDMA 驱动程序。该项目无法编译! 级别:错误 类型:验证 工具:工具链/IDE 项目 来源:外围设备 目标:工具链/IDE 项目:cm33_core0 资源:platform.drivers.edma4 我没有直接使用 edma 元器件。我使用的是 lpspi_edma 元器件,但如果我没弄错的话,它包含了 edma 元器件。 我的主要问题是使用 lpspi_edma 2.1.4 是否可行在 SPI 环境中实现 DMA 的最新方法是什么?(我的 SDK 向导将 edma 列为 2.10.14 版本,以及 2.10.13 版本)可以肯定的是:该项目编译和运行都没有问题。 我的 .mex他说: 2.9.0 我的eDMA驱动程序版本是: #define FSL_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 10, 14)) /*!< 版本 2.10.14。 */ Re: edma4 error message since SDK 26 09 00 in Peripherals Tool 亲爱的塞莱斯特, 是的,我用的是MCXN947。 Re: edma4 error message since SDK 26 09 00 in Peripherals Tool 你好@PAChristiaans , 感谢您的帖子。 在查看您的问题之前,请您确认一下您是否正在使用 MCXN947? BR 塞莱斯特 Re: edma4 error message since SDK 26 09 00 in Peripherals Tool 你好@PAChristiaans , 感谢您的耐心等待。我这边进行了一些测试,能够重现这个问题。 根据我的测试,SDK中提供的驱动程序版本是正确的。问题似乎与配置工具外围工具中的 eDMA 元器件验证有关。我会将此事上报给配置工具团队进行进一步调查。 如有任何最新进展,我会及时通知您。 BR 塞莱斯特 Re: edma4 error message since SDK 26 09 00 in Peripherals Tool 你好@PAChristiaans , 我找到原因了。新的 SDK 26.09 不包含 platform.drivers.edma4 驱动程序,因为软件团队决定将该元器件重命名为platform.drivers.edma_unified 。由于 MCXN947 受到旧版 SDK 的支持(其中存在 edma4 驱动程序),因此该工具由于后向兼容性旧版 SDK 而提供了所有选项。您应该选择项目中已存在的驱动程序。 请看下图: 选择工具链项目的筛选条件后,系统只会提供正确的驱动程序: 希望对您有所帮助。 BR 塞莱斯特 Re: edma4 error message since SDK 26 09 00 in Peripherals Tool 你好,Celeste, 非常感谢您的回复。 我使用的是 MCUXpresso 25.6 和 SDK 26 09 00 FRDM MCXN947,但在我的客户端上看起来略有不同。 如果我查看我的 fsl_edma.c 文件驱动文件,我假设我的版本是正确的,但不知何故,用户界面看起来不一样。 再次说明,我的项目编译没有出现任何问题,但我确实收到了错误消息。我可以忽略它们吗? 此致敬礼 Re: edma4 error message since SDK 26 09 00 in Peripherals Tool 你好@PAChristiaans , 是的。根据你的截图,这似乎是一个警告而不是错误,所以你可以忽略它。 至于用户界面差异,可能是由于集成的 MCUXpresso 配置工具版本不同造成的。我使用的是 26.09 版本。 您可以参考MCUXpresso IDE 链接中的“更新配置工具”进行更新。当然,如果您的当前版本运行良好,您也可以继续使用它而无需更新。 希望对您有所帮助。 BR 塞莱斯特
View full article
mimxrt1160_evk SDK v26.09 与 J-Link Ultra+ 不兼容 我正在使用NXP 1160开发板。我将 SDK 从 v26.06 升级到 v26.09,现在遇到了 j-link 无法调试代码(单步执行代码等)的问题。该应用程序可以对开发板进行编程,但调试失败(代码似乎在执行 main 函数之前就卡住了)。如果我重启电路板,新编写的代码就能运行。我使用的是 vscode mcuxpresso(不是旧版 Eclipse IDE)。 我尝试过很多方法。 我从 v26.09 SDK 导入了一个新的演示项目(但仍然无效),所以问题似乎不在我的项目中。 基于旧版 Eclipse 的 IDE。从 v26.09 版本导入了一个新应用程序,并且成功了。我能够顺利地单步执行代码。 在另一台计算机上全新安装 vscode mcuxpresso 和 sdk v26.09。无法调试。 回滚到 v26.06 SDK。调试功能恢复正常。 更改跳线以使用板编程器/调试器 CMSIS。这在 v26.09 版本中有效。 还有其他人遇到过类似问题吗?大家有什么想法,可以从哪些方面着手解决这个问题?我希望能够访问 v26.09 版本中的新 BLE edgefast 中间件。谢谢。 Re: mimxrt1160_evk sdk v26.09 not working with j-link ultra+ 谢谢回复。我忘了提及这个重要的细节……我认为“hello world”演示应用程序没有使用QSPI闪存来存储代码。我也成功地让 SDK 26.09 运行了“hello world”演示应用程序。是那些需要编程到 QSPI 闪存的演示应用程序没有正常工作。您可以尝试运行 wifi_cli_cm7 或 wifi_setup_cm7,看看是否会失败(您不需要 wifi 模块 - 只需检查是否到达初始断点即可)?谢谢。 以下是尝试调试 wifi_setup_cm7 演示应用程序时生成的日志: Launching GDB: "C:\\Users\\xxxxxx\\.mcuxpressotools\\arm-gnu-toolchain-14.2.rel1-mingw-w64-x86_64-arm-none-eabi\\bin\\arm-none-eabi-gdb.exe" -q --interpreter=mi2 IMPORTANT: Set "showDevDebugOutput": "raw" in "launch.json" to see all GDB transactions. Launching GDB server: "C:\\Program Files\\SEGGER\\JLink_V980\\JLinkGDBServerCL.exe" -SettingsFile "c:\\Work\\Git-projects\\evkmimxrt1160_wifi_setup_cm7\\flexspi_nor_debug\\JLink_evkmimxrt1160_wifi_setup_cm7_cm7.jlink" -nosilent -singlerun -endian little -noir -speed 4000 -port 2366 -vd -device MIMXRT1166xxx6_M7 -if SWD -reportuseraction -nogui -select usb=504501851 -halt -swoport 2368 -telnetport 2367 -jlinkscriptfile "C:/nxp/mimxrt1160_evk/mcuxsdk/examples/_boards/evkmimxrt1160/evkmimxrt1160_connect_cm4_cm7side.jlinkscript" Please check TERMINAL tab (GDB server console) for output from "C:\Program Files\SEGGER\JLink_V980\JLinkGDBServerCL.exe" Output radix now set to decimal 10, hex a, octal 12. Input radix now set to decimal 10, hex a, octal 12. 0x00223104 in ?? () Program stopped, probably due to a reset and/or halt issued by the debugger. Resetting target Executed SetRestartOnClose=1 Resetting target DEBUG [18]: Enqueuing request {"command":"disassemble","arguments":{"memoryReference":"0x300397E8","instructionCount":4,"resolveSymbols":true},"type":"request","seq":18} NOTE: The following memory regions were detected by using GDB command "info mem" and by invoking "objdump -h". This information is used to adjust bounds only when normal disassembly fails. ================================================================================ Using the following memory regions for disassembly: ================================================================================ Size VMA Start VMA End LMA Start LMA End Attributes ================================================================================ No memory information from GDB (or GDB server). ------------------------------------------------------------------------------ 00000200 30000400 30000600 -------- -------- (.flash_config) contents alloc load readonly data 00000030 30001000 30001030 -------- -------- (.ivt) contents alloc load readonly data 00000400 30002000 30002400 -------- -------- (.interrupts) contents alloc load readonly data 000ac1e0 30002400 300ae5e0 -------- -------- (.text) contents alloc load readonly code 000000a0 300ae5e0 300ae680 -------- -------- (.text.memcpy) contents alloc load readonly code 00000008 300ae680 300ae688 -------- -------- (.ARM) contents alloc load readonly data 00000004 300ae688 300ae68c -------- -------- (.init_array) contents alloc load data 00000004 300ae68c 300ae690 -------- -------- (.fini_array) contents alloc load data 00000cbc 20000000 20000cbc 300ae690 300af34c (.data) contents alloc load data 00019680 00000000 00019680 300af34c 300c89cc (.ram_function) contents alloc load readonly code 00000084 20000cbc 20000d40 300af34c 300af3d0 (.ncache) alloc 00025878 20000d40 200265b8 300af3e0 300d4c58 (.bss) alloc 0000f963 202c0000 202cf963 -------- -------- (.wlan_data) contents alloc load data 00000400 200265b8 200269b8 300d4c58 300d5058 (.heap) alloc 00000400 200269b8 20026db8 300d5058 300d5458 (.stack) alloc ================================================================================ DEBUG [18]: Dequeuing DEBUG: Executing "-data-disassemble -s 0x300397e8 -e 0x3003983c -- 5 84 bytes (__errno)" DEBUG: "data-disassemble -s 0x300397e8 -e 0x3003983c -- 5" => found $39 instructions. With source code: 0, without source code: 39. DEBUG: [18]: Elapsed time for disassembly request: 015 ms warning: could not convert 'main' from the host encoding (CP1252) to UTF-32. Re: mimxrt1160_evk sdk v26.09 not working with j-link ultra+ 亲爱的@houe , 我已确认 SDK 26.09 中的默认 wifi_setup_cm7 示例在我这边也存在同样的调试问题。 可以通过从 mcuxsdk\examples\wifi_examples\wifi_setup\flexspi_nor_debug\runners.yaml 中删除以下行来解决此问题: - --tool-opt=-jlinkscriptfile C:/2609/mcuxsdk/mcuxsdk/examples/_boards/evkmimxrt1160/evkmimxrt1160_connect_cm4_cm7side.jlinkscript 移除此选项后,我可以正常调试示例:   作为对比,SDK 26.06 wifi_setup_cm7 示例的 runners.yaml 不包含此行: 请试一试。 顺祝商祺! 雪莉 Re: mimxrt1160_evk sdk v26.09 not working with j-link ultra+ 感谢你彻底查清此事!非常感谢!
View full article
[BUG] 模块名称冲突:wave511 下游驱动程序和 wave5 上游驱动程序冲突 你好, lf-6.18.20-2.0.0 内核 (6.18.y) 中的 NXP Wave511 VPU 驱动程序构建了一个与主线 Chips&Media Wave5 驱动程序同名的模块。任何同时启用这两个功能的配置,例如allmodconfig或allyesconfig ,都会导致版本失败。 细节: - 上游驱动程序(自 v6.8 起已合并到主线): drivers/media/platform/chips-media/wave5/    obj-$(CONFIG_VIDEO_WAVE_VPU) += wave5.o - NXP驱动程序: drivers/mxc/vpu/wave511/    obj-$(CONFIG_MXC_VIDEO_WAVE511) += wave5.o    obj-$(CONFIG_MXC_VIDEO_WAVE511_CTRL) += wave5-ctrl.o 这两个 Kconfig 符号是独立的,因此可以同时启用这两个模块。Kbuild 随后停止运行: error: the following would cause module name conflict: drivers/media/platform/chips-media/wave5/wave5.ko drivers/mxc/vpu/wave511/wave5.ko 即使没有触发检查, modules_install也会用一个 wave5.ko 文件覆盖另一个wave5.ko文件。 驱动程序绑定了不同的兼容模块( ti,j721s2-wave521c和nxp,wave511-vpu ),因此只有模块名称冲突。 重现步骤: make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- allmodconfig make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- -j$(nproc) modules 这个问题能否在即将发布的 Linux IMX 版本中得到解决? 感谢您提前给予的支持。 马修斯·巴博萨 Toradex i.MX 8 系列 | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano i.MX6 全部 Linux Re: [BUG] Module name conflict: wave511 downstream driver and upstream wave5 你好, 我正在 Toradex 电路板支持包。中添加 Wave511 驱动程序以支持 i.MX952,尽管所使用的处理器与下游内核中报告的错误无关。 我们为所有受电路板支持包。支持的 ARM64 SoC 构建了一个共享配置的内核,它是一个超集,可以启用许多模块。其中包括 CONFIG_VIDEO_WAVE_VPU。 这是主线内核中存在的驱动程序,它会安装“wave5.ko”。到模块目录。 我找到了一个变通方法。 由于无法在该通用配置中启用 WAVE511 驱动程序,因此我只对 i.MX SoC 执行了此操作,并禁用了它们的 CONFIG_VIDEO_WAVE_VPU。 我已经禁用了 OE 层中 i.MX 处理器的 CONFIG_VIDEO_WAVE_VPU,以便暂时启用 CONFIG_MXC_VIDEO_WAVE511 模块。 预期allmodconfig能够顺利构建,但当前的下游驱动程序破坏了这一点。这就是我举报它的原因。 Re: [BUG] Module name conflict: wave511 downstream driver and upstream wave5 你好, 此前未曾报告过此问题,目前也暂无解决方案计划。 你使用的是哪款处理器? 你试过禁用某个 Kconfig 选项或者在本地重命名模块吗? 顺祝商祺! Re: [BUG] Module name conflict: wave511 downstream driver and upstream wave5 你好, 谢谢你提供的详细信息,我已经将此事汇报给了内部团队。 我会尽快向您汇报我们这边的后续行动。 顺祝商祺! Re: [BUG] Module name conflict: wave511 downstream driver and upstream wave5 你好, 请查看内部团队的最新消息: 我在 lf-6.18.20-2.0.0 (nxp-imx/linux-imx) 的全新检出版本上重现了此问题,并确认根本原因与工单中的描述完全一致: 上游驱动程序/媒体/平台/芯片媒体/wave5/Makefile:obj-$(CONFIG_VIDEO_WAVE_VPU) += wave5.o NXP drivers/mxc/vpu/wave511/Makefile: obj-$(CONFIG_MXC_VIDEO_WAVE511) += wave5.o 这两个 Kconfig 符号是独立的,因此 allmodconfig/allyesconfig 会同时选择它们,导致 scripts/modules-check.sh 因报告的错误而中止。我通过向脚本提供包含两个真实模块路径的 modules.order 来重现完全相同的错误文本——与工单中引用的内容字节完全相同。还检查了较新的 lf-6.18.37-2.1.0 版本。标签:碰撞仍然存在。 建议的解决方法:将 drivers/mxc/vpu/wave511/Makefile 中 NXP 模块的构建目标从 wave5.o/wave5-ctrl.o 重命名为 wave511.o/wave511-ctrl.o。源文件名保持不变——这只是一个 Makefile 文件的更改,对驱动程序的功能/行为没有任何影响。我已验证它可以顺利构建,并且此更改生效后,scripts/modules-check.sh 不再标记冲突。 我考虑过另一种方案,即在 NXP Kconfig 中添加对 !VIDEO_WAVE_VPU 的依赖,但模块重命名是更持久的长期解决方案:它解决了实际的命名冲突,而不是依赖互斥(互斥会在 allmodconfig/allyesconfig 下悄悄删除一个驱动程序,并可能掩盖真正的版本问题),而且即使未来的板合并了这两个 IP 模块,它仍然是正确的。 仅下游影响:任何对 NXP Wave511 驱动程序硬编码 modprobe wave5 / wave5.ko 的内容(例如 yocto 配方或 rootfs 模块加载配置)都需要改用引用 wave511.ko。我在内核树中没有找到任何此类引用。 补丁将内部提供审核。 顺祝商祺!
View full article
mimxrt1160_evk sdk v26.09 not working with j-link ultra+ I am working with the NXP 1160 development board. I upgraded from sdk v26.06 to v26.09 and am now having difficulty getting j-link to be able to debug code (step through code etc.). The application does program the dev board, but debugging fails (code seems to lock up prior to hitting main). If I power cycle the board the newly programmed code does run. I am using vscode mcuxpresso (not legacy eclipse ide). I have tried a number of things. imported a new demo project from the v26.09 sdk (did not work either) so problem doesn't seem to be in my project. legacy eclipse based ide. Imported a new application from v26.09 and this did work. I was able to step through code fine. clean install of vscode mcuxpresso and sdk v26.09 on a separate computer. Was not able to debug. Revert to v26.06 sdk. Debugging works again. changed jumpers to use on board programmer/debugger CMSIS. This worked with v26.09. Has anyone else had similar issues? Any thoughts where to look to resolve this? I would like to gain access to the new BLE edgefast middleware in this v26.09 release. Thanks. Re: mimxrt1160_evk sdk v26.09 not working with j-link ultra+ Thanks for the reply. I forgot to mention this important detail... I think the "hello world" demo application does not use QSPI flash for code. I too have been able to get the "hello world" demo app to work from SDK 26.09. It is the demo applications that program to QSPI flash that haven't worked. Could you try wifi_cli_cm7 or wifi_setup_cm7 and see if that fails (you don't need a wifi module - just check if you hit the initial break point)? Thanks. Below are the logs from trying to debug the wifi_setup_cm7 demo application: Launching GDB: "C:\\Users\\xxxxxx\\.mcuxpressotools\\arm-gnu-toolchain-14.2.rel1-mingw-w64-x86_64-arm-none-eabi\\bin\\arm-none-eabi-gdb.exe" -q --interpreter=mi2 IMPORTANT: Set "showDevDebugOutput": "raw" in "launch.json" to see all GDB transactions. Launching GDB server: "C:\\Program Files\\SEGGER\\JLink_V980\\JLinkGDBServerCL.exe" -SettingsFile "c:\\Work\\Git-projects\\evkmimxrt1160_wifi_setup_cm7\\flexspi_nor_debug\\JLink_evkmimxrt1160_wifi_setup_cm7_cm7.jlink" -nosilent -singlerun -endian little -noir -speed 4000 -port 2366 -vd -device MIMXRT1166xxx6_M7 -if SWD -reportuseraction -nogui -select usb=504501851 -halt -swoport 2368 -telnetport 2367 -jlinkscriptfile "C:/nxp/mimxrt1160_evk/mcuxsdk/examples/_boards/evkmimxrt1160/evkmimxrt1160_connect_cm4_cm7side.jlinkscript" Please check TERMINAL tab (GDB server console) for output from "C:\Program Files\SEGGER\JLink_V980\JLinkGDBServerCL.exe" Output radix now set to decimal 10, hex a, octal 12. Input radix now set to decimal 10, hex a, octal 12. 0x00223104 in ?? () Program stopped, probably due to a reset and/or halt issued by the debugger. Resetting target Executed SetRestartOnClose=1 Resetting target DEBUG [18]: Enqueuing request {"command":"disassemble","arguments":{"memoryReference":"0x300397E8","instructionCount":4,"resolveSymbols":true},"type":"request","seq":18} NOTE: The following memory regions were detected by using GDB command "info mem" and by invoking "objdump -h". This information is used to adjust bounds only when normal disassembly fails. ================================================================================ Using the following memory regions for disassembly: ================================================================================ Size VMA Start VMA End LMA Start LMA End Attributes ================================================================================ No memory information from GDB (or GDB server). ------------------------------------------------------------------------------ 00000200 30000400 30000600 -------- -------- (.flash_config) contents alloc load readonly data 00000030 30001000 30001030 -------- -------- (.ivt) contents alloc load readonly data 00000400 30002000 30002400 -------- -------- (.interrupts) contents alloc load readonly data 000ac1e0 30002400 300ae5e0 -------- -------- (.text) contents alloc load readonly code 000000a0 300ae5e0 300ae680 -------- -------- (.text.memcpy) contents alloc load readonly code 00000008 300ae680 300ae688 -------- -------- (.ARM) contents alloc load readonly data 00000004 300ae688 300ae68c -------- -------- (.init_array) contents alloc load data 00000004 300ae68c 300ae690 -------- -------- (.fini_array) contents alloc load data 00000cbc 20000000 20000cbc 300ae690 300af34c (.data) contents alloc load data 00019680 00000000 00019680 300af34c 300c89cc (.ram_function) contents alloc load readonly code 00000084 20000cbc 20000d40 300af34c 300af3d0 (.ncache) alloc 00025878 20000d40 200265b8 300af3e0 300d4c58 (.bss) alloc 0000f963 202c0000 202cf963 -------- -------- (.wlan_data) contents alloc load data 00000400 200265b8 200269b8 300d4c58 300d5058 (.heap) alloc 00000400 200269b8 20026db8 300d5058 300d5458 (.stack) alloc ================================================================================ DEBUG [18]: Dequeuing DEBUG: Executing "-data-disassemble -s 0x300397e8 -e 0x3003983c -- 5 84 bytes (__errno)" DEBUG: "data-disassemble -s 0x300397e8 -e 0x3003983c -- 5" => found $39 instructions. With source code: 0, without source code: 39. DEBUG: [18]: Elapsed time for disassembly request: 015 ms warning: could not convert 'main' from the host encoding (CP1252) to UTF-32. Re: mimxrt1160_evk sdk v26.09 not working with j-link ultra+ Dear @houe , I confirmed that the default wifi_setup_cm7 example in SDK 26.09 has the same debug issue on my side. The issue can be worked around by removing the following line from mcuxsdk\examples\wifi_examples\wifi_setup\flexspi_nor_debug\runners.yaml : - --tool-opt=-jlinkscriptfile C:/2609/mcuxsdk/mcuxsdk/examples/_boards/evkmimxrt1160/evkmimxrt1160_connect_cm4_cm7side.jlinkscript After removing this option, I can debug the example normally:   For comparison, the runners.yaml for the SDK 26.06 wifi_setup_cm7 example does not include this line:  Please try it. Best Regards, Shelly Re: mimxrt1160_evk sdk v26.09 not working with j-link ultra+ Thanks for getting to the bottom of this! Much appreciated!
View full article
[バグ]モジュール名の競合:wave511下りドライバーと上流wave5 こんにちは、 NXP Wave511 VPUドライバーは、lf-6.18.20-2.0.0カーネル(6.18.y)に搭載されており、メインラインのChips&Media Wave5ドライバーと同じ名前のモジュールを構築します。allmodconfigやallyesconfigなど、両方を有効にする設定では、ビルドが失敗します。 詳細: - アップストリームドライバー(v6.8以降メインライン): drivers/media/platform/chips-media/wave5/    obj-$(CONFIG_VIDEO_WAVE_VPU) += wave5.o - NXPドライバ: drivers/mxc/vpu/wave511/    obj-$(CONFIG_MXC_VIDEO_WAVE511) += wave5.o    obj-$(CONFIG_MXC_VIDEO_WAVE511_CTRL) += wave5-ctrl.o 2つのKconfigシンボルは独立しているため、両方のモジュールを同時に有効化できます。Kbuild はそこで停止します: error: the following would cause module name conflict: drivers/media/platform/chips-media/wave5/wave5.ko drivers/mxc/vpu/wave511/wave5.ko チェックに引っかからなかった場合でも、 modules_install は一方のwave5.koをもう一方の wave5.ko で上書きします。 ドライバは異なる互換性(ti,j721s2-wave521c 、 nxp,wave511-vpu)を割り当てているため、モジュール名だけが衝突します。 再現手順: make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- allmodconfig make ARCH=arm64 CROSS_COMPILE=aarch64-linux-gnu- -j$(nproc) modules 今後のLinux IMXリリースで修正できるのでしょうか? ごサポートにあらかじめ感謝いたします。 マテウス・バルボサ Toradex i.MX 8ファミリ | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano i.MX6 全て Linux Re: [BUG] Module name conflict: wave511 downstream driver and upstream wave5 こんにちは、 私はWave511ドライバを追加して、Toradex BSPでi.MX952をサポートするつもりですが、使用中のプロセッサは下流カーネルで報告されたバグには関係ありません。 弊社では、BSPでサポートされているすべてのARM64 SoC向けに共有設定を使用してカーネルを構築しています。これは多くのモジュールを有効にするスーパーセットです。これにはCONFIG_VIDEO_WAVE_VPUが含まれます。 これはメインラインに存在し、「wave5.ko」をインストールするカーネルドライバーです。モジュールディレクトリへ移動します。 回避策を作成しました 一般的な設定ではWAVE511ドライバーを有効にすることができないので、i.MX SoCに対してだけ有効にし、それらのCONFIG_VIDEO_WAVE_VPUも無効にしました。 i.MX プロセッサのOE層でCONFIG_VIDEO_WAVE_VPUを無効にし、CONFIG_MXC_VIDEO_WAVE511をモジュールとして有効化できるようにしています。 allmodconfigはクリーンにビルドすることが期待されますが、現在の下流ドライバーがこれを壊しています。それが私がこの件を報告する理由です。 Re: [BUG] Module name conflict: wave511 downstream driver and upstream wave5 こんにちは、 この問題はこれまで報告されておらず、現時点では解決策を実施する予定もありません。 どのプロセッサを使っていますか? Kconfigのオプションを1つ無効にしたり、モジュールの名前をローカルで変更したりしてみましたか? よろしくお願いいたします。 Re: [BUG] Module name conflict: wave511 downstream driver and upstream wave5 こんにちは、 詳細情報ありがとうございます。社内チームに報告しました。 弊社側の今後の対応については、できるだけ早くご報告いたします。 よろしくお願いいたします。 Re: [BUG] Module name conflict: wave511 downstream driver and upstream wave5 こんにちは、 社内チームからの最新情報をご確認ください。 これをlf-6.18.20-2.0.0(nxp-imx/linux-imx)のクリーンチェックアウトで再現し、根本原因がチケットと完全に一致していることを確認しました: Upstream ドライバ/プレスリリース、製品ニュース/プラットフォーム/chips-media/wave5/Makefile: obj-$(CONFIG_VIDEO_WAVE_VPU) += wave5.o NXP ドライバ/mxc/vpu/wave511/Makefile: obj-$(CONFIG_MXC_VIDEO_WAVE511) += wave5.o 両方のKconfigシンボルは独立しているため、allmodconfig/allyesconfigは両方を選択し、scripts/modules-check.sh は報告されたエラーで中止します。チケットに記載されているものとバイト単位で同一の、2つの実際のモジュールパスを含む modules.order をスクリプトに渡すことで、まったく同じエラーテキストを再現しました。さらに新しいlf-6.18.37-2.1.0も確認しました。タグ: 衝突はまだそこに存在します。 推奨される修正方法:ドライバ/mxc/vpu/wave511/MakefileのNXPモジュールのビルドターゲットをwave5.o/wave5-ctrl.oからwave511.o/wave511-ctrl.oに名前変更してください。ソースファイル名はそのままです。これは1ファイルだけの変更で、ドライバに機能的・動作的な影響はありません。変更を適用した後、ビルドが正常に完了し、scripts/modules-check.sh で競合が検出されなくなったことを確認しました。 代わりに、depends on!を追加することも考えました。NXP KconfigにVIDEO_WAVE_VPUするのですが、モジュールの名前の変更が長期的にはより持続的な解決策です。相互排除に頼る代わりに実際のネーミング衝突を解決できます(相互排除はallmodconfig/allyesconfigの下にドライバを一つ無視し、実際のビルド問題を隠す可能性があります)。また、FUTURE両方のIPブロックを組み合わせるボードがあっても正しいまま維持できます。 下流の影響としては、NXP Wave511ドライバ用にmodprobe wave5 / wave5.koをハードコードするもの(例:Yoctoレシピやrootfsモジュールロード設定)はwave511.koを参照する必要があります。このカーネルツリー内には、そのような参照箇所は見つかりませんでした。 パッチは社内レビューのために提供されます。 よろしくお願いいたします。
View full article
i.MX 95 的 QEMU 你好, 我们已为OpenBMC i.MX 95(机器 ->evb-imx95 ,图像 ->obmc-phosphor-image )版本,使用walnascar 分支的nxp-imx-support 存储库(https://github.com/nxp-imx-support/meta-nxp-openbmc/tree/walnascar)。 我们没有可供测试的评估板,因此我们想知道 i.MX 95 平台是否支持 QEMU 仿真以运行 OpenBMC 镜像。 具体来说: NXP 是否为 i.MX 95 提供 QEMU 机器模型(例如,在 imx-qemu 存储库中),并且它是否支持启动 OpenBMC 镜像?如果没有,有没有推荐的无需硬件即可测试 OpenBMC 镜像的方法? 我们检查了上游 QEMU,没有找到 i.MX 95 机器类型。 谢谢 Re: QEMU for i.MX 95 嗨@Kavinraj_08 我们尚未发布支持 i.MX 95 的 QEMU 软件包。同时,目前还没有针对 i.MX 95 OpenBMC 的无硬件测试解决方案。 B.R
View full article