Hi NXP Support Team,
I downloaded the "Safety Peripheral Drivers for S32K3 Version 1.0.6"
After installing and importing the SPD_example_S32K388_M7_0_0 project into S32 Design Studio, I found that the main.c is essentially empty
**My Environment:** - S32 Design Studio for S32 Platform 3.5 - SPD Version: 1.0.6 (SW32K3_SPD_1.0.6_D2512_DesignStudio_updatesite_updated.zip) - Target: S32K388 M7_0
**What I Expected**
Please send complete register-level examples for:
ECC on all memories (Flash, SRAM, TCM) -
FCCU (Fault Collection and Control Unit) -
STCU2 (Self-Test Control Unit 2 with LBIST/MBIST) -
EIM (Error Injection Module) -
ERM (Error Reporting Module) -
CMU (Clock Monitor Unit) -
Lockstep Core -
SWT (Software Watchdog)
Or provide download link.
Thank you.
Best regards,
Hi @xlele,
Copilot said: The SPD provides a complete demo project, but it is available only for EB Tresos and not for the S32DS IDE.
The demo is distributed in the standalone .exe version.
danielmartynek_0-1782819658938.png
Here is an unofficial SPD example for S32DS IDE.
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-BIST-eMCEM-SPD106-v2-0-S32DS365-RTD...
There is one bare-metal EIM, ERM example:
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-EIM-ERM-DTCM-SRAM-Baremetal-v3-0-S3...
One CMU_FC example:
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-MCAL-MCU-ClockMonitor-v1-0-S32DS36-...
SWT example can be found by default in RTD.
Best regards,
Daniel