Abstract
This example presents an use case for analogue data capturing using eMIOS, BCTU, SAR-ADC and DMA modules on S32K39-37-36 series based on the RTD low level API to support diverse application needs.
Connections:
S32K396-BGA-DC1 -> Pin -> Signal -> Label
J62-1 -> PTC30 -> siul2_gpio_xx -> GPIO1_GPT (D0)
J58-1 -> PTE14 -> emios_0_ch_19_z -> PWM1
J58-2 -> PTG9 -> siul2_gpio_xx -> GPIO2_eMIOS_Trigger
J62-2 -> PTC31 -> siul2_gpio_xx -> GPIO3_BTCU_Trigger
J62-4 -> PTD6 -> siul2_gpio_xx -> GPIO4_BTCU_Watermark
J62-24 -> PTB14 -> adc1_s21 -> ADC1
*To use the potentiometer of S32X-MB connect:
J62-24 (in S32K396-BGA-DC1) to P26-1 (in S32X-MB)
Note:
Following line should be added in project/generate/src/Bctu_Ip_PBcfg.c every time the code is updated in Config Tools:
#define DMA_LOGIC_CH_0 ((uint8)0U)
Detailed Description:
The Compare Value of GPT eMIOS_0_ch_0 generates a time-out period. Once time-out is reached its Emios Notification toggles GPIO1. This allows us to observe in scope 2 events, which describe the start and the end of the signal sequence.
The eMIOS_0_ch_23 channel is configured as global counter bus A. In this setup, it can act as the time base for other eMIOS_0 channels, enabling synchronization between other them—there is just one PWM in this case. This synchronization ensures that channels share the same time base, thereby defining a common period for their operation.
The emios_0_ch_19_g channel is configured as OPWMT mode, which offer more flexibility for triggering. An interrupt is requested on every flag event, during which GPIO2 is toggled—happens at half the time high in this case. This flag event, can be configured using Trigger parameter.
For more details about eMIOS, please refer to S32M27x/S32K3 – eMIOS Usage, considering differences for porting from S32K3 to S32K39-37-36 in AN14301.
The BCTU implements a list for parallel conversions using ADC0 and ADC1. Which is triggered by the eMIOS channel, and the resulting data is stored in FIFO1, as follows:
For debugging purposed the GPIO3 is toggled every BCTU Trigger Notification. Additionally, the GPIO4 is toggled in BCTU Watermark Notification, which happens every time the number of active entries in FIFO exceeds the watermark level, and therefore the data is available for reading.
See full signal sequence in Figure 1:
Figure 1. Signals of example project
When you suspend debug session, in Expressions tab (Figure 2) you can observe results: g_fifo1Result, which corresponds to the BCTU list measurements, meanwhile g_fifo1Volts corresponds to the conversion in volts.
Figure 2. Expressions tab of example project
References
Application Software:
- S32K396_RTD600_eMIOS_BCTU_SARADC_DMA_Ip_example
Example was built and tested using the following IDE and Driver versions:
- S32 Design Studio for S32 Platform Version 3.6.3
- S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0