1993717_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1993717_en-US

1993717_en-US

HARDWARE RESET or SOFTWARE RESET

Hi there,

Can someone help me with enabling a Watchdog timer and also steps to initiate Software reset. I am using a S32k14x EAR SDK v0.8.6 for writing my vehicle application code. So i want to enable Watchdog timer so couldn't able to figure any knowledge base where i can get help from. And also i need help in Hardawre reset and Software Reset process.

It would be really helpfull if some one lends me hand here. Thanks in advance 

#S32K146

Re: HARDWARE RESET or SOFTWARE RESET

Hi @Julián_AragónM 

Thank you for the information.


Re: HARDWARE RESET or SOFTWARE RESET

 Hi @akhilranga,

For SW reset, please look at chapter 25.2.2.7 from the S32K Reference Manual, it explains the reset control register. 

You can also use this example as reference, where a SW reset is implemented to test the ram retention: Example S32K144 RAM Retention S32DS.R1 - NXP Community.

There is also this function in the system_S32K144.c file:

Julin_AragnM_0-1731595074372.png

For the watchdog, there are many community posts sharing some reference code, such as:

You can also refer to the examples inside the EAR SDK.

Best regards,
Julián

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 03:04 PM
更新者: