1899624_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1899624_en-US

1899624_en-US

The best way to build a PCB first time right with KW47 (Automotive) or MCX W72 (IoT/Industrial)

Please, find the important link to build a PCB using a KW4x or MCX W7x and all concerning the radio performances, low power and radio certification (CE/FCC/IC).

matthieu_baudry_0-1768238081772.pngmatthieu_baudry_0-1768238081772.png

“As RF behavior are dependent of PCB layout & manufacturing; PCB prototypes (based on NXP recommendations) will have to be fine-tuned to insure the expected qualified in RF is reached on the final productized platform.”

KW47 product NXP web page:  https://www.nxp.com/products/KW47

MCXW72 product NXP web page: https://www.nxp.com/products/MCX-W72

Board pages: 

KW47-EVK Evaluation Kit with Bluetooth® Low Energy 6.0

KW47-LOC Localization Reference Design using KW47

MCXW72-LOC Localization Board for MCX W72 Bluetooth Channel Sounding MCU

FRDM-MCXW72 Development Board for MCX W72 Wireless MCU

 

in addition of the product webpages please refer to KW47 Knowledge Hub


Do not use pre-production or production board prior to April 2026 KW47-LOC or MCXW72-LOC platform for Channel Sounding certification - contact NXP for further note

NXP Channel Sounding PAGE

       (Bluetooth® SiG Channel Sounding Technical Overview )

More Channel Sounding enablement Available on request to NXP 

Channel Sounding Fundamentals for the KW47 and MCX W72[AN14865]
Fundamental Steps to Design a Channel Sounding Board - Creating a Simple PCB without Diversity[AN14832]
Fundamental Steps to Design a Complex Channel Sounding Board[AN14869]

       Printed Channel Sounding Antennas for the KW47 and MCX W72[AN14779]

HARDWARE

KW47-MCXW72-EVK HW guideline:

KW47 Hardware Design Guide[UG10127]

MCX W72 Hardware Design Guide[UG10273]

HVQFN48 package specification: SOT619-17(D)   pending release of SOT619-17(DD)  

KW47-MCXW72-EVK User Manual 

KW47-LOC Board User Manual[UM12114]
KW47-EVK Board User Manual[UM12094]
MCXW72-LOC Board User Manual[UM12113]
FRDM-MCXW72 User Manual[UM12222]

Minimum BoM (attached file) 

DCDC management guide (AN13831) :  Power Management Hardware (nxp.com) - KW45 applicable for KW47 waiting release of KW47/MCXW72 

Design-In check list: see attached file at the bottom of this article

RF matching: S parameters (attached file) Available on request 

 

How to handle coincell application on PCB:

 Coin Cell Hardware Recommendations for Kinetis Bluetooth LE Applications[AN14664]

KW47-MCXW72 module can also be handled in standalone:

 How to run KW47-M2 standalone

RF output power level:

Please note it is expected that each final PCB platform, is refine with the right RF matching and filtering, to fit your market and region mandatory certification.

For instance the +10dBm at pin level can be exceeded in some configuration. It is final PCB owner responsibility to build a system (incl. all Rf path loss) with the expected target power level fitting with Bluetooth SiG Core spec and European radio certification target. Then the Tx power has to be adjusted at application level.

 

UFL SMA CABLE: On EVK, to connect M10 module for RF trials a µFL to SMA cable is recommended: 

CSH-SGFB-200-UFFR TE Connectivity / Linx Technologies | Mouser France

On KW47-LOC or MCXW72-LOC to connect SMA specific connector has to be populated: TE Connectivity Ltd CONSMA021.062-G. Warning to solder SMA connector:  please insure the PCB edge is well cut and right smooth; if not please mill a bit with a sand paper. (risk is to get SMA core line not well soldered on PCB line)

Also for higher Harmonics the µFL is not convenient as connector is limited above 6GHz (an SMA has to be soldered to control RF losses )

RF matching component tolerance:

Please note, on NXP EVK, FRDM and LOCalization platform the RF matching components (Inductors, Capacitors) are using the HIGH tolerance Muratasets. During your RF board tuning you may need to use low tolerance Murata set to insure all RF limits are passing.

Eg: GJM1555C1H3R3CB01D is +/-0.25pF tolerance where GJM1555C1H3R3BB01 with +/-0.1pF tolerance may be preferred

Eg2: LQG15HS1N3S02D  is +/-0.3nH tolerance where LQG15HS1N3B02D   with +/-0.1nH tolerance may be preferred

KW47 from KW45 hardware porting : 

KW47 is pin to pin compatible with KW45. However from HW point of view, some components values will have to be adjusted like RF matching components values.

Other components around KW4x are not foreseen as to change based on current silicon validation.

 Please also note some new muxing is in place to get new features of KW47 on pins. For instance on KW47 a second Flex CAN is available. See attached file

RADIO

RF report: 

       AN14461: KW47-EVK RF System Evaluation Report for Bluetooth Low Energy Applications | NXP Semiconduc...

KW47-LOC RF System Evaluation Report for Bluetooth Low Energy Applications

       AN14580: MCX W72 RF System Evaluation Report for Bluetooth and IEEE.802.15.4 Applications | NXP Semi...


Radio co-existence: 

Kinetis Wireless Family Products Bluetooth Low Energy Coexistence with Wi-Fi Application (nxp.com) p...

Antenna: 

Compact Planar Antennas for 2.4 GHz Communication Designs and Applications within NXP EVK Boards

Printed Channel Sounding Antennas for the KW47 and MCX W72[AN14779]

Return loss (S11) measurement: How to measure the return loss of your RF matching (S11) part of the RF report (AN13728)

Loadpull: Loadpull Test Report for KW47[AN14696]

SW tools for RF trials:

    IoT Tool box (mobile application)

    Connectivity test tool for connectivity products (part of the IoT toolbox)

    DTM: How to use the HCI_bb on Kinetis family products a... - NXP Community

https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/BLE-HCI-Application-to-set-transmitter-...


CRYSTAL

  Recommended Crystal attached

  Articles: KW47/MCX W72 32MHz & 32kHz Oscillation margins - NXP Community 

32 kHz Crystal-less Mode on KW47[AN14884]

  Please note for Channel Sounding feature with higher 10dBm transmit output, some specific care have to be taken adding to pass all harmonics on all Bluetooth Channels: see "32 MHz crystal harmonics design recommendations" chapter in "AN14826: KW47-LOC RF System Evaluation Report" where an extra inline inductor on Xtal path may be needed.

LowPower

     All power profiling tools are available in this NXP community web page:

             KW35, KW38, KW45, KW47 & MCX W71, MCX W72 & MCX W23 Power Profile Tools (including Localization)


     Bluetooth LE power profile estimator Tool 

             KW45_WK47_MCXW71_MCXW72_BLE_power_profile_calculator vx.x.xls

     802.15.4 Matter & Zigbee power profile estimator Tool

              MCX W7x 802.15.4 Matter ICD SIT LIT & ZED Power profile vx.x.xls


     CCC Channel Sounding BLE power profile estimator Tool

              KW47 Digital Key CCC CS Power Estimator tool vx.x.xls

              AN14628_AN14628_KW47_CCC_CS_Power_Profile_estimator tool_release.pdf


CERTIFICATION

RF full certification of KW47/MCXW72  available on board product pages

KW47 and MCXW72 are Bluetooth 6.x channel Sounding certified!

Tags (1)
No ratings
Version history
Last update:
‎08-24-2026 08:01 AM
Updated by: