1100375_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1100375_en-US

1100375_en-US

DEVKIT-ZVL128 EVB review

The DEVKIT platform

The NXP released new board platform for automotive products – DEVKIT.

The DEVKIT is a low-cost development platform with Arduino UNO/Mega pin compatibility. In my review, I will focus mainly on DEVKIT-ZVL128 board.

                                         166907_166907.jpgSNC01165 (800x527).jpg

The DEVKIT boards are similar to FRDM boards, but they are slightly wider (58mm versus 53mm) due to moving MCU specific pins to external rows of Arduino pin compatible connectors. So, we should be able to access MCU specific pins even when we connect any Arduino shield on top of this board.

 

166908_166908.jpgSNC01161 (800x285).jpg


The other currently or soon available DEVKIT boards are:

DEVKIT-S12ZVL

DEVKIT-S12ZVC

DEVKIT-S12G128

DEVKIT-S12XE

DEVKIT-S12VR64

DEVKIT-MPC5748G

DEVKIT-MPC5744P

FRDM-KEA128

FRDM-KEA64

FRDM-KEA32

DEVKIT-COMM - 6 LIN and 4 CAN transceivers shield

DEVKIT-MOTORGD – three-phase motor control shield with GD3000 N-channel MOSFETs driver and power stage

Note: The FRDM-KEA boards belongs also into the DEVKIT platform despite on the “FRDM” in the board name.



The Content

What you will get for US$35 (current price on NXP web pages):

  • Antistatic paper box
  • DEVKIT-ZVL128 board
  • short micro-USB cable

 

166909_166909.jpgSNC01164 (800x662).jpg 

 

The sticker on the box points to the NXP web pages for downloading more documents such as the quick start guide, schematic, PCB BOM and design files, code examples or buy the same board again ;-).

Unfortunately, the board User Guide is not available yet.


This web page is also offering “Getting Started” tab with the interactive quick start guide – quite useless feature since the page forgets on necessary 12V power supply for MCU powering and it proposes old CW5.1 (Classic IDE) for S12(X) instead of CW10 (Eclipse IDE).


What else you will need:

  • The IDE – for example, the NXP CodeWarrior or Cosmic ZAP
  • 12V DC power supply (3.8V~40V) with barrel connector (6mm outside diameter x 2mm inside diameter)
  • MCU code

The Board

DEVKIT-ZVL128 board is assembled by:

  • S12ZVLA128 MCU (Big Knox) in 48-pin LQFP package
  • 8MHz crystal
  • Standard 2mm DC power jack connector for 12V power supply
  • On-board OSBDM debugger trough micro-USB connector
  • Standard BDM connector
  • Arduino UNO pin compatible connectors with extended connectivity (the internal rows of the connectors are arranged to fulfill Arduino™ shields compatibility)
  • RGB LED and 2 x push button switches
  • LIN and CAN connectors
  • CAN transceiver MC33901
  • 5k potentiometer and RESET switch
  • 3V/150mA and 5V/150mA LDO voltage regulators


The great thing is that the board has connector pins named from the bottom side of the PCB = less tracking on schematic.

 

166910_166910.jpgSNC01166 (800x532).jpg

 

On another side, some of the MCU pins may be routed to Arduino connectors trough zero Ohm resistors. Since these resistors are very small (size 0402), the potential re-routing will need a solid hand.

 

166911_166911.pngZeroOhmResistors.png

 

It is great that loop type test points arrived finally also on low-cost development boards – now in surface mount version. The small loops may be simply locked by test hooks and measured by laboratory equipment.

 

166914_166914.jpgSNC01168 (800x431).jpg

166913_166913.pngTestLoop.png

 

 

The MCU

The S12ZVLA128 is one of MagniV family MCUs using the 180nm NVM + UHV technology that offers the capability to integrate 40V analog components. It integrates S12Z core, features from the existing S12 portfolio together with “high-voltage” analog modules, including the voltage regulator (VREG) and a Local Interconnect Network (LIN) physical layer (LIN PHY).

The S12ZVL(A)128/96/64 derivatives introduces several unique enhancements in comparison with older S12ZVL32/S12ZVL16 derivatives:

  • Significantly bigger memories (64/96/128kB flash, 1/2kB EEPROM, and 4/8kB RAM)
  • The VDDX voltage regulator is capable of providing 5V or 3.3V
  • MsCAN module
  • The S12ZVLA derivatives additional features/improvements:
  • 2% VDDX regulator tolerance improvements
  • 10/6 channel 12bit ADC
  • 8bit DAC module
  • the rail-to-rail analog comparator (ACMP)
  • the Programmable Gain Amplifier (PGA)

I am going to use the PGA for thermocouple measurement in the near future.


Software

The Software Integration Guide guides us through CW 10.6.4 installation and creating a new project with Processor Expert (PE) tool. Unfortunately, while following that guide, I discovered that the CW10.6.4 does not offer PE as an option (only project without PE) when I tried to create an S12ZVL128 project. But this option is available in newer CW10.7 version.

Note: If S12ZVL(A)128 derivative is missing in your CW10.6.4 IDE, please update your CW IDE via menu-Help-Install New Software-FSL MCU Eclipse Update Site and focus mainly on “S12Z Support” and “MCU 10.6.4 Updates” folders.


The code examples contains three primitive example projects:

DEVKIT-ZVL128_Lab1GPIO – configure GPIO pins

DEVKIT-ZVL128_Lab2ADC – initialize and measure ADC value

DEVKIT-ZVL128_Lab3PWM – configure voltage regulator, initialize CLOCK, initialize and measure ADC value, generate PWM


Note: The zip file contains already built projects. The loading it into MCU does not work due to different paths. We have to clean it and build again in our workspace prior loading into the MCU.


These projects are really simple, but they omit some specific potential issues.

For example:

  • I would like to recommend to configure CPMUVREGCTL_VREG5VEN bit also in GPIO example since this bit influences output pin voltage levels. The value of the CPMUVREGCTL_VREG5VEN bit is not influenced by any MCU reset. So, we have to be careful especially when we are starting a new project with new peripherals connected to the S12ZVL128 GPIO pins.
  • The ADC command lists (adc0_cmdlist) and ADC result lists (adc0_results) are not aligned in these example codes. It may be fixed by simple modification:
    volatile unsigned char adc0_cmdlist[1][4] __attribute__ ((aligned (4))) = {0xC0,0xD0,0xA0,0x00};
    volatile unsigned short adc0_results[1] __attribute__ ((aligned (4)));‍‍‍‍

The NXP offers for this MCU also LIN2.x and SAE J2602 Stack and S12Z NVM Standard Software Driver (Flash/EEPROM driver).


There are also well-documented example codes at Community from Technical support team which may be used for an inspiration. For example:

S12ZVM clock module and PLL configuration - SW examples

S12Z Interrupt catcher for unexpected interrupts

S12Z voltage measurement

A Library of Functions for HD44780 Based LCD Modules (no R/W) for S12Z devices

S12ZVL-TIM-FrequencyMeasurement

S12Z Flash example code

S12Z EEPROM example code


The next source of information may be NXP application notes. For example:

AN4723 S12Z MagniV Bootloader with SW,

AN4731 Understanding Injection Current on Freescale Automotive Microcontrollers,

AN4841 S12ZVL LIN Enabled Ultrasonic Distance Measurement with SW,

AN4842 S12ZVL LIN Enabled RGB LED Lighting Application with SW,

AN5084 Hardware Design Guidelines for S12ZVL Microcontrollers,

AN5122 Using Freescale’s LIN Driver with the MagniV Family with SW


Summary

One of the best advantages of DEVKIT platform is the price. When we compare DEVKIT board prices with alternative evaluation boards (if any exist), we may save between 40 and 95 % EVB price depending on target MCU family. For example, the older TRK-S12ZVL board (assembled by S12ZVL32) is bigger, additionally offers 9 user switches, buzzer, HVI potentiometer, switchable LIN_OUT connector and header ring with all MCU pins. But the price is also almost three times higher than the price of DEVKIT-ZVL128.

Also, the connectors with standard 100mils pitch are definitely plus in comparison with previously used TWRPI/PCI EXPRESS connectors and the board allows using plenty of available Arduino shields without complex hardware interconnections. You may look for it for example at Arduino pages, shieldlist.org, Adafruit, …


From my side - thumbs up :smileycheck:.

Re: New EVB platform: DEVKIT-ZVL128 Review.

Hi Peter,

Thank you for notification. I reported this issue almost two years ago.

It seems, that nobody fixed it until now.

I will report it again.


The issue is related to QSG and Getting Started page also …


There is just simple Note on the board web page “12V (1 Amp) power supply is required for debugging and CAN/LIN communication, this is not included in the kit”

https://www.nxp.com/support/developer-resources/hardware-development-tools/ultra-reliable-mcus-devel...

Best regards

Radek

Re: New EVB platform: DEVKIT-ZVL128 Review.

Hello Radek,

Thanks for the clear explanation.

Do you know if this is somewhere documented?

I have found the quick-reference-guide/DVKITZVL128QSG.pdf but this only suggests the opposite:

"CAUTION:

               When powered from the USB bus, do not exceed the 500mA maximum allowable current drain. Damage to the target board or host PC may result."
Re: New EVB platform: DEVKIT-ZVL128 Review.

Hi Peter,

Unfortunately, the DEVKIT-ZVL128 board cannot be directly powered from USB.

The assembled S12ZVL128 MCU is part of MagniV family which is designed for powering directly from 12V line. So, the 5V from USB is simply not sufficient for MCU powering.


Note: The S12ZVL128 MCU may be theoretically directly powered from 5V power supply connected to the VDDX/VDDA pin (MCU is not designed for such use). However, in such case we must connect also VSUP pin the same power line for avoiding any issue with transient effects. Such connection will also disable main features of this MCU(integrated power supply, internal LIN PHY,…)


Yes, the 'Power Supply Selection section with jumper option to P5V_SWUSB' is just misunderstanding.

The jumper J13 (+JP1) choose one of source power supplies (MCU, USB, U13 voltage regulator) only for on-board CAN transceiver and Arduino-Uno compatible J3 header. The output from J13 jumper is P5V0 signal.


I hope it helps you.

Best reagrds

Radek

Re: New EVB platform: DEVKIT-ZVL128 Review.

Hi,

You mention a "12V DC power supply (3.8V~40V) with barrel connector (6mm outside diameter x 2mm inside diameter)" is needed. Can the board also be powered by USB?

My guess is yes as the schematic shows a 'Power Supply Selection section with jumper option to P5V_SWUSB' .

Therefore I tried setting the jumper 13 between 2-3 but no connection 'Target MCU is not responding'. Measuring their is no power on J13 Pin3. This makes me believe MIC2026-1YM is not enabling OUTB because ENB is not powered. (Measuring proves this hypothesis). Why is +VTRG_ENB not enabled by MC9S08JM60CGTE?

Or am I misunderstanding jumper 13?

Re: New EVB platform: DEVKIT-ZVL128 Review.

Hi Robin,

You are right and thank you for notification.

The final name is DEVKIT-MOTORGD.

I will update this document.

I hope it helps you.

Have a great day,
Radek

Re: New EVB platform: DEVKIT-ZVL128 Review.

Hi

One of the customer want to get the DEVKIT-MCSHIELD.

DEVKIT-MCSHIELD.png

I notice that "Note: The grayed names are just for prototype boards, the final board names may be different."

I am not sure if that board has another name: DEVKIT-MOTORGD. Since it look like the same.

DEVKIT-MOTORGD.png

Would you please tell me where can the customer get DEVKIT-MCSHIELD?

Thank you for the help in advance!

 

Best Regards,

Robin

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-20-2025 06:30 AM
更新者: