dsp56f803

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dsp56f803

566 Views
Alex1972andr
Contributor I

 здравствуйте помогите разобраться как настроить Code Warrior

Для работы с для работы с DSP56F803 для работы с DSP56f803 . за рабочую информацию судовольствием оплачу заранее очень благодарен
установил Code Warrior помогите разобраться как ее настроить для работы с данным контроллером

0 Kudos
Reply
1 Reply

548 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @Alex1972andr ,

Thanks for your post. The DSP56f803 need to use CodeWarrior Classic v8.3. 

CodeWarrior Classic v8.3 link: CodeWarrior Development Tools for 56800/E DSC | NXP Semiconductors

You can refer to CodeWarrior ™ Development Studio for Freescale ™ 56800/E Digital Signal Controllers - Quick Start to simply learn how to use it.

For more information, you can click "Documentation"  and then choose any doc you want.

Celeste_Liu_0-1733222750920.png

Regarding the operation of CodeWarrior Classic on non-Windows XP systems, you can refer to:

Windows 7/10: Using USB TAP on CodeWarrior for DSC - NXP Community

Hope it can help you.

Best Regards,

Celeste

 

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

an_flash_over_jtag.fm

0 Kudos
Reply