hi, TechSupport
When we use GD3160 to drive Sic(used in hil, no rear high voltage and real current).under some Test case. INTB will be triggered. and the STATAS1 VCCOV bit is "1", i don't know why is the fault reported. and i don't find the config about VCCOV .could you give me some advice? which signals should we test?(The test case which triggered fault is to generate a large current with PWM)
Hi,
I would recommend you to take a close look at our AN13129 - Fault management, diagnostics, interrupt, and priority table of GD316x advanced IGBT and SiC gate driver:
Please make sure you are signed in to nxp.com. If you do not see AN13129, please click on "Request additional access" or edit your secure access rights by going to My NXP > Profile. For more information about secure access rights, please refer to this website:
https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS
BRs, Tomas