Cannot run FreeMASTER MCAT on MTRDEVKSPNK144 kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot run FreeMASTER MCAT on MTRDEVKSPNK144 kit

ソリューションへジャンプ
3,068件の閲覧回数
radudrosescu
Contributor III

Hi,

I bought the MTRDEVKSPNK144 - 3-Phase PMSM Motor kit through the Farnell distributor. Now I see that there are newer (active) versions, MTRDEVKSBNK144 and MCSPTE1AK144 and I would like to know the hardware and software/firmware differences between these kits. The kit I bought does not contain any software support (CD, DVD, Memory stick) and although the motor is running controlled by SW2, SW3 (OK LED) I can't connect it to FreeMaster (3.1). Specifically in the C:\NXP folder there is no installed application or folders \ MCSPTE1AK144, \MC_DevKits\MCSPTE1AK144\sw. The only application I found in S32K SDK is freemaster_s32k144.pmp. There is no s32_pmsm_sensorless.pmp application to allows access to FreeMASTER MCAT (steps 7-10 from QSG) or to control the motor.

Thanks very much!

Radu

0 件の賞賛
返信
1 解決策
3,057件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

please follow the user guide in order to setup demo kit with freemaster.

petervlna_0-1606294245465.png

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/arm-based-solutions...

You can find SW release notes in folder where the SW is installed.

SW link:

https://www.nxp.com/webapp/Download?colCode=MTRDEVKSPNK144_SW&appType=license

I do not expect that HW changes will cause any issues. I will ask demo author if there were any which can influence the application execution.

 

best regards,

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,048件の閲覧回数
radudrosescu
Contributor III

Hi Peter,

Hi Peter,

Thank you very much. I solved the problem after your first answer. You can consider the matter closed.

Best regards!

Radu

0 件の賞賛
返信
3,055件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

OK, I got some information from author:

There is no change in HW at all. The Naming of the KIt was changed in order to better describe kit.

Additionally there were MTRDEVKSBNK144, MTRDEVKSPNK144 and now it is replaced with one kit MCSPTE1AK144 where you can burn 4 different example SW.

 

best regards,

Peter

0 件の賞賛
返信
3,058件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

please follow the user guide in order to setup demo kit with freemaster.

petervlna_0-1606294245465.png

https://www.nxp.com/design/development-boards/automotive-motor-control-solutions/arm-based-solutions...

You can find SW release notes in folder where the SW is installed.

SW link:

https://www.nxp.com/webapp/Download?colCode=MTRDEVKSPNK144_SW&appType=license

I do not expect that HW changes will cause any issues. I will ask demo author if there were any which can influence the application execution.

 

best regards,

Peter

0 件の賞賛
返信