the Parameter calculation does not match

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the Parameter calculation does not match

4,002件の閲覧回数
董培董
Contributor II

hi ,

 When calculating the parameters of the observer, if the motor and electrical parameters are exactly the same, according to the method in the document(MC9S12ZVMMCLUG), the result calculated by MATLAB is different from the result calculated by MCAT. Is that accurate?The picture is as follows:

微信截图_20200921182715.png微信截图_20200921182715.png

微信截图_20200921183615.png微信截图_20200921183615.png

微信截图_20200921184242.png微信截图_20200921184242.png

微信截图_20200921184352.png微信截图_20200921184352.png

I want to get your help ,thank you very much!!!

 

0 件の賞賛
返信
5 返答(返信)

3,909件の閲覧回数
Bark_8
Contributor I

thanks

0 件の賞賛
返信

3,913件の閲覧回数
Bark_8
Contributor I

Thanks for this info

0 件の賞賛
返信

3,965件の閲覧回数
nofake_drstrang
Contributor III

hi @董培董 ,

one question please:

 

do you use the example :

"\NXP_MBDToolbox_S12ZVMx\S12ZVM_Examples\s12zvm\mc\PMSM_Demo\PMSM_ClosedLoop"

of the new toolbox version 1.4 

thanks in advance!

Best regards.

0 件の賞賛
返信

3,949件の閲覧回数
董培董
Contributor II

Hi, The soft version is as follows,and the FREEMASTER is 3.0,I hope I can get help,thank you very much

董培董_0-1601166193157.png董培董_0-1601166193157.png

 

0 件の賞賛
返信

3,988件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

@marekmusak , can you please comment on this?

Thank you,

Marius

0 件の賞賛
返信