sweep mask parameter in a for loop -- block "MC3377xC Get Values" NXP Model-Based Design Toolbox

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

sweep mask parameter in a for loop -- block "MC3377xC Get Values" NXP Model-Based Design Toolbox

跳至解决方案
1,000 次查看
CZ_FB
Contributor I

Hello, 

I am using the block "MC3377xC Get Values" (and other blocks in the 'BMS_3377xC' library) from the NXP Model-Based Design Toolbox in Matlab Simulink 2023b.

I would like to know how to sweep the mask parameters (such as the 'Instance' and 'CID' values in the "MC3377xC Get Values" block) in a For Loop in Simulink simulation and for embedded code generation. 

Thanks

Cheng

0 项奖励
回复
1 解答
914 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @CZ_FB,

Unfortunately, this requirement is not possible right away, because it requires a serious update/patch coming from the MBDT team. We have to redesign and modify the blocks from the toolbox to accept both the CID and the Instance as a block input. I will open a ticket for such changes, but because we have no roadmap to cover a new release for the MBDT for S32K1, I cannot promise this will be implemented.

To faster help you with such requirements, I can identify 2 options:

1. You could use a switch case, and in each case place a block to handle the CID and Instance you need to cover.

2. The second option would be to create a block that uses custom code, after a template or method described in this article https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...

How many BCCs do you need to cover?

Regards,

Marius

在原帖中查看解决方案

1 回复
915 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @CZ_FB,

Unfortunately, this requirement is not possible right away, because it requires a serious update/patch coming from the MBDT team. We have to redesign and modify the blocks from the toolbox to accept both the CID and the Instance as a block input. I will open a ticket for such changes, but because we have no roadmap to cover a new release for the MBDT for S32K1, I cannot promise this will be implemented.

To faster help you with such requirements, I can identify 2 options:

1. You could use a switch case, and in each case place a block to handle the CID and Instance you need to cover.

2. The second option would be to create a block that uses custom code, after a template or method described in this article https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...

How many BCCs do you need to cover?

Regards,

Marius