*.rbf file flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

*.rbf file flash

2,660 Views
jiangfeng
Contributor III

Hi,Dear Surpport:

I download the s12zvm.rbf  file into the S12ZVMx12EVB when I used the Motor Control toolbox  .

However I can't flash any other program into the board via BDM after finishing the s12zvm.rbf.

So I want to erase the bootloader while it 's been protected like the last picture.

Could you help me to solve this? Thanks very much.

pastedImage_2.pngpastedImage_1.png

Tags (1)
0 Kudos
Reply
3 Replies

2,397 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi jiangfeng‌,

Have you tried to check the "Unprotect flash memory before erase" option ? Is it the same error ?

Best regards,

Daniel

0 Kudos
Reply

2,397 Views
jiangfeng
Contributor III

Hi, Daniel

First Thanks for your answers,

I just tried your methods, but it didn't work well ,like the following picture.

pastedImage_1.png

0 Kudos
Reply

2,397 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi jiangfeng‌,

What about from Matlab ? Does it still work to download an application into the flash memory this way ? 

I want to check if this is a system issue or is just an issue with flash operations from CW IDE.

Best regards,
Daniel

0 Kudos
Reply