no CAN communication on MPC5744

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

no CAN communication on MPC5744

1,861件の閲覧回数
hoeldMech
Contributor I

Hi,

I tried to send data from my simulink model over the onboard CAN pins (PB0, PB1) but I cannot get any valid information. Trying to read the signals with a Vector box I only get error frames.
So I tried to make the CAN example project "FlexCAN Master" running which does work neither. I use the MPC5744P RevE. Is it possible that any hardware changes between revB and revE make some issues?
An external power supply of 12 V is used.

Thank for your help!

0 件の賞賛
返信
1 返信

1,841件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @hoeldMech ,

I would first try to run a simple GPIO example to make sure that the code deployment, and the bord is working fine.

Secondly, Can you tell me which are settings for the J43, J44 and J45 jumpers? I would try to put the J43, J44 and J45 on position 2-3 to set the external power for the MCU as well.

Can you give both this a try?

Hope this helps,

Marius

0 件の賞賛
返信