about dtypelib.tlc version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about dtypelib.tlc version

1,840件の閲覧回数
prorubber
Contributor II

hollow,

Recently, my OS is win7, with  matlab2017b , NXP_MBDToolbox_MPC57xx toolboxs(3.0) reintalled. Use the "\code\MPC_Examples\mpc574x\fcan " path,open "flexcan_mpc574x.mdl",error message is:

### Loading TLC function libraries
Error: File: D:\Program Files\MATLAB\R2017b\rtw\c\tlc\lib\dtypelib.tlc Line: 4705 Column: 1
Unrecognized directive "%endieComplexNax" seen
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Error: File: D:\Program Files\MATLAB\R2017b\rtw\c\tlc\lib\dtypelib.tlc Line: 4696 Column: 11
The %if directive on this line has no matching %endif directive
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Error: File: D:\Program Files\MATLAB\R2017b\rtw\c\tlc\lib\dtypelib.tlc Line: 4659 Column: 9
The %if directive on this line has no matching %endif directive
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Error: File: D:\Program Files\MATLAB\R2017b\rtw\c\tlc\lib\dtypelib.tlc Line: 4649 Column: 7
The %if directive on this line has no matching %endif directive
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)

I had installed "MBDToolboxMPC574xPReleaseV2.0.0"+"matlab2017b" ,the error message is about the "dtypelib.tlc" file,and "MBDToolboxMPC574xPReleaseV2.0.0"+"matlab2016b" no problem;when installed "MBDToolboxMPC574xP_V3.0.0"+"matlab2017b" ,build operation error message above;  

want to know ,HOWTO do.

thanks

Prorubber

ラベル(2)
0 件の賞賛
返信
1 返信

1,746件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello 陈宏 陈,

Unfortunately the file dtypelib.tlc is not provided with our toolbox. More than that, I've checked the file that error mentioned and I don't have that text at line 4705. 

 

Can you please be sure that the Matlab is installed correctly, or can you try with different version?

Hope this helps,

Marius

0 件の賞賛
返信