about dtypelib.tlc version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about dtypelib.tlc version

1,847 Views
prorubber
Contributor II

hollow,

Recently, my OS is win7, with  matlab2017b , NXP_MBDToolbox_MPC57xx toolboxs(3.0) reintalled. Use the "\code\MPC_Examples\mpc574x\fcan " path,open "flexcan_mpc574x.mdl",error message is:

### Loading TLC function libraries
Error: File: D:\Program Files\MATLAB\R2017b\rtw\c\tlc\lib\dtypelib.tlc Line: 4705 Column: 1
Unrecognized directive "%endieComplexNax" seen
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Error: File: D:\Program Files\MATLAB\R2017b\rtw\c\tlc\lib\dtypelib.tlc Line: 4696 Column: 11
The %if directive on this line has no matching %endif directive
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Error: File: D:\Program Files\MATLAB\R2017b\rtw\c\tlc\lib\dtypelib.tlc Line: 4659 Column: 9
The %if directive on this line has no matching %endif directive
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Error: File: D:\Program Files\MATLAB\R2017b\rtw\c\tlc\lib\dtypelib.tlc Line: 4649 Column: 7
The %if directive on this line has no matching %endif directive
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)
Main program:
==> [00] D:\Program Files\MATLAB\R2017b\rtw\c\tlc\mw\funclib.tlc:<NONE>(85)

I had installed "MBDToolboxMPC574xPReleaseV2.0.0"+"matlab2017b" ,the error message is about the "dtypelib.tlc" file,and "MBDToolboxMPC574xPReleaseV2.0.0"+"matlab2016b" no problem;when installed "MBDToolboxMPC574xP_V3.0.0"+"matlab2017b" ,build operation error message above;  

want to know ,HOWTO do.

thanks

Prorubber

Labels (2)
0 Kudos
Reply
1 Reply

1,753 Views
mariuslucianand
NXP Employee
NXP Employee

Hello 陈宏 陈,

Unfortunately the file dtypelib.tlc is not provided with our toolbox. More than that, I've checked the file that error mentioned and I don't have that text at line 4705. 

 

Can you please be sure that the Matlab is installed correctly, or can you try with different version?

Hope this helps,

Marius

0 Kudos
Reply