What is the difference between S32 Design Studio v2.0 vs. V2018.R.1, which one should I use?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between S32 Design Studio v2.0 vs. V2018.R.1, which one should I use?

1,489件の閲覧回数
nbutts
Contributor I

It is very confusing. I downloaded and installed S32 Design Studio V2018.R.1 because that had a newer date. But the videos refer to V2.0. Which one is newer and which one should I use?

0 件の賞賛
返信
1 返信

1,415件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi [email protected]‌,

The latest one is S32 Design Studio for ARM 2018.R1 (Windows/Linux) released! and for the MBDT S32K1xx toolbox latest version we recommend using this 2018.R1 in case you want to do debugging.

FYI, the latest MBDT toolboxes contains the GCC v6.3.1 as part of installation package.

Hope this helps!

Daniel

0 件の賞賛
返信