Using the NXP for CAN signals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the NXP for CAN signals

2,053件の閲覧回数
vssaini
Contributor I

Does anyone know what kind of CAN data does the FCAN module output in simulink? 

0 件の賞賛
返信
2 返答(返信)

1,942件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

The CAN receive block outputs data of uint8 type

pastedImage_1.png

You can click on the block to open the mask, then click on Help to get more information on all blocks from our toolbox.

Kind regards,

Razvan.

1,942件の閲覧回数
vssaini
Contributor I

Hi Constantin, 

Thanks for this. I also want to use the vehicle network toolbox that comes with simulink to unpack the CAN messages the FCAN receive will output. Would you happen to know what type of CAN signal the vehicle network toolbox takes as input? 

0 件の賞賛
返信