Using TWR-KV11Z75M with MC toolbox for for Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using TWR-KV11Z75M with MC toolbox for for Kinetis

1,881件の閲覧回数
m_benderradji
Contributor II

Hi,

As far as i know, the Motor Control toolbox for Kenietis support the following MCU's family:

pastedImage_1.png

However, after discussion with NXP team they told me that the KV11 series is an extension to KV10 with more memory and peripherals, and therefore it might simply work with the the MC toolbox using the KV10 blocks.

I understand from this that I can use the TWR-KV11Z75M with the MC toolbox for Kinetis.

Could you please, you members of the NXP MBDT community confirm that it is possible. Thanks in advance.

Best regards

0 件の賞賛
返信
2 返答(返信)

1,765件の閲覧回数
m_benderradji
Contributor II

Thank you for your feedback

0 件の賞賛
返信

1,765件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

the KV11 series is an extension to KV10 with more memory and peripherals, and therefore it might simply work with the the MC toolbox using the KV10 blocks.

I understand from this that I can use the TWR-KV11Z75M with the MC toolbox for Kinetis.

For the moment I can not say if this statement is true or false, as I do not know if all the peripherals are the same and are mapped to the same addresses, if the clock structure is the same, etc. We will have to investigate if our toolbox  works 'out-of-the-box' with KV11. I will get back to you once we test it out and I can be certain that it either works, or it does not. Please note that this will take a while as our team is at the moment in the midst of a MPC574x release and all the focus is on it.

Kind regards,

Razvan.

0 件の賞賛
返信