Using the NXP for CAN signals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the NXP for CAN signals

2,076 Views
vssaini
Contributor I

Does anyone know what kind of CAN data does the FCAN module output in simulink? 

0 Kudos
Reply
2 Replies

1,965 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

The CAN receive block outputs data of uint8 type

pastedImage_1.png

You can click on the block to open the mask, then click on Help to get more information on all blocks from our toolbox.

Kind regards,

Razvan.

1,965 Views
vssaini
Contributor I

Hi Constantin, 

Thanks for this. I also want to use the vehicle network toolbox that comes with simulink to unpack the CAN messages the FCAN receive will output. Would you happen to know what type of CAN signal the vehicle network toolbox takes as input? 

0 Kudos
Reply