Using MBDT in Simulink Projects with "Refresh Simulink customizations" option enabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using MBDT in Simulink Projects with "Refresh Simulink customizations" option enabled

ソリューションへジャンプ
3,273件の閲覧回数
mks004
Contributor II

I am running into an issue when I try to access the MBDT library from the Simulink Library Browser. Everything works as expected when I open a Simulink model and access the Library Browser, i.e. I can see the MBDT blocks in the Library Browser. However when I add the same Simulink model to a Simulink Project with "Refresh Simulink customizations" configuration option enabled, open the model from the project view, and then access the Library Browser, the MBDT blocks are no longer there. All other library blocks still show up as expected.

I use these versions of software:
MATLAB R2020a Update 7
NXP_MBDToolbox_S32K1xx 4.2.0

This issue manifests itself with any model I open. Any help is appreciated.

0 件の賞賛
返信
1 解決策
3,246件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @mks004 ,

Can you please press the F5 button when you open the Simulink library?

If a window appears, select the second option, smth with Generate ... in memory. I am sorry, I cannot reproduce that window now.

Hope this helps,

Marius

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,233件の閲覧回数
mks004
Contributor II

Hello @mariuslucianand ,

This works, thank you.

0 件の賞賛
返信
3,247件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @mks004 ,

Can you please press the F5 button when you open the Simulink library?

If a window appears, select the second option, smth with Generate ... in memory. I am sorry, I cannot reproduce that window now.

Hope this helps,

Marius

0 件の賞賛
返信