Using MBDT in Simulink Projects with "Refresh Simulink customizations" option enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using MBDT in Simulink Projects with "Refresh Simulink customizations" option enabled

Jump to solution
3,281 Views
mks004
Contributor II

I am running into an issue when I try to access the MBDT library from the Simulink Library Browser. Everything works as expected when I open a Simulink model and access the Library Browser, i.e. I can see the MBDT blocks in the Library Browser. However when I add the same Simulink model to a Simulink Project with "Refresh Simulink customizations" configuration option enabled, open the model from the project view, and then access the Library Browser, the MBDT blocks are no longer there. All other library blocks still show up as expected.

I use these versions of software:
MATLAB R2020a Update 7
NXP_MBDToolbox_S32K1xx 4.2.0

This issue manifests itself with any model I open. Any help is appreciated.

0 Kudos
Reply
1 Solution
3,254 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @mks004 ,

Can you please press the F5 button when you open the Simulink library?

If a window appears, select the second option, smth with Generate ... in memory. I am sorry, I cannot reproduce that window now.

Hope this helps,

Marius

View solution in original post

0 Kudos
Reply
2 Replies
3,241 Views
mks004
Contributor II

Hello @mariuslucianand ,

This works, thank you.

0 Kudos
Reply
3,255 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @mks004 ,

Can you please press the F5 button when you open the Simulink library?

If a window appears, select the second option, smth with Generate ... in memory. I am sorry, I cannot reproduce that window now.

Hope this helps,

Marius

0 Kudos
Reply