Undefined function or variable 'lic_err'.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Undefined function or variable 'lic_err'.

Jump to solution
6,239 Views
释然111
Contributor III

Hi,

   When I click on the run prompt “Undefined function or variable 'lic_err' ”, I used 5744MBD,My license are already registered on the website. I am using the DOS Command mode.Can you help me Solve this problem? 

1 Solution
5,438 Views
constantinrazva
NXP Employee
NXP Employee

Hello,

Please find the hotfix for this issue here: https://community.nxp.com/message/915572?commentID=915572#comment-915572 

In that thread you will find all the necessary steps to fix the license disk id limitation by updating a single file in the installation folder. Please confirm if this works in your case.

Thank you!

Razvan.

View solution in original post

6 Replies
5,438 Views
abhishek_kumar1
Contributor IV

Hello, 
 I have tried fixes but it does not work. I am using Matlab 2018b version.

Licence file

#Model-Based Design Toolbox for MATLAB/Simulink - Model Based Design Toolbox #for MATLAB/Simulink MBD supporting MPC574xP for Abhishek Kumar Software #Account # License for DISK_SERIAL_NUM=1A7C7AC0 54E1AD26E296 INCREMENT MC_Toolbox_574xP freescale 1.0 permanent uncounted \      VENDOR_STRING="Model Based Design Toolbox for MATLAB/Simulink \      MBD supporting MPC574xP" HOSTID=DISK_SERIAL_NUM=1a7c7ac0 \      ISSUER="Freescale Semiconductor" ISSUED=29-oct-2018 ck=213 \      SN="FSL - 24906237" TS_OK SIGN="1918 DEAC 1B3C C2A7 58B0 9D87 \      531E 5368 497E B1A2 132F D362 FCAE FE6E 74D9 13F9 D10A 52D1 \      1308 AD33 3513 72FE B870 2F43 D5D4 D486 F68F D03F 7A25 2BF3"

pastedImage_1.png

pastedImage_2.png

Please provide some information.

Regards

0 Kudos
Reply
5,438 Views
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

Can you please attache here (Use Advance editor to show the attach button) the license file and the screen capture with the Window CMD console after you have typed: vol c: command (or whatever partition you used to install the the toolbox on)

Thank you!

Daniel

0 Kudos
Reply
5,438 Views
释然111
Contributor III

QQ截图20170619163039.bmp

QQ截图20170619163133.bmp

license.dat

#Motor Control Toolbox for MATLAB/Simulink MBD - Model Based Design Toolbox
#for MATLAB/Simulink MBD supporting MPC574xP for ? ? Software Account
# License for DISK_SERIAL_NUM=4823 boy
INCREMENT MC_Toolbox_574xP freescale 1.0 permanent uncounted \
VENDOR_STRING="Model Based Design Toolbox for MATLAB/Simulink \
MBD supporting MPC574xP" HOSTID=DISK_SERIAL_NUM=4823 \
ISSUER="Freescale Semiconductor" ISSUED=19-jun-2017 ck=205 \
SN="FSL - 20103187" TS_OK SIGN="1741 D00E E5A3 3705 537E ACBA \
3179 06B4 4947 08F1 AE1A 6B46 FB9E F6ED 395B 1450 BC0D CAAC \
3605 58E1 BC7D 6B97 5CCA 1336 7786 BC39 4EC2 1181 7876 08FE"

0 Kudos
Reply
5,438 Views
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

It looks like you are in this kind of situation: https://community.nxp.com/thread/451913 

since we have a Disk ID with  only 4 numbers. 

We will prepare a patch to fix it and send it to you ASAP.

Thank you!

Daniel

0 Kudos
Reply
5,438 Views
constantinrazva
NXP Employee
NXP Employee

Hello,

Please find the hotfix for this issue here: https://community.nxp.com/message/915572?commentID=915572#comment-915572 

In that thread you will find all the necessary steps to fix the license disk id limitation by updating a single file in the installation folder. Please confirm if this works in your case.

Thank you!

Razvan.

5,438 Views
释然111
Contributor III

thank you very much, it can be used normally!

0 Kudos
Reply