about MPC5744P's bottom drive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about MPC5744P's bottom drive

1,520 Views
gu_dingjie
Contributor I

Detail description:

I am writing bottom drive of MPC5744P in matlab/simulink, but i cant't find Codewarrior which version can support MPC5744P,so I want to get NXP’s guidance.

My detailed steps:

First: writing S-Function of CAN_Transmit.c / CAN_Receive.c / adc_Block.c / adcGroup_Block.c … … in Simulink; Second: Masking those file .c ;

Third: Writing the TLC of file .c;

Fourth: compileing those file by Codewarrior;

But now, no Codewarrior version to support MPC5744P in nxp.com .and then .i found S32 Design Studio is compiler provided by NXP.com. Can I write bottom drive of MPC5744P in Simulink and compile the file by S32 Design Studio

Tags (1)
0 Kudos
Reply
1 Reply

1,387 Views
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

Yes, you can use the S32 Design Studio PA 2017.R1: https://community.nxp.com/docs/DOC-335614 

Also, make sure you apply these hot fixes on top of Matlab/Simulink Toolbox for MPC5744P in order to have it working with this version of S32DS for PA 2017.R1

Best regards,
Daniel

0 Kudos
Reply