Turn off external XTAL frequency warning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Turn off external XTAL frequency warning

ソリューションへジャンプ
2,237件の閲覧回数
ruihang_wu
Contributor III

This is a minor issue.

 

We are using a custom board with S32k processor that uses 40mhz crystal instead of the 8mhz on the evb. When we are compiling from simulink we get a warning that the selected XTAL frequency does not match the one found on the evb.

 

ruihang_wu_0-1627911012878.png

I'm wondering if there is a way to turn off this warning.

 

Thank you

0 件の賞賛
返信
1 解決策
2,219件の閲覧回数
adriantudor
NXP Employee
NXP Employee

Hi @ruihang_wu ,

To disable this warning, you have to uncheck this highlighted check from "Diagnostic" tab of MCU config. block.

adriantudor_0-1628066312305.png

 

Best regards,

Adrian

元の投稿で解決策を見る

1 返信
2,220件の閲覧回数
adriantudor
NXP Employee
NXP Employee

Hi @ruihang_wu ,

To disable this warning, you have to uncheck this highlighted check from "Diagnostic" tab of MCU config. block.

adriantudor_0-1628066312305.png

 

Best regards,

Adrian