Setting up the Target Compilers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting up the Target Compilers

Jump to solution
4,805 Views
zhuaoci
Contributor II

What does the following picture mean? What should I do?

1 Solution
4,350 Views
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

Step 1: Go to System/Advanced system SettingspastedImage_1.png

Step 2: Select the Environmental Variables

 pastedImage_4.png

Step 3: Add a new System Variable

pastedImage_5.png

Additionally you can check the video embedded in the https://community.nxp.com/thread/451240 at 5'10''

Hope this helps!

Daniel

View solution in original post

6 Replies
4,350 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi zhuaoci‌,

I think you have forgot to add the picture.

You can simply copy paste a picture in order to insert it into the message. Otherwise select "Use advanced editor" and the attach button will appear on the bottom of the edition window.

Best regards,
Daniel

0 Kudos
Reply
4,350 Views
zhuaoci
Contributor II

hi Daniel,

      How do I set the target conpiler? what does the follwing picture mean ? I do not understand.

pastedImage_1.png

0 Kudos
Reply
4,351 Views
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

Step 1: Go to System/Advanced system SettingspastedImage_1.png

Step 2: Select the Environmental Variables

 pastedImage_4.png

Step 3: Add a new System Variable

pastedImage_5.png

Additionally you can check the video embedded in the https://community.nxp.com/thread/451240 at 5'10''

Hope this helps!

Daniel

4,350 Views
zhuaoci
Contributor II

Dear daniel,

        Thank you very much.Your answer has solved my problem. But I have another question. Why can't I find the model based design for matlab /simulink MBD supporting MPC5604P?Can you give me some information based on model control for 3-Phase PMSM Kit with Qorivva MPC5604P MCU? What I'm using is 3-Phase PMSM Motor Control Development Kit with Qorivva MPC5604P MCU.)$[M[[~Y$3`7}4`Q(UT`HBD.png

0 Kudos
Reply
4,350 Views
Daniel_Popa
NXP Employee
NXP Employee

For the second question the answer is here: https://community.nxp.com/thread/462635#comment-954320 

0 Kudos
Reply
4,350 Views
zhuaoci
Contributor II

hello daniel,

          Why does the automatically generated code have no project  files?

pastedImage_1.pngpastedImage_2.png

0 Kudos
Reply