S32K344_clockout_s32ct example no clock output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344_clockout_s32ct example no clock output

1,030件の閲覧回数
ErwinR
Contributor III

While learning to use a S32K344 evalboard with Simulink MBDT I've stumbled upon a problem concerning "s32k344_clockout_s32ct" project. The main problem is that there is no clock output on the PTD14 pin that is mentioned in the example project. While checking the Configuration Tool for hardware it seemed that the PTD14 pin wasn't selected for the CLOCKOUT peripheral at all. Although after selecting the pin as the CLOCKOUT output nothing really changed and I didn't get any signal on the osciloscpe. Is there a possible reason and solution for this?

タグ(5)
0 件の賞賛
返信
1 返信

1,016件の閲覧回数
dragostoma
NXP Employee
NXP Employee

Hello, @ErwinR,

Please analyze the response from the other similar thread and come back with information on how it worked. 

 

Best regards,

Dragos

 

0 件の賞賛
返信