S32K344 Freemaster CAN Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 Freemaster CAN Connection

2,815件の閲覧回数
Baris
Contributor II

Is there a CAN connection in Freemaster for the S32K344 MBDT toolbox?
If there is how I use can. If anyone knows can you help me?

Baris_0-1679736414708.png

 

4 返答(返信)

2,714件の閲覧回数
Baris
Contributor II

I want to connect to Freemaster via CAN, what should I do? can you help me?

0 件の賞賛
返信

2,745件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hello @Baris ,

Unfortunately, the S32K3 toolbox does not include support for FreeMASTER over CAN, hence only the Serial option is available in the Connection type dropdown of the configuration block. If further information on how to use the FreeMASTER functionality inside MBDT for S32K3 is required, please let us know about the issues you are encountering.

Regards,

Irina

0 件の賞賛
返信

2,344件の閲覧回数
SSH23
Contributor I
Are there any updates coming in that will support calibration in FreeMaster over CAN for S32K344
0 件の賞賛
返信

2,316件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hello @SSH23 

We can't provide an exact time frame of when FreeMASTER over CAN will be available inside MBDT for S32K3, yet this is a feature we are currently looking into. We will keep you updated on the availability of this functionality.

Thank you,
Irina

0 件の賞賛
返信