S32K344 Freemaster CAN Connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 Freemaster CAN Connection

2,921 Views
Baris
Contributor II

Is there a CAN connection in Freemaster for the S32K344 MBDT toolbox?
If there is how I use can. If anyone knows can you help me?

Baris_0-1679736414708.png

 

4 Replies

2,820 Views
Baris
Contributor II

I want to connect to Freemaster via CAN, what should I do? can you help me?

0 Kudos
Reply

2,851 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hello @Baris ,

Unfortunately, the S32K3 toolbox does not include support for FreeMASTER over CAN, hence only the Serial option is available in the Connection type dropdown of the configuration block. If further information on how to use the FreeMASTER functionality inside MBDT for S32K3 is required, please let us know about the issues you are encountering.

Regards,

Irina

0 Kudos
Reply

2,450 Views
SSH23
Contributor I
Are there any updates coming in that will support calibration in FreeMaster over CAN for S32K344
0 Kudos
Reply

2,422 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hello @SSH23 

We can't provide an exact time frame of when FreeMASTER over CAN will be available inside MBDT for S32K3, yet this is a feature we are currently looking into. We will keep you updated on the availability of this functionality.

Thank you,
Irina

0 Kudos
Reply