S32K344 Freemaster CAN Connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K344 Freemaster CAN Connection

1,903 次查看
Baris
Contributor II

Is there a CAN connection in Freemaster for the S32K344 MBDT toolbox?
If there is how I use can. If anyone knows can you help me?

Baris_0-1679736414708.png

 

4 回复数

1,802 次查看
Baris
Contributor II

I want to connect to Freemaster via CAN, what should I do? can you help me?

0 项奖励
回复

1,833 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hello @Baris ,

Unfortunately, the S32K3 toolbox does not include support for FreeMASTER over CAN, hence only the Serial option is available in the Connection type dropdown of the configuration block. If further information on how to use the FreeMASTER functionality inside MBDT for S32K3 is required, please let us know about the issues you are encountering.

Regards,

Irina

0 项奖励
回复

1,432 次查看
SSH23
Contributor I
Are there any updates coming in that will support calibration in FreeMaster over CAN for S32K344
0 项奖励
回复

1,404 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hello @SSH23 

We can't provide an exact time frame of when FreeMASTER over CAN will be available inside MBDT for S32K3, yet this is a feature we are currently looking into. We will keep you updated on the availability of this functionality.

Thank you,
Irina

0 项奖励
回复