S32K3 MBD I2C Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 MBD I2C Support

ソリューションへジャンプ
1,946件の閲覧回数
Alfredo_Rubio
Contributor II

I have seen that not I2C support is provided in the las S32K3 MDB package.

We were planning to use this bus in our current project. Is there any news on when do you expect to include support to I2C on the MDB package?

Thanks, you in advance.

0 件の賞賛
返信
1 解決策
1,928件の閲覧回数
dragostoma
NXP Employee
NXP Employee

Hi, @Alfredo_Rubio ,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

The I2C support will be included in the upcoming MBDT S32K3xx version 1.5.0 release, which is scheduled for the second quarter.

 

Best regards,

Dragos

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,929件の閲覧回数
dragostoma
NXP Employee
NXP Employee

Hi, @Alfredo_Rubio ,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

The I2C support will be included in the upcoming MBDT S32K3xx version 1.5.0 release, which is scheduled for the second quarter.

 

Best regards,

Dragos

0 件の賞賛
返信
1,626件の閲覧回数
pabloprieto
Contributor I
Any news regarding this issue.
BR

Pablo
0 件の賞賛
返信
1,613件の閲覧回数
dragostoma
NXP Employee
NXP Employee

Hi, @pabloprieto ,

The MBDT S32K3xx version 1.5.0 is not released yet. Until the new version of the toolbox containing I2C support is released, custom code can be used to integrate the I2C component in current projects. You can check the following link with steps to integrate custom code in your model: QSPI for S32K3 is not implemented in the MBDT

Best regards,

Dragos

0 件の賞賛
返信