S32K3 MBD I2C Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3 MBD I2C Support

跳至解决方案
3,091 次查看
Alfredo_Rubio
Contributor II

I have seen that not I2C support is provided in the las S32K3 MDB package.

We were planning to use this bus in our current project. Is there any news on when do you expect to include support to I2C on the MDB package?

Thanks, you in advance.

0 项奖励
回复
1 解答
3,073 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @Alfredo_Rubio ,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

The I2C support will be included in the upcoming MBDT S32K3xx version 1.5.0 release, which is scheduled for the second quarter.

 

Best regards,

Dragos

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,074 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @Alfredo_Rubio ,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

The I2C support will be included in the upcoming MBDT S32K3xx version 1.5.0 release, which is scheduled for the second quarter.

 

Best regards,

Dragos

0 项奖励
回复
2,771 次查看
pabloprieto
Contributor I
Any news regarding this issue.
BR

Pablo
0 项奖励
回复
2,758 次查看
dragostoma
NXP Employee
NXP Employee

Hi, @pabloprieto ,

The MBDT S32K3xx version 1.5.0 is not released yet. Until the new version of the toolbox containing I2C support is released, custom code can be used to integrate the I2C component in current projects. You can check the following link with steps to integrate custom code in your model: QSPI for S32K3 is not implemented in the MBDT

Best regards,

Dragos

0 项奖励
回复