S32K3 MBD I2C Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 MBD I2C Support

Jump to solution
3,097 Views
Alfredo_Rubio
Contributor II

I have seen that not I2C support is provided in the las S32K3 MDB package.

We were planning to use this bus in our current project. Is there any news on when do you expect to include support to I2C on the MDB package?

Thanks, you in advance.

0 Kudos
Reply
1 Solution
3,079 Views
dragostoma
NXP Employee
NXP Employee

Hi, @Alfredo_Rubio ,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

The I2C support will be included in the upcoming MBDT S32K3xx version 1.5.0 release, which is scheduled for the second quarter.

 

Best regards,

Dragos

View solution in original post

0 Kudos
Reply
3 Replies
3,080 Views
dragostoma
NXP Employee
NXP Employee

Hi, @Alfredo_Rubio ,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

The I2C support will be included in the upcoming MBDT S32K3xx version 1.5.0 release, which is scheduled for the second quarter.

 

Best regards,

Dragos

0 Kudos
Reply
2,777 Views
pabloprieto
Contributor I
Any news regarding this issue.
BR

Pablo
0 Kudos
Reply
2,764 Views
dragostoma
NXP Employee
NXP Employee

Hi, @pabloprieto ,

The MBDT S32K3xx version 1.5.0 is not released yet. Until the new version of the toolbox containing I2C support is released, custom code can be used to integrate the I2C component in current projects. You can check the following link with steps to integrate custom code in your model: QSPI for S32K3 is not implemented in the MBDT

Best regards,

Dragos

0 Kudos
Reply