S32K146EVB-Q144 model building error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K146EVB-Q144 model building error

2,114 次查看
ca_liu
Contributor II

Hi

There is an error occurred and i need your help. 

When I tried to build a Simulink model to the board, the program did not report any errors,and the green light next to the mk20d began to flash, indicating that it was downloading. When the download is complete and the green light is on, the red reset light will flash. The entire download process is then repeated. Unless the board is disconnected from the computer, this process will continue to repeat.  After reconnecting, the red reset light will remain on. After that, I tried other models, and the same thing happened. Then I tried S32K DS,it was downloaded and running normally.

The models i‘m trying to buiid is the example models of NXP MBDT 2018.R1(ADC、ADC1、ADC2).The download interface is opensda(both simulink and S32K DS). 

Thanks.

标记 (1)
0 项奖励
回复
5 回复数

1,855 次查看
mariuslucianand
NXP Employee
NXP Employee

Hi liuhuangc@sina.com‌,

We are currently out of office due to the Christmas Holidays so our answers will be delayed. The problem you are facing seems to be linked with the OpenSDA. When you are downloading it using our toolbox the program copies the .mot file in the newly mounted disk drive on OpenSDA while when downloading an S32K DS project it will use the OpenSDA as a JTAG. Maybe the OpenSDA firmware must be updated but unfortunately I can't provide one right now but I think you cand found one on PeMicro's website. 

But as a workaround, you can flash your MBDT generated code using the S32K DS. In the Simulink project generated folder you will find an .elf file. So flash that file using the S32DS on the board and I think the model generated code will work.

Hope this helps, 

Marius 

0 项奖励
回复

1,855 次查看
ca_liu
Contributor II

Hi Marius,

You are right, it is possible to download MBDT code to evb with S32K DS, but it will waste some time compared to direct download. If possible, I still want to build directly with simulink. As for the opensda update you mentioned, I downloaded the update package. The bootloader version is lower than the one on the board. Then I updated the opensda application file according to the evb manual, but the result is the same. Other than that, is there any other way?
The following figure shows the board information and update package information.

Thanks

evb information.png pastedImage_2.png

0 项奖励
回复

1,855 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello liuhuangc@sina.com‌,

I've checked and we are using the same version for OpenSDA. Another way you can try is to manually copy the .mot generated file in the Local Disk mounted when you connect the EVB. The OpenSDA will take the .mot file and flash it on the mcu. If not, a file (LASTSTAT.TXT) containing a status will be available on the mounted disk. Let's check the status.

Best regards,

Marius

0 项奖励
回复

1,855 次查看
ca_liu
Contributor II

Hi Marius,

Yes, this method is ok, I have tried this way. It's just that I don't quite understand why did this happenned. Will you continue to investigate? If so, can you tell me the result later?
No other questions, thank you.

0 项奖励
回复

1,855 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello liuhuangc@sina.com‌,

I am glad it works. So the OpenSDA seems to be fine, but now let's investigate a little bit the settings from your model. 

You can try this:

1.Please check that your settings are right: 

         - the Download Code after Build is checked

         - the Download Interface is OpenSDA

         - the OpenSDA Drive Name is the right one. Also if the Refresh button does not shows you the right Drive letter, please select custom and type the right letter. 

 pastedImage_1.png

2. Delete the .mot file from the OpenSDA S32K146EVB Local Disk mounted, and after that please rebuild your model and check if the new .mot has been copied on the S32K146EVB Local Disk. If this happens the transfer between Simulink and board might work. '

If all of the above steps are not successful please after program board using them check the status file from the OpenSDA and replay here the file content. 

Please also consider sending us your model to check here if works or not. 

Best regards, 

Marius

0 项奖励
回复