S32K MBD-Toolbox generate code for IAR bug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K MBD-Toolbox generate code for IAR bug

3,046件の閲覧回数
cg0
Contributor II

Hello,I use matlab 2018b, And I generate code for IAR, I already install the patch.

After generate code, I import the code to IAR for more coding, also I select the "S32K14x.icf" as Linker file. But it always run into fault. Because before I choose the .icf file from matlab, and this situation can run normally.

So, I replace the .icf file, it do works. Then I compare the two .icf file. The matlab generated .icf alway use S32K148 256k flash.icf, no matter what MCU selected.

ラベル(2)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

2,852件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello cg0‌,

Thank you for your investigation! We will make this fix and provide a patch in the S32K Hotfixes page, but we'll do so most probably in May, after the Holidays are over.

Kind regards,

Razvan.

0 件の賞賛
返信

2,852件の閲覧回数
cg0
Contributor II

Hi Razvan

As I know  from https://community.nxp.com/thread/484197, the next version will be released this Q2. Could you tell me will S32K116/118 be added in?

0 件の賞賛
返信

2,852件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello cg0‌,

Indeed, S32K116/118 will be added in our next release.

Kind regards,

Razvan.

0 件の賞賛
返信