HotFix: MBD Toolbox 2018.R1 for S32K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HotFix: MBD Toolbox 2018.R1 for S32K

11,149 Views
constantinrazva
NXP Employee
NXP Employee

HotFix_1: CAN extended ID not working properly

 

Problem: When trying to send with extended ID, it does not set the proper configurations

 

Root Cause: Coding building error

 

Workaround:  Update the files attached in the following folders 

 {install_dir}\mbdtbx_s32k14x\mbdtbx_s32k14x\mscripts\fcan\mbd_s32k14_fcan_send_sdk_params.p

Customer Report: 

Special thanks to gramirezv‌  for reporting and testing our fix.

Labels (1)
9 Replies

9,714 Views
constantinrazva
NXP Employee
NXP Employee

Cumulative patch:

Starting from today, all patches will come in the form of self-extracting zips and will contain all the patches, up-to-date. A user can install at any point in time the latest patch and get all the patches from before, regardless if he had or had not installed some previous patch.

Usage:

Run MBDT_cumulative_patch_1.exe and enter the following path when prompted:

{YOUR_INSTALL_DIR}\NXP_MBDToolbox_S32K1xx\code

e.g.: C:\Users\my_user_name\Documents\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\code

Most likely you will be asked if you want to overwrite some files - just click on 'Yes to All' option. 

MBDT_cumulative_patch_1 contains:

  • HotFix1 - CAN extended ID not working properly
  • HotFix2 - SPI Peripheral Chip Select
  • HotFix3 - GCC 6.3 compilation error

MBDT_cumulative_patch_2 contains:

  • All fixes from MBDT_cumulative_patch_1
  • HotFix4 - CAN Receive individual masking not working as expected

MBDT_cumulative_patch_3 contains:

  • GCC makefile error - nosys.specs not finding file
0 Kudos
Reply

9,716 Views
sparkee
Contributor V

Is this necessary if we have the latest 4.1 build of the toolbox?

0 Kudos
Reply

9,716 Views
constantinrazva
NXP Employee
NXP Employee

Hello sparkee‌,

It is not necessary - these were integrated in the 4.1 version. Furthermore, if you install these updates over v4.1, you'll break some links to our blocks. We'll make another hotfix page when issues are found and fixed for v4.1.

Kind regards,

Razvan.

9,716 Views
JesseBeeker
Contributor III

Thank you for the patch. I have been installing everything in the default method and there is not a \code directory that was used in the referenced path. It seems to line up with this path without the \code folder, which does not exist in my 4.0.0 install on R2018b.

...\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx

0 Kudos
Reply

9,716 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi JesseBeeker‌,

The existence of the "code" folder is dictated&controlled by the MATLAB version used: for 2018a or smaller the installation of the toolboxes (any) will be placed in "code" folder while on the newer versions of MATLAB that "code" folder is no longer used.

Thanks for bringing this in discussion, and hopefully making this clear for everyone using our toolboxes.

Best regards,

Daniel

9,716 Views
constantinrazva
NXP Employee
NXP Employee

HotFix_3: GCC 6.3 compilation error

 

Problem: Not able to build any model using gcc 6.3 due to missing path to libwinpthread-1.dll missing.

 

Root Cause: Missing path to .dll

 

Workaround:  Update the files attached in the following folders 

{MBDT_ROOT}\mbdtbx_s32k14x\mbdtbx_s32k14x\mbd_s32k14_make_rtw.p [modify]

{MBDT_ROOT}\mbdtbx_s32k\mscripts\utils\mbd_s32k_add_gcc_to_path.p [add]

0 Kudos
Reply

9,716 Views
constantinrazva
NXP Employee
NXP Employee

HotFix_5: GCC makefile error - nosys.specs not finding file

 

Problem: GCC compilation fails when having spaces in the path

" No such file or directory arm-none-eabi-gcc: error: nosys.specs: No such file or directory"

 

Root Cause: Paths not taken into account in the template makefile for the -nosys.specs option.

 

Workaround: Install cumulative patch (minimum version 3)

For this fix, the patch will replace mbd_s32k14.tmf fiile.

0 Kudos
Reply

9,716 Views
constantinrazva
NXP Employee
NXP Employee

HotFix_4: CAN Receive individual masking not working as expected

 

Problem: When using CAN Receive block, individual masking is not enabled

 

Root Cause: Reset value of MCR[IRMQ] is 0 - global masking enabled;

 

Workaround:  Update the following file:

{ROOT_DIR}\mbdtbx_s32k14x\mbdtbx_s32k14x\blocks\fcan\fcan_s32k14_receive.tlc

which enabled individual masking for MBs.

Customer Report: 

Special thanks to [email protected] for reporting this issue and testing our fix!

0 Kudos
Reply

9,712 Views
constantinrazva
NXP Employee
NXP Employee

HotFix_2: SPI Peripheral Chip Select

 

Problem: Not able to change PCS on every transfer - only from Configuration block; this limits the SPI usage to 1 PCS.

Edit: Not able to select only the PCS pins that you need to use.

 

Root Cause: Lack of use-cases/examples

 

Workaround:  Update the files attached in the following folders 

- lpspi_s32k14_config.tlc move to {TOOLBOX_ROOT_DIR}\mbdtbx_s32k14x\mbdtbx_s32k14x\blocks\lpspi folder

- lpspi_s32k14_master_transfer.tlc move to {TOOLBOX_ROOT_DIR}\mbdtbx_s32k14x\mbdtbx_s32k14x\blocks\lpspi folder

- lpspi_s32k14_slave_transfer.tlc move to {TOOLBOX_ROOT_DIR}\mbdtbx_s32k14x\mbdtbx_s32k14x\blocks\lpspi folder

- mbd_s32k14_ec_toolbox.mdl move to move to {TOOLBOX_ROOT_DIR}\mbdtbx_s32k14x\mbdtbx_s32k14x folder

- mbd_s32k14_lpspi_get_pin_info.p move to {TOOLBOX_ROOT_DIR}\mbdtbx_s32k14x\mbdtbx_s32k14x\mscripts\lpspi folder 

- mbd_s32k14_lpspi_instance_callback.p move to {TOOLBOX_ROOT_DIR}\mbdtbx_s32k14x\mbdtbx_s32k14x\mscripts\lpspi folder 

- mbd_s32k14_lpspi_transfer_sdk_params.p move to {TOOLBOX_ROOT_DIR}\mbdtbx_s32k14x\mbdtbx_s32k14x\mscripts\lpspi folder

 

Customer Report: 

Special thanks to Gustavo Ramirez  for reporting this issue and testing our fix!