Re: Why can't I use processor expert in S32 design(for PA)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: Why can't I use processor expert in S32 design(for PA)?

1,139件の閲覧回数
Zhangfeng1
Contributor I

Hi Lukas,

I have a devkit-MPC5744p,i am using the MBD toolbox and i want to write data in the flash.But there's no such a block in this toolbox.So i would like to write some code to deal with this problem.

The S32DS's version is S32DS_Power_Win32_v2017.R1_b171019.It seems like i only have two SDKs,one is FreeMaster_MPC57xx 2.0.0,the other is MPC574xP_AMMCLIB_s32ds 1.1.9.

Regards,

Zhang Feng

0 件の賞賛
返信
1 返信

1,127件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

SDK for MPC5744P was available right at the beginning, it was available already in early release 0.8.2 in first update and there's RTM3.0.0 in the last update 11 for S32DS 2017.R1. So, you can check if you have the latest update installed:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-Power-Architectu...

Because it is related rather to MBDT, I will move this thread to MBDT community space, I guess they could provide more help in this matter.

Regards,

Lukas

 

 

0 件の賞賛
返信