Re: Pil Mode on KV3x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: Pil Mode on KV3x

1,756件の閲覧回数
pbgemann001
Contributor III

Hi paulvlase,

another problem occured. After setting up on another PC everything except the PIL works. I get the following error

PILfail.PNG

I am using the same model, Matlabversion and DevBoard as before.

I will attach the slprj and the diagnostics output.

I guess it has to do with the location of files again? I have installed Matlab in D instead C on this PC could that be the cause?

Thank you for your help

Paul

0 件の賞賛
返信
1 返信

1,615件の閲覧回数
paulvlase
NXP Employee
NXP Employee

Hi [email protected]‌,

Sorry for answering so late, but we were working on MBDT for S32K 4.0.1 release.

Right now the PIL is not working using the GCC compiler, somehow the application crashes on the board. I mentioned that here https://community.nxp.com/message/1145564#comment-1162694 .

I will try to fix this issue the next week.

Can you try to run PIL simulation using the IAR compiler?

0 件の賞賛
返信