Question about etimer(MPC5744) in simulink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about etimer(MPC5744) in simulink

3,315件の閲覧回数
ebookkankan
Contributor II

Dear All:

       How can I solve the problem about etimer(MPC5744) in simulink?

      I  am using the Devkit MPC5744P Rev B and the Model Based Design Toolbox 3.0.0(in matlab2018b).When I run the example about "etimer",it shows error.

pastedImage_5.png

pastedImage_7.png

pastedImage_8.png

Who can help me?

Thanks.

wangzhe

0 件の賞賛
返信
4 返答(返信)

3,169件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Your question is the same with the one asked here etimer_output_frequency_mpc574xP for MBD Toolbox? so we will continue to discuss this topic there.

Thank you,

Marius

0 件の賞賛
返信

3,169件の閲覧回数
haoxue1027
Contributor V

Hello,

Sorry to confirm for you.

Is the error above solved?

best regards

hao 

0 件の賞賛
返信

3,169件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Well, to be honest with you, the Model-Based Design Toolbox 3.0.0 is two versions behind So we strongly suggest start using the 3.0.2 version. There are a lot of patches already integrated into the latest version.

 

By the way, this error appears during code generation? or when you simulate something?

Hope this helps,

Marius

3,169件の閲覧回数
haoxue1027
Contributor V

Hello,Marius.

The errors occured when I simulate that.

The code generation is normal.

best regards 

hao

0 件の賞賛
返信