Question about etimer(MPC5744) in simulink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question about etimer(MPC5744) in simulink

2,390 次查看
ebookkankan
Contributor II

Dear All:

       How can I solve the problem about etimer(MPC5744) in simulink?

      I  am using the Devkit MPC5744P Rev B and the Model Based Design Toolbox 3.0.0(in matlab2018b).When I run the example about "etimer",it shows error.

pastedImage_5.png

pastedImage_7.png

pastedImage_8.png

Who can help me?

Thanks.

wangzhe

0 项奖励
回复
4 回复数

2,244 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello ebookkankan@sina.com‌,

Your question is the same with the one asked here etimer_output_frequency_mpc574xP for MBD Toolbox? so we will continue to discuss this topic there.

Thank you,

Marius

0 项奖励
回复

2,244 次查看
haoxue1027
Contributor V

Hello,

Sorry to confirm for you.

Is the error above solved?

best regards

hao 

0 项奖励
回复

2,244 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello haoxue1027@qq.com‌,

Well, to be honest with you, the Model-Based Design Toolbox 3.0.0 is two versions behind So we strongly suggest start using the 3.0.2 version. There are a lot of patches already integrated into the latest version.

 

By the way, this error appears during code generation? or when you simulate something?

Hope this helps,

Marius

2,244 次查看
haoxue1027
Contributor V

Hello,Marius.

The errors occured when I simulate that.

The code generation is normal.

best regards 

hao

0 项奖励
回复