Question about etimer(MPC5744) in simulink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about etimer(MPC5744) in simulink

3,314 Views
ebookkankan
Contributor II

Dear All:

       How can I solve the problem about etimer(MPC5744) in simulink?

      I  am using the Devkit MPC5744P Rev B and the Model Based Design Toolbox 3.0.0(in matlab2018b).When I run the example about "etimer",it shows error.

pastedImage_5.png

pastedImage_7.png

pastedImage_8.png

Who can help me?

Thanks.

wangzhe

0 Kudos
Reply
4 Replies

3,168 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Your question is the same with the one asked here etimer_output_frequency_mpc574xP for MBD Toolbox? so we will continue to discuss this topic there.

Thank you,

Marius

0 Kudos
Reply

3,168 Views
haoxue1027
Contributor V

Hello,

Sorry to confirm for you.

Is the error above solved?

best regards

hao 

0 Kudos
Reply

3,168 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Well, to be honest with you, the Model-Based Design Toolbox 3.0.0 is two versions behind So we strongly suggest start using the 3.0.2 version. There are a lot of patches already integrated into the latest version.

 

By the way, this error appears during code generation? or when you simulate something?

Hope this helps,

Marius

3,168 Views
haoxue1027
Contributor V

Hello,Marius.

The errors occured when I simulate that.

The code generation is normal.

best regards 

hao

0 Kudos
Reply