Problem when I try load my program in MDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem when I try load my program in MDB

12,711 Views
JonAnder_Amante
Contributor II

Hi,

 

I am using th example of "s32k344_mc_pmsm_2sh_s32ct" with model based design in simulinkin version 2022b. When I try to load to my Kit MCSPTE1AK344 I can´t load well and I don´t get any result. Moreover, I think the file .mex it´s wrong so someone can give a project with .mex?

JonAnder_Amante_0-1760514649079.png

 

Could you give some solution?

 

Thank you,

0 Kudos
Reply
18 Replies

12,736 Views
JonAnder_Amante
Contributor II

Hi,

I have bought your Kit MCSPTE1AK344 but I have different problems when I try to load. I open my project called "s32k344_mc_pmsm_2sh_s32ct" but I have always the same error. I have donde your steps to load but I don´t get nothing. 

JonAnder_Amante_0-1760430742948.png

Thank you,

 

Jon Ander Amante

 

0 Kudos
Reply

12,679 Views
stefanvlad
NXP Employee
NXP Employee

Hi @JonAnder_Amante ,

 

Thank you for using MBDT for S32K3,

I do recommend you follow the Getting started with MCSPTE1AK344  | NXP Semiconductors

Have you connected USB cable to the board and PC? 

3.5 Connect the Debugger Cable

Connect a micro-USB cable to the J40 connector to debug via the onboard S32K3 debugger.

 

 

If yes, than can you open Device Manager, to see if the PEMicro shows up as OpenSDA Debug Driver and OpenSDA CDC Serial Port:

stefanvlad_2-1760519200655.png

if not, than you need to install the latest PEmicro drivers from PEmicro Hardware Interface Drivers, v.12 (7/8/10/11)

 

Best regards,

Stefan V.

 

0 Kudos
Reply

12,662 Views
JonAnder_Amante
Contributor II

Hi, 

I have already connected USB cable to the board and PC but I have looked Device manager and I don´t PE micro drivers. Could you tell me which I have to install?

Thank you, 

 

 

 

 

 

 

0 Kudos
Reply

12,651 Views
stefanvlad
NXP Employee
NXP Employee

Hi @JonAnder_Amante ,

 

I have send the link above, but once again, here it is: https://www.pemicro.com/downloads/download_file.cfm?download_id=53

 

Regards,

Stefan V.

0 Kudos
Reply

12,731 Views
JonAnder_Amante
Contributor II

When I try to show the errors I have:

JonAnder_Amante_0-1760431043698.png

 

0 Kudos
Reply

12,556 Views
JonAnder_Amante
Contributor II

Hi, 

 

I get to load my program but my led is always red and never change to blue or green. My exmaple of program is "S32K344_mc_pmsm_2sh_S32ct" and my version of matlab is R2022b. Could you give any solution?

0 Kudos
Reply

12,676 Views
JonAnder_Amante
Contributor II

Hi, 

 

Sorry but I have a critical question. I am using Simulink with Model Based Design but I haven´t installed the application S32 Design studio. I have bought a kit MCSPTE1AK344 and I am trying to compile the example of project called "S32K344_mc_pmsm_2sh_s32ct". I compile well but when I open the configuration of pins, peripherals ... appear empty (in this picture you can see the configuration). I don´t know if you need to install S32 Design studio to see well the configuration. Moreover, the version of Matlab and Simulink and S32 Design Studio is important as I have 2022b version in Matlab in Simulink. 

JonAnder_Amante_0-1760526060297.png

 

Thank you for all, 

0 Kudos
Reply

12,622 Views
dragostoma
NXP Employee
NXP Employee

Hi, @JonAnder_Amante,

Please consider the following aspects: S32 Design Studio is an IDE used for debugging, but its absence does not affect the proper functioning of the toolbox. S32 Configuration Tools is the utility through which you configure pins, clocks, peripherals, and all necessary settings required to build a model. It can be confusing because S32 Configuration Tools is also integrated into S32 Design Studio, which may lead to some misunderstanding. However, for the current situation, installing S32 Design Studio is not required.

Furthermore, what you see in the image is not empty. You have simply selected the Functional Group named Adc_Pins_MBDT from the dropdown menu in the top bar, which displays only the pins configured for the ADC peripheral. By clicking on the Functional Group section, you will be able to select the pins you need.

dragostoma_0-1760596890005.png

The image you presented is from the Pins tab, but by switching to the Peripherals tab, you can view the configuration settings for each individual peripheral. Similarly, you can switch between tabs depending on what you need to modify or inspect: Pins, Peripherals, or Clocks.

dragostoma_1-1760597279202.png

 

Hope this helps,

Dragos

 

 

0 Kudos
Reply

12,607 Views
JonAnder_Amante
Contributor II

Hi, 

 

I get to load my program but my led is always red and never change to blue or green. My example of program is "S32K344_mc_pmsm_2sh_S32ct" and my version of matlab is R2022b. Could you give any solution?

0 Kudos
Reply

12,582 Views
stefanvlad
NXP Employee
NXP Employee

Hi @JonAnder_Amante 

 

Have you followed the steps in Getting started with MCSPTE1AK344  | NXP Semiconductors

3.4 Plug in the Power Supply

Switch SW1 to the OFF position (fully to the left).

Connect the 12 V power supply adapter

and switch SW1 to the ON position (fully to the right).

When power is applied to the EVB, four orange LED’s adjacent to the voltage regulators show the presence of the supply voltages (12 V, 5 V, 3.3 V and 1.5 V).

 

Also check if the GD3000 board is properly inserted into the S32K344-T172 board, by pressing on the Pins headers.

 

Best regards,

Stefan V.

 

0 Kudos
Reply

12,538 Views
JonAnder_Amante
Contributor II

Hi,

I have connected all connections well but I have the same problem so the led is always red. Moreover, if I look the interfaz of freemaster I have different problems in current Ia and current Ib. 

JonAnder_Amante_0-1760623988330.png

 

0 Kudos
Reply

12,530 Views
stefanvlad
NXP Employee
NXP Employee

Hi @JonAnder_Amante 

 

The FreeMaster S32K_PMSM_Sensorless.pmpx file you opened is not from MBDT S32K3 Toolbox, it is from the Bare-metal C code from C:\NXP\MC_DevKits\MCSPTE1AK344\sw\MCSPTE1AK344_PMSM_FOC_2Sh_ll

 

Use MBDT S32K3 Toolbox project from S32K3\src\S32K3_Examples\mc\PMSM\s32k344_mc_pmsm_2sh_s32ct 

  • open the model s32k344_mc_pmsm_2sh_s32ct.mdl and press CTRL+B to build and deploy
  • or you can flash the .elf file on the S32K344 board with Matlab command: >> mbd_s32k3.nxp.download.jtag('s32k344_mc_pmsm_2sh_s32ct.elf','S32K344')
  • open the corresponding FreeMaster file: s32k344_mc_pmsm_2sh_s32ct.pmpxstefanvlad_1-1760629608356.png

 

Second i have kindly asked you to press on the GD3000 Pin Headers to make better contact with S32K344-T172 board, as in the picture below:

MCTPTX1AK344 Press on Headers Pins.png

 

Third , have you connected the 12V power supply on the GD3000 board, as below?

 

 

 

Can you send me a picture with your boards and setup? 

Have you followed the steps above?

 

0 Kudos
Reply

12,146 Views
JonAnder_Amante
Contributor II

Hi,

 

I have managed to get the engine to turn correctly but I have a qquestion. When I open freemaster there are some variables that have a interrogation and I don´t know why. 

JonAnder_Amante_0-1760947261551.png

JonAnder_Amante_1-1760947279395.png

Thank you for all

 

Tags (1)
0 Kudos
Reply

12,084 Views
stefanvlad
NXP Employee
NXP Employee

Hi @JonAnder_Amante ,

 

Some variables appear with "?" since they haven't been implemented in the Simulink model, as the FreeMASTER project comes from the bare metal S32K3 Motor control SW examples.

 

What was the problem regarding your setup? can you please provide feedback? 

 

Also, i recommend you press button "Accept as Solution" the topic that helped you solve the issues you had, in order to close this topic 

 

Best regards,

Stefan V.

0 Kudos
Reply

11,967 Views
JonAnder_Amante
Contributor II

HI, 

 

Today I load my project but suddenly the led switched off and the chip FS26 started to heat so I don´t know if I have done dead short.

0 Kudos
Reply

11,912 Views
stefanvlad
NXP Employee
NXP Employee

Hi @JonAnder_Amante ,

 

Sorry to hear that, you can check voltages in the S32K344-T172 Schematic, there is also a block diagram: 

stefanvlad_0-1761054124375.png

 

You can order a new board from S32K3X4EVB-T172 Evaluation Board

or you can also order the new S32K312MINI-EVB Evaluation Board

 

Best regards,

Stefan V.

0 Kudos
Reply

12,668 Views
JonAnder_Amante
Contributor II

Hi,

 

I have found the solution but I have another problem. I got debug my project but in the example which I told you, the configuration of S32 Config tool is empty as there aren´t any pin configured. The example is "S32K344_mc_pmsm_2sh_s32ct". I don´t know if you can help me. Thank you

 

JonAnder_Amante_1-1760523802657.png

 

0 Kudos
Reply

12,643 Views
stefanvlad
NXP Employee
NXP Employee

Hi @JonAnder_Amante ,

 

In the screenshot you provided there is ADC_POT0 pin PTA11, there are more pins in Functional Group, by selecting other than Adc_Pins_MBDT. 

Also press on Pin Name to sort it, and you will see all green highlighted pins that are used:

stefanvlad_0-1760536082064.png

 

For more details we have a compressive guide here Interacting with Digital Inputs/Outputs on MR-CANHUBK344 - NXP Community

 

Regards,

Stefan V.

0 Kudos
Reply