NXP Model-Based Design Toolbox for S32K3 is not found by MATLAB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Model-Based Design Toolbox for S32K3 is not found by MATLAB

Jump to solution
2,246 Views
JohnHarmon
Contributor I

After I install the sw32_mbdt_s32k3_1.6.0_d2501.mltbx I get the following error when I try to Verify the installation although I have checked that the installation exists.

JohnHarmon_0-1760555486075.png

 

0 Kudos
Reply
1 Solution
2,215 Views
dragostoma
NXP Employee
NXP Employee

Hi, @JohnHarmon,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

We have recently released a new version of the toolbox (Model-Based Design Toolbox for S32K3 version 1.7.0). You may upgrade to this version and try reinstalling the toolbox using the Support Package installer. Please note that the toolbox can also be installed without using the Support Package utility—simply by dragging and dropping the .mltbx file. This method allows you to use the toolbox without encountering the verification issues experienced previously.

 

Hope this helps,

Dragos

View solution in original post

0 Kudos
Reply
1 Reply
2,216 Views
dragostoma
NXP Employee
NXP Employee

Hi, @JohnHarmon,

Thank you for your interest into Model-Based Design Toolbox for S32K3.

We have recently released a new version of the toolbox (Model-Based Design Toolbox for S32K3 version 1.7.0). You may upgrade to this version and try reinstalling the toolbox using the Support Package installer. Please note that the toolbox can also be installed without using the Support Package utility—simply by dragging and dropping the .mltbx file. This method allows you to use the toolbox without encountering the verification issues experienced previously.

 

Hope this helps,

Dragos

0 Kudos
Reply