NXP MBDT model

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP MBDT model

1,727件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport
Hello,

In my NXP MBDT model, I'm using two I2C config block which is I2C-Channel 0 and I2C-Channel 1 for a particular application, Now while I'm generating the code it show the error of 'redefinition of the LPI2C config function' . How can I solve it
 
Best regards,
Peter
0 件の賞賛
返信
2 返答(返信)

1,593件の閲覧回数
SorinIBancila
NXP Employee
NXP Employee

Hello, 

Indeed there is a bug in the implementation of the LPI2C. Can you please download and install this hotfix and see if it solves the problem?

Best regards,

Bancila Sorin

0 件の賞賛
返信

1,628件の閲覧回数
Johnwhitee
Contributor I

Hello,

In my NXP MBDT model, I'm using two I2C config block which is I2C-Channel 0 and I2C-Channel 1 for a particular application, Now while I'm generating the code it show the error of 'redefinition of the LPI2C config function' . How can I solve it

Best regards,
Peter

Hello,

To resolve the redefinition of the LPI2C config function error in your NXP MBDT model, ensure that you have distinct and unique function names for configuring I2C-Channel 0 and I2C-Channel 1. Avoid using the same function name for both configurations. This will prevent the compiler from encountering a naming conflict, allowing you to generate the code without errors. 

 

 

 

0 件の賞賛
返信