NXP MBDT model

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP MBDT model

1,739 次查看
petervlna
NXP TechSupport
NXP TechSupport
Hello,

In my NXP MBDT model, I'm using two I2C config block which is I2C-Channel 0 and I2C-Channel 1 for a particular application, Now while I'm generating the code it show the error of 'redefinition of the LPI2C config function' . How can I solve it
 
Best regards,
Peter
0 项奖励
回复
2 回复数

1,605 次查看
SorinIBancila
NXP Employee
NXP Employee

Hello, 

Indeed there is a bug in the implementation of the LPI2C. Can you please download and install this hotfix and see if it solves the problem?

Best regards,

Bancila Sorin

0 项奖励
回复

1,640 次查看
Johnwhitee
Contributor I

Hello,

In my NXP MBDT model, I'm using two I2C config block which is I2C-Channel 0 and I2C-Channel 1 for a particular application, Now while I'm generating the code it show the error of 'redefinition of the LPI2C config function' . How can I solve it

Best regards,
Peter

Hello,

To resolve the redefinition of the LPI2C config function error in your NXP MBDT model, ensure that you have distinct and unique function names for configuring I2C-Channel 0 and I2C-Channel 1. Avoid using the same function name for both configurations. This will prevent the compiler from encountering a naming conflict, allowing you to generate the code without errors. 

 

 

 

0 项奖励
回复