MPC5748G PIL timeout error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G PIL timeout error

ソリューションへジャンプ
2,013件の閲覧回数
championzhang
Contributor I

Hello,

I recently brought MPC5748G REV board. 

I am using MATLAB 2018b

I tried to run the example in MPC _Example -> common-.> Pil 

code gets generated, compiled, flashing starts with erasing and completes 100%.

Then error comes and stops. 

Error: "The Timeout of 10 seconds for receiving...." 

I am sure is the problem that the wrong set of the PIL interface!

How to set the PIL interface? (as shown in the following figure)

屏幕截图 2022-03-30 213519.jpg

Thanks in advance

 

0 件の賞賛
返信
1 解決策
1,989件の閲覧回数
championzhang
Contributor I

I got it!

答案如下图所示,哈哈,完美运行 

微信图片_20220331133013.png

元の投稿で解決策を見る

1 返信
1,990件の閲覧回数
championzhang
Contributor I

I got it!

答案如下图所示,哈哈,完美运行 

微信图片_20220331133013.png