MPC5744P does not work properly for PWM input capture based on MBD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P does not work properly for PWM input capture based on MBD

1,492件の閲覧回数
Yunhe
Contributor I

Hi, 

When I configured input capture based on MBD to measure the frequency and duty cycle of PWM, I encountered a problem:
First of all, I configured one input capture according to the official example, as follows:

1010183396_0-1640431580335.png

The code generated by this model is working properly,Then I continued to configure a few others, but found that they did not work properly, the configuration is as follows:

Through debug, it was found that this inoperable code did not generate a configured interrupt, that is, Input Capture 2 Flag Interrupt, and the corresponding interrupt function is as follows:

1010183396_1-1640431723584.png

Of course, I have set the corresponding interrupt in the model and made sure that the PWM signal is input to the chip, as follows:

1010183396_2-1640431830563.png

Later, normal operation can be realized through the register, and the corresponding configuration is as follows:

void ETimer_EtcInit(u8 ucETimerNo, u8 ucChNo)
{
	pETIMER[ucETimerNo]->ENBL.R &= (~((1<<ucChNo)));// disable Timer channels
	/* CTRL1---0x3F00
	 * bit15-13:	CNTMODE = 1	count rising edge of primary source
	 * bit12-8:	PRIsrc=0x1F	ip bus clock divide by 128
	 * bit12-8:	PRIsrc=0x1C	ip bus clock divide by 16
	 * bit7:	ONCE	= 0	count repeatedly
	 * bit6:	LENGTH	= 0	continue counting to roll over
	 * bit5:	DIR	= 0	count up
	 * bit4-0:	SECsrc=n	counter #n input pin
	 */
#if (PWM_FRE_RANGE == RANGE_HIGH)
	pETIMER[ucETimerNo]->CH[ucChNo].CTRL1.R = 0x3C00 | (ucChNo);
#else
	pETIMER[ucETimerNo]->CH[ucChNo].CTRL1.R = 0x3F00 | (ucChNo);
#endif
	pETIMER[ucETimerNo]->CH[ucChNo].COMP1.R = 0xFFFF;
	/* CCCTRL---0x0264
	 * bit15-13:	CLC2	= 0	never preload
	 * bit12-10:	CLC1	= 0	never preload
	 * bit9-8:	CMPMODE	= 2	comp1 for counting up;	comp2 for counting down
	 * bit7-6:	CPT2MODE= 1	CAPT2	capture falling edge
	 * bit5-4:	CPT1MODE= 2	CAPT1	capture rising edge
	 * bit3-2:	CFWM	= 1	capture FIFO water mark
	 * bit1:	ONESHOT	= 0	free running(not one shot mode)
	 * bit0:	ARM	= 0	input capture disable
	 */
	pETIMER[ucETimerNo]->CH[ucChNo].CCCTRL.R = 0x0264;
	/* INTDMA---0x0080
	 * bit15:	ICF2DE	= 0	Input Capture 2 Flag DMA disable
	 * bit14:	ICF1DE	= 0	Input Capture 1 Flag DMA disable
	 * bit13:	CMPLD2DE= 0	Comparator Load Register 2 Flag DMA disable
	 * bit12:	CMPLD1DE= 0	Comparator Load Register 1 Flag DMA disable
	 * bit9:	WDFIE	= 0	Watchdog Flag Interrupt disable
	 * bit8:	RDFIE	= 0	Redundant Channel Flag Interrupt disable
	 * bit7:	ICF2IE	= 1	Input Capture 2 Flag Interrupt enable
	 * bit6:	ICF1IE	= 0	Input Capture 1 Flag Interrupt  disable
	 * bit5:	IEHFIE	= 0	Input Edge High Flag Interrupt  disable
	 * bit4:	IELFIE	= 0	Input Edge Low Flag Interrupt  disable
	 * bit3:	TOFIE	= 0	Timer Overflow Flag Interrupt  enable
	 * bit2:	TCF2IE	= 0	Timer Compare 2 Flag Interrupt  disable
	 * bit1:	TCF1IE	= 0	Timer Compare 1 Flag Interrupt  disable
	 * bit0:	TCFIE	= 0	Timer Compare Flag Interrupt  disable
	 */
	pETIMER[ucETimerNo]->CH[ucChNo].INTDMA.R = 0x0080;		//Input Capture 2
	pETIMER[ucETimerNo]->CH[ucChNo].CTRL3.R	= 1;

	pETIMER[ucETimerNo]->ENBL.R |= (1<<ucChNo);				// enable Timer channels

	pETIMER[ucETimerNo]->CH[ucChNo].CCCTRL.B.ARM = 1;// input capture enable
}

Finally, after configuring the model according to the corresponding register, the code generated by the model still does not work properly。

I put all the models in the attachment:
The first model is a model that can work normally, and the second is a model that does not work properly。

Kind regards,

zhang.

0 件の賞賛
返信
0 返答(返信)