MPC5744P EVB Locked during programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P EVB Locked during programming

2,073件の閲覧回数
davischen
Contributor I

Hi  Daniel,

We have meet a stranged situation: Our EVB has been locked during programming with this operation of this chapter. 

I have attached the last screenshot,

a867b3896ca5ae35818726ebfdd7b11.png

and it cannot be programmed with other application anymore.

wrong.jpg

It seems this board has been secured. But I think I do not do any relative action.

However, I have do this with others and works well.

Do you have any idea about this?

Thanks, BR.

Davis

0 件の賞賛
返信
2 返答(返信)

1,960件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi davischen,

Did it happen after or during you have programmed the elf with RAppID bootloader?

Apparently, the microprocessor is dead or in a continuous reset - i do not think it is secured.

If you try to connect over the JTAG directly (not over the USB) can you connect with the device ?

Best regards,
Daniel

0 件の賞賛
返信

1,960件の閲覧回数
davischen
Contributor I

Hi Daniel,

Thanks for your reply.

Yes, it is. In the meantime, I also have tried cyclone-max to program it (with JTAG), and it cannot be programmed well anymore.

It seems I enable this lock feature during my opration.

But I just wonder how it happen...

BR.

Davis

0 件の賞賛
返信