MPC564xL Motor Control Toolbox patch for Matlab/Simulink 2017b

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC564xL Motor Control Toolbox patch for Matlab/Simulink 2017b

3,748 次查看
mcgillformulael
Contributor I

Hello,

We are having trouble with the hardware implementation of our MPC564xL with Matlab & Simulink R2017b. Indeed, our Motor Control Toolbox Hardware Implementation blocks are not compatible with R2017b, and return errors when trying to generate code with Simulink. See picture attached. As seen, even the simplest model leads to an error when trying to generate code. "Undefined function 'slsfnagctlr' for input arguments of type 'char'." 

Therefore, I wanted to know if this is an issue that can be fixed? I have seen the same issue on the Community Forum but with a different Microprocessor. Would it be possible to fix the issue also on the MPC564xl?

Kind Regards,

Michael

McGill Formula Electric

标记 (3)
0 项奖励
回复
2 回复数

3,308 次查看
paulvlase
NXP Employee
NXP Employee

Hi mcgillformulaelectric‌,

I've created HotFix_1 for this. Can you please try it and confirm that it works for you?

Thank you,

Paul

0 项奖励
回复

3,308 次查看
mcgillformulael
Contributor I

Hi paulvlase‌,

Thank you for your excellent support. The patch did work!

Best,

Michael

0 项奖励
回复