MODEL BASED DESIGN TOOLBOX [Registration Code, S32K144]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MODEL BASED DESIGN TOOLBOX [Registration Code, S32K144]

2,769 次查看
electronica2pow
Contributor III

Hello to the community,

I am owner of a S32K144 platform and i would like to download the "Model Based Design Toolbox", but when i click on the link appears a message: "There is currently no Software or Support in your account. To register a new product, enter the registrion code below." Where could i find the "Registration code" in order to download that model?

I was entering codes from the NXP package, but none of them works. 

Regards,

Jorge

标记 (2)
3 回复数

2,531 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Jorge, 

Please go to this link: Model-Based Design Toolbox|NXP 

Select Download

pastedImage_2.png

If you are logged in with a valid NXP account then you should see this page:

pastedImage_3.png

Can you confirm this ?

Perhaps the link you are trying to download is broken or the re-direct might not temporary working.

Hope this helps!

Daniel

2,531 次查看
electronica2pow
Contributor III

It was really helpful and you solved my problem Daniel.

But i want to tell you that your coworkers should give a look to the Reference Manual of the Toolbox: https://www.nxp.com/docs/en/reference-manual/MBDT-User-Manual-for-S32K.pdf 

Pictures don't appear, so maybe there is an issue there.

Thanks,

Jorge

0 项奖励
回复

2,530 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Jorge, 

Thank you for reporting the issue. Please use this one attached. I'll inform our web admin. Anyhow, please be aware that starting with v3.0.0 we have replaced the PDF documentation with MATLAB Help.

Best regards,
Daniel

0 项奖励
回复